![]() |
SDL API Guide for J721S2
|
This structure defines the inject error configuration.
Data Fields | |
uint32_t * | pErrMem |
uint64_t | errMem64 |
uint32_t | flipBitMask |
uint32_t | chkGrp |
uint32_t* SDL_ECC_InjectErrorConfig_t::pErrMem |
Address to inject error
uint64_t SDL_ECC_InjectErrorConfig_t::errMem64 |
Address to inject error for accessible mem where baseaddress is > 64-bits
uint32_t SDL_ECC_InjectErrorConfig_t::flipBitMask |
Bit location to flip bits
uint32_t SDL_ECC_InjectErrorConfig_t::chkGrp |
Group checker (for Interconnect RAM ID's only)