![]() |
SDL API Guide for J721S2
|
Header file containing various enumerations, structure definitions and function declarations for the VBUSM Slave Timeout Gasket IP.
(C) Copyright 2021, Texas Instruments, Inc.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
Neither the name of Texas Instruments Incorpo_toged nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Go to the source code of this file.
TOG configuration flags | |
This enumerator defines the possible configuration flags | |
#define | SDL_TOG_CFG_TIMEOUT 0x01U |
#define | SDL_TOG_CFG_INTR_PENDING 0x02U |
typedef uint8_t | SDL_TOG_cfgCtrl |
Data Structures | |
struct | SDL_TOG_errInfo |
This structure contains timeout error information. More... | |
struct | SDL_TOG_config |
This structure contains TOG configuration information. More... | |
struct | SDL_TOG_staticRegs |
Slave TOG Static Registers. More... | |
Functions | |
int32_t | SDL_TOG_init (SDL_TOG_Inst instance, const SDL_TOG_config *pConfig) |
Initialize TOG module with respect of instance. More... | |
int32_t | SDL_TOG_verifyConfig (SDL_TOG_Inst instance, const SDL_TOG_config *pConfig) |
Verifying written configuration with TOG module. More... | |
int32_t | SDL_TOG_setIntrEnable (SDL_TOG_Inst instance, SDL_TOG_IntrSrc intrSrcs, bool enable) |
Enable/disable interrupt source(s) More... | |
int32_t | SDL_TOG_clrIntrPending (SDL_TOG_Inst instance, SDL_TOG_IntrSrc intrSrc) |
Clear pending interrupt source(s) More... | |
int32_t | SDL_TOG_getIntrPending (SDL_TOG_Inst instance, SDL_TOG_IntrSrc *pPendInts) |
Get masked (enabled) pending interrupt sources. More... | |
int32_t | SDL_TOG_ackIntr (SDL_TOG_Inst instance, SDL_TOG_IntrSrc intrSrc, uint32_t ackCnt) |
Ack interrupt source. More... | |
int32_t | SDL_TOG_start (SDL_TOG_Inst instance) |
Start the timer counter. More... | |
int32_t | SDL_TOG_stop (SDL_TOG_Inst instance) |
Stop the timer counter. More... | |
int32_t | SDL_TOG_reset (SDL_TOG_Inst instance) |
Reset the timeout functionality. More... | |
int32_t | SDL_TOG_getErrInfo (SDL_TOG_Inst instance, SDL_TOG_errInfo *pErrInfo) |
Get timeout error information. More... | |
int32_t | SDL_TOG_getStaticRegisters (SDL_TOG_Inst instance, SDL_TOG_staticRegs *pStaticRegs) |
Readback Static configuration registers. More... | |
int32_t | SDL_TOG_setFlushMode (SDL_TOG_Inst instance, bool enable) |
Enable/disable flush mode. More... | |
int32_t | SDL_TOG_getIntrCount (SDL_TOG_Inst instance, SDL_TOG_IntrSrc intrSrc, uint32_t *pIntrCnt) |
Get interrupt count. More... | |