![]() |
SDL API Guide for J721S2
|
Header file containing various enumerations, structure definitions and function declarations for the Voltage and Thermal Monitor (VTM) IP.
Go to the source code of this file.
Data Structures | |
struct | SDL_VTM_tsGlobal_cfg |
VTM Global Configuration Registers. More... | |
struct | SDL_VTM_Ctrlcfg |
VTM temperature sensor band gap control. More... | |
struct | SDL_VTM_tsThrVal |
VTM temperature sensor threshold values. More... | |
struct | SDL_VTM_Stat_val |
VTM temperature sensor Stat values. More... | |
Typedefs | |
typedef uint8_t | SDL_VTM_configVdCtrl |
This enumerator define for VTM VD configuration valid map. More... | |
typedef uint8_t | SDL_VTM_configTsCtrl |
This enumerator define for VTM TS configuration valid map. More... | |
typedef uint8_t | SDL_VTM_vid_opp |
This enumerator defines the possible VID Codes to set various voltage domain supply voltages. More... | |
typedef uint8_t | SDL_VTM_ts_stat_vd_map |
This enumerator defines the core voltage domain mapping of VTM VD. More... | |
typedef uint16_t | SDL_VTM_intrCtrl |
This enumerator define for VTM Voltage domain threshold interrupt control. More... | |
typedef uint16_t | SDL_VTM_vdEvtSel_set |
This enumerator define for VTM Voltage domain Event selection set. More... | |
typedef uint32_t | SDL_VTM_tsGlobal_ctrl_valid_map |
This enumerator defines for VTM Temperature sensor id control update valid maps. This controls the selective update of the fields in the temperature sensor control field. More... | |
typedef uint8_t | SDL_VTM_tsGlobal_clkSel |
This enumerator define for VTM Temperature sensor global control Clock select options. More... | |
typedef uint8_t | SDL_VTM_tsGlobal_clkDiv |
This enumerator define for VTM Temperature sensor global control Clock divide options. More... | |
typedef uint8_t | SDL_VTM_tsGlobal_any_maxt_outrg_alert_en |
This enumerator define for VTM Temperature sensor global control any max temperature alert enable control. More... | |
typedef uint16_t | SDL_VTM_tsGlobal_samples_per_count |
This enumerator define for VTM Temperature sensor global control samples per count. More... | |
typedef uint8_t | SDL_VTM_tsCtrl_valid_map |
This enumerator define for VTM Temperature sensor control valid map. More... | |
typedef uint8_t | SDL_VTM_tsCtrl_max_outrg_alert |
This enumerator define for VTM temperature sensor band gap maximum temperature out of range alert control. More... | |
typedef uint8_t | SDL_VTM_tsCtrl_resetCtrl |
This enumerator define for VTM temperature sensor band gap reset control bits. More... | |
typedef uint8_t | SDL_VTM_tsCtrl_mode |
This enumerator define for VTM temperature sensor mode control bits. More... | |
typedef uint8_t | SDL_VTM_tsCtrl_singleshot_conv_stat |
This enumerator define for VTM temperature sensor band gap single shot mode start of conversion trigger. More... | |
typedef uint8_t | SDL_VTM_thr_valid_map |
This enumerator define for VTM Temperature Sensor thresholds valid bit map. More... | |
typedef uint8_t | SDL_VTM_Stat_read_ctrl |
This enumerator define for VTM temperature sensor STAT read valid map. More... | |
typedef int16_t | SDL_VTM_adc_code |
This enumerator define for VTM temperature sensor ADC code This is the data_out value of the temperature sensor stat register. More... | |
typedef uint8_t | SDL_VTM_vdEvt_status |
This enumerator define for VTM Voltage domain event status. More... | |
Functions | |
void | SDL_VTM_getSensorVDCount (const SDL_VTM_cfg1Regs *p_cfg1) |
get sensor and VD count More... | |
SDL_VTM_adc_code | SDL_VTM_getBestValue (SDL_VTM_adc_code c0, SDL_VTM_adc_code c1, SDL_VTM_adc_code c2) |
select best ADC code More... | |
SDL_VTM_adc_code | SDL_VTM_getAdcCode (const SDL_VTM_cfg1Regs_TMPSENS *p_sensor) |
read Temperature sensor ADC code More... | |
int32_t | SDL_VTM_vdSetOppVid (const SDL_VTM_cfg1Regs *p_cfg1, SDL_VTM_InstVd instance, SDL_VTM_vid_opp vid_opp, uint8_t vid_opp_val) |
set the VID OPP Code for VID OPP register More... | |
int32_t | SDL_VTM_vdGetOppVid (const SDL_VTM_cfg1Regs *p_cfg1, SDL_VTM_InstVd instance, SDL_VTM_vid_opp vid_opp, uint8_t *p_vid_opp_val) |
get VTM VID OPP Code from VID OPP register More... | |
int32_t | SDL_VTM_vdEvtSelSet (const SDL_VTM_cfg1Regs *p_cfg1, SDL_VTM_InstVd instance, SDL_VTM_vdEvtSel_set vd_temp_evts) |
set Voltage domain a event select and control set register. In this API, select which of the event contributions of the temp-monitors controlled by this VTM will contribute to generate the merged event/alerts of this VD. Any combination of them could be selected More... | |
int32_t | SDL_VTM_tsSetGlobalCfg (const SDL_VTM_cfg2Regs *p_cfg2, const SDL_VTM_tsGlobal_cfg *p_tsGlobal_cfg) |
VTM Temperature Sensor Set Global configuration values. More... | |
int32_t | SDL_VTM_tsGetGlobalCfg (const SDL_VTM_cfg2Regs *p_cfg2, SDL_VTM_tsGlobal_cfg *p_tsGlobal_cfg) |
VTM Temperature Sensor Get Global configuration values. More... | |
int32_t | SDL_VTM_tsSetCtrl (const SDL_VTM_cfg2Regs *p_cfg2, SDL_VTM_InstTs instance, const SDL_VTM_Ctrlcfg *p_tsCtrl_cfg) |
VTM Temperature Sensor Control. More... | |
int32_t | SDL_VTM_tsGetCtrl (const SDL_VTM_cfg2Regs *p_cfg2, SDL_VTM_InstTs instance, SDL_VTM_Ctrlcfg *p_tsCtrl_cfg) |
Read VTM Temperature Sensor Control. More... | |
int32_t | SDL_VTM_tsSetThresholds (const SDL_VTM_cfg1Regs *p_cfg1, SDL_VTM_InstTs instance, const SDL_VTM_tsThrVal *p_thr_val) |
VTM Temperature sensor set, clear threshold values and enable, disable threshold events. More... | |
int32_t | SDL_VTM_tsGetThresholds (const SDL_VTM_cfg1Regs *p_cfg1, SDL_VTM_InstTs instance, SDL_VTM_tsThrVal *p_thr_val) |
VTM Temperature Sensor get threshold values and threshold enable/disable status. More... | |
int32_t | SDL_VTM_tsConvADCToTemp (SDL_VTM_adc_code adc_code, SDL_VTM_InstTs instance, int32_t *p_milli_degree_temp_val) |
VTM Temperature ADC code to Temperature conversion. More... | |
int32_t | SDL_VTM_tsConvTempToAdc (int32_t milli_degree_temp_val, SDL_VTM_InstTs instance, SDL_VTM_adc_code *p_adc_code) |
VTM Temperature to ADC code conversion. More... | |
int32_t | SDL_VTM_tsSetMaxTOutRgAlertThr (const SDL_VTM_cfg2Regs *p_cfg2, SDL_VTM_InstTs instance, int32_t high_temp_in_milli_degree_celcius, int32_t low_temp_in_milli_degree_celcius) |
VTM Temperature Sensor Maximum Temperature Out of Range Alert threshold. More... | |