40 #ifndef SDL_IP_MTOG_H_ 41 #define SDL_IP_MTOG_H_ 49 #include "sdlr_mtog.h" 85 #define SDL_MTOG_VAL_1K ((uint32_t) 0U) 87 #define SDL_MTOG_VAL_4K ((uint32_t) 1U) 89 #define SDL_MTOG_VAL_16K ((uint32_t) 2U) 91 #define SDL_MTOG_VAL_64K ((uint32_t) 3U) 93 #define SDL_MTOG_VAL_256K ((uint32_t) 4U) 95 #define SDL_MTOG_VAL_1M ((uint32_t) 5U) 97 #define SDL_MTOG_VAL_2M ((uint32_t) 6U) 99 #define SDL_MTOG_VAL_4M_MINUS_1 ((uint32_t) 7U) uint32_t SDL_MTOGVal
Definition: sdl_ip_mtog.h:83
int32_t SDL_MTOG_setTimeoutVal(SDL_MTOG_Regs *pRegs, SDL_MTOGVal timeOut)
Set the timeout value.