![]() |
SDL API Guide for J721S2
|
Timeout values | |
This enumerator defines the possible timeout values | |
typedef uint32_t | SDL_MTOGVal |
#define | SDL_MTOG_VAL_1K ((uint32_t) 0U) |
#define | SDL_MTOG_VAL_4K ((uint32_t) 1U) |
#define | SDL_MTOG_VAL_16K ((uint32_t) 2U) |
#define | SDL_MTOG_VAL_64K ((uint32_t) 3U) |
#define | SDL_MTOG_VAL_256K ((uint32_t) 4U) |
#define | SDL_MTOG_VAL_1M ((uint32_t) 5U) |
#define | SDL_MTOG_VAL_2M ((uint32_t) 6U) |
#define | SDL_MTOG_VAL_4M_MINUS_1 ((uint32_t) 7U) |
#define SDL_MTOG_VAL_1K ((uint32_t) 0U) |
1024 clock cycles
#define SDL_MTOG_VAL_4K ((uint32_t) 1U) |
4096 clock cycles
#define SDL_MTOG_VAL_16K ((uint32_t) 2U) |
16,384 clock cycles
#define SDL_MTOG_VAL_64K ((uint32_t) 3U) |
65,536 clock cycles
#define SDL_MTOG_VAL_256K ((uint32_t) 4U) |
262,144 clock cycles
#define SDL_MTOG_VAL_1M ((uint32_t) 5U) |
1,048,576 clock cycles
#define SDL_MTOG_VAL_2M ((uint32_t) 6U) |
2,097,152 clock cycles
#define SDL_MTOG_VAL_4M_MINUS_1 ((uint32_t) 7U) |
4,194,303 clock cycles
typedef uint32_t SDL_MTOGVal |