![]() |
SDL API Guide for J721S2
|
===========================================================================
Functions | |
int32_t | SDL_MTOG_setTimeoutVal (SDL_MTOG_Regs *pRegs, SDL_MTOGVal timeOut) |
Set the timeout value. More... | |
int32_t SDL_MTOG_setTimeoutVal | ( | SDL_MTOG_Regs * | pRegs, |
SDL_MTOGVal | timeOut | ||
) |
Set the timeout value.
This function sets the desired timeout value. This function should only be called when the timeout is disabled.
pRegs | [IN] Pointer to the desired VBUSM Master Timeout Gasket Control register |
timeOut | [IN] Timeout count value. See SDL_MTOGVal for a list of valid timeout values. |