![]() |
SDL API Guide for J721S2
|
Functions | |
void | SDL_ROM_Checksum_init (SDL_ROM_Checksum_obj *const md) |
This API will Initialize the buffer where hash value to be stored. More... | |
int32_t | SDL_ROM_Checksum_process (SDL_ROM_Checksum_obj *md, uint8_t *in, uint32_t inlen) |
This API is used to process the ROM region data. More... | |
void | SDL_ROM_Checksum_compress (SDL_ROM_Checksum_obj *md, uint8_t *buf) |
This API is used to compress the data of ROM region and store the result in md->state. More... | |
int32_t | SDL_ROM_Checksum_done (SDL_ROM_Checksum_obj *md) |
This API will increase our data length with the help of padding ( because our algorithm can compress only 1024-bit length of data at a time) and will compress then will store final has value in md->state. More... | |
int32_t | SDL_ROM_Checksum_compareResult (uint64_t buflen, SDL_ROM_Checksum_obj *md, uint64_t *golden_value) |
This API will compare the resultant hash value of golden value. More... | |
void | SDL_memcpy (void *dest, void *src, uint32_t n) |
This API will copy source pointer data to destination pointer. More... | |
void SDL_ROM_Checksum_init | ( | SDL_ROM_Checksum_obj *const | md | ) |
This API will Initialize the buffer where hash value to be stored.
int32_t SDL_ROM_Checksum_process | ( | SDL_ROM_Checksum_obj * | md, |
uint8_t * | in, | ||
uint32_t | inlen | ||
) |
This API is used to process the ROM region data.
void SDL_ROM_Checksum_compress | ( | SDL_ROM_Checksum_obj * | md, |
uint8_t * | buf | ||
) |
This API is used to compress the data of ROM region and store the result in md->state.
int32_t SDL_ROM_Checksum_done | ( | SDL_ROM_Checksum_obj * | md | ) |
This API will increase our data length with the help of padding ( because our algorithm can compress only 1024-bit length of data at a time) and will compress then will store final has value in md->state.
int32_t SDL_ROM_Checksum_compareResult | ( | uint64_t | buflen, |
SDL_ROM_Checksum_obj * | md, | ||
uint64_t * | golden_value | ||
) |
This API will compare the resultant hash value of golden value.
void SDL_memcpy | ( | void * | dest, |
void * | src, | ||
uint32_t | n | ||
) |
This API will copy source pointer data to destination pointer.