![]() |
SDL API Guide for J721S2
|
This structure is used to store the resultant value of ROM Checksum.
Data Fields | |
uint64_t | length |
uint64_t | state [8] |
uint32_t | curlen |
uint8_t | buf [128] |
uint64_t SDL_ROM_Checksum_obj::length |
Actual data length
uint64_t SDL_ROM_Checksum_obj::state[8] |
Random seek value
uint32_t SDL_ROM_Checksum_obj::curlen |
Used to keep track of data length in incomplete block
uint8_t SDL_ROM_Checksum_obj::buf[128] |
Memory storage use in padding