![]() |
SDL API Guide for J721S2
|
===========================================================================
Functions | |
int32_t | SDL_ESM_getNErrorStatus (SDL_ESM_Inst instance, uint32_t *pStatus) |
SDL ESM API to get the status of the nError pin for the specified ESM instance. More... | |
int32_t | SDL_ESM_getStaticRegisters (SDL_ESM_Inst instance, SDL_ESM_staticRegs *pStaticRegs) |
SDL ESM API to read the static registers. The API reads and returns the static register configuration for the ESM module for the specified instance. This API can be used by the application to read back the static configuration. Comparision of the static configuration registers against expected values is the responsibility of the application. More... | |
int32_t | SDL_ESM_verifyConfig (SDL_ESM_Inst instance, const SDL_ESM_config *pConfig) |
SDL ESM API to verify the written configuration of the ESM module. The API verifies the written config that was done during SDL_ESM_init against the provided configuration. More... | |
int32_t | SDL_ESM_clrNError (SDL_ESM_Inst instance) |
SDL ESM API to clear the nError pin for the specified ESM instance. More... | |
int32_t | SDL_ESM_setNError (SDL_ESM_Inst instance) |
SDL ESM API to set the nError pin for the specified ESM instance. More... | |
int32_t | SDL_ESM_registerECCCallback (SDL_ESM_Inst instance, uint32_t eventBitMap[], SDL_ESM_applicationCallback eccCallback, void *callbackArg) |
There are modules within SDL which will generate ESM errors intentionally in the course of running self-tests. The ECC module is one such module. To allow these modules to get the notification when the ESM error occurs, callback registration APIs are provided. The following APIs allow registration of a callback for specific events. This API is used by other SDL modules and not by the application. More... | |
int32_t | SDL_ESM_registerCCMCallback (SDL_ESM_Inst instance, uint32_t eventBitMap[], SDL_ESM_applicationCallback ccmCallback, void *callbackArg) |
There are modules within SDL which will generate ESM errors intentionally in the course of running self-tests. The CCM module is one such module. To allow these modules to get the notification when the ESM error occurs, callback registration APIs are provided. The following APIs allow registration of a callback for specific events. This API is used by other SDL modules and not by the application. More... | |
int32_t | SDL_ESM_init (SDL_ESM_Inst instance, const SDL_ESM_config *pConfig, SDL_ESM_applicationCallback applicationCallback, void *appArg) |
SDL ESM API to initialize an ESM instance. The API initializes the specified ESM instance with the provided configuration. The configuration will allow the application to specify for each event whether the interrupt is enabled or disabled, the priority of the event, and whether the nErrorPin assertion is enabled or disabled for the event. More... | |
int32_t SDL_ESM_getNErrorStatus | ( | SDL_ESM_Inst | instance, |
uint32_t * | pStatus | ||
) |
SDL ESM API to get the status of the nError pin for the specified ESM instance.
============================================================================
instance | ESM Instance |
pStatus | Pointer to variable to store the status. If status is 1, then error pin is not active. If status is 0, then error pin is active. |
int32_t SDL_ESM_getStaticRegisters | ( | SDL_ESM_Inst | instance, |
SDL_ESM_staticRegs * | pStaticRegs | ||
) |
SDL ESM API to read the static registers. The API reads and returns the static register configuration for the ESM module for the specified instance. This API can be used by the application to read back the static configuration. Comparision of the static configuration registers against expected values is the responsibility of the application.
============================================================================
instance | ESM Instance |
pStaticRegs | Pointer to the static config register structure |
int32_t SDL_ESM_verifyConfig | ( | SDL_ESM_Inst | instance, |
const SDL_ESM_config * | pConfig | ||
) |
SDL ESM API to verify the written configuration of the ESM module. The API verifies the written config that was done during SDL_ESM_init against the provided configuration.
============================================================================
instance | ESM Instance |
pConfig | Pointer to the ESM configuration to be used for verification. |
int32_t SDL_ESM_clrNError | ( | SDL_ESM_Inst | instance | ) |
SDL ESM API to clear the nError pin for the specified ESM instance.
============================================================================
instance | ESM Instance |
int32_t SDL_ESM_setNError | ( | SDL_ESM_Inst | instance | ) |
SDL ESM API to set the nError pin for the specified ESM instance.
============================================================================
instance | ESM Instance |
int32_t SDL_ESM_registerECCCallback | ( | SDL_ESM_Inst | instance, |
uint32_t | eventBitMap[], | ||
SDL_ESM_applicationCallback | eccCallback, | ||
void * | callbackArg | ||
) |
There are modules within SDL which will generate ESM errors intentionally in the course of running self-tests. The ECC module is one such module. To allow these modules to get the notification when the ESM error occurs, callback registration APIs are provided. The following APIs allow registration of a callback for specific events. This API is used by other SDL modules and not by the application.
============================================================================
instance | ESM Instance |
eventBitMap | Bitmap for ESM error event of interest for this callback. Array of uint32_t type with each bit representing one ESM error event. |
eccCallback | Pointer to the callback to be called by the ESM Handler to notify the ECC module of an ESM error event |
callbackArg | Argument that will be passed along with the callback. |
int32_t SDL_ESM_registerCCMCallback | ( | SDL_ESM_Inst | instance, |
uint32_t | eventBitMap[], | ||
SDL_ESM_applicationCallback | ccmCallback, | ||
void * | callbackArg | ||
) |
There are modules within SDL which will generate ESM errors intentionally in the course of running self-tests. The CCM module is one such module. To allow these modules to get the notification when the ESM error occurs, callback registration APIs are provided. The following APIs allow registration of a callback for specific events. This API is used by other SDL modules and not by the application.
============================================================================
instance | ESM Instance |
eventBitMap | Bitmap for ESM error event of interest for this callback. Array of uint32_t type with each bit representing one ESM error event. |
ccmCallback | Pointer to the callback to be called by the ESM Handler to notify the CCM module of an ESM error event |
callbackArg | Argument that will be passed along with the callback. |
int32_t SDL_ESM_init | ( | SDL_ESM_Inst | instance, |
const SDL_ESM_config * | pConfig, | ||
SDL_ESM_applicationCallback | applicationCallback, | ||
void * | appArg | ||
) |
SDL ESM API to initialize an ESM instance. The API initializes the specified ESM instance with the provided configuration. The configuration will allow the application to specify for each event whether the interrupt is enabled or disabled, the priority of the event, and whether the nErrorPin assertion is enabled or disabled for the event.
============================================================================
instance | ESM Instance |
pConfig | Pointer to the ESM configuration structure |
applicationCallback | Pointer to the callback to be called by the ESM Handler to notify the application of an ESM error event. |
appArg | Application argument that will passed to the application when the application callback is called. |