MCUSW
Cdd_IpcRegRbValues Struct Reference

Data Fields

uint32 numRegisters
 
uint32 regValues [CDD_IPC_CORE_ID_MAX]
 
uint32 cddipcRev
 
uint32 cddipcsyscfg
 
uint32 cddipceoi
 
uint32 cddipcmsg
 
uint32 cddipcfifosts
 
uint32 cddipcmsgsts
 
uint32 cddipcirqrawsts
 
uint32 cddipcclrsts
 
uint32 cddipcenbclr
 
uint32 cddipcenbset
 
uint32 reserved
 

Field Documentation

◆ numRegisters

uint32 Cdd_IpcRegRbValues::numRegisters

Will specify number of registers values provided

◆ regValues

uint32 Cdd_IpcRegRbValues::regValues[CDD_IPC_CORE_ID_MAX]

Values of critical registers that's read and provided

◆ cddipcRev

uint32 Cdd_IpcRegRbValues::cddipcRev

MAILBOX_REVISION Register

◆ cddipcsyscfg

uint32 Cdd_IpcRegRbValues::cddipcsyscfg

MAILBOX_SYSCONFIG Register

◆ cddipceoi

uint32 Cdd_IpcRegRbValues::cddipceoi

MAILBOX_EOI Register

◆ cddipcmsg

uint32 Cdd_IpcRegRbValues::cddipcmsg

MAILBOX_MESSAGE_y Register

◆ cddipcfifosts

uint32 Cdd_IpcRegRbValues::cddipcfifosts

MAILBOX_FIFO_STATUS_y Register

◆ cddipcmsgsts

uint32 Cdd_IpcRegRbValues::cddipcmsgsts

MAILBOX_MSG_STATUS_y Register

◆ cddipcirqrawsts

uint32 Cdd_IpcRegRbValues::cddipcirqrawsts

MAILBOX_IRQ_STATUS_RAW_i Register

◆ cddipcclrsts

uint32 Cdd_IpcRegRbValues::cddipcclrsts

MAILBOX_CLR_STATUS_i Register

◆ cddipcenbclr

uint32 Cdd_IpcRegRbValues::cddipcenbclr

MAILBOX_ENABLE_CLR_i Register

◆ cddipcenbset

uint32 Cdd_IpcRegRbValues::cddipcenbset

MAILBOX_ENABLE_SET_i Register

◆ reserved

uint32 Cdd_IpcRegRbValues::reserved

Reserved field