![]() |
MCUSW
|
Defines processor identifiers Core on which MCAL/AUTOSAR is hosted and other cores with which IPC is desired.
Data Fields | |
uint32 | ownProcID |
uint32 | numProcs |
uint32 | remoteProcID [CDD_IPC_CORE_ID_MAX] |
uint32 | reserved |
uint32 Cdd_IpcMpType::ownProcID |
Defines processor ID on which MCAL/AUTOSAR is being hosted
uint32 Cdd_IpcMpType::numProcs |
Number of remote processor which with IPC is desired
uint32 Cdd_IpcMpType::remoteProcID[CDD_IPC_CORE_ID_MAX] |
Remote processor identifiers
uint32 Cdd_IpcMpType::reserved |
Future use if any