![]() |
MCUSW
|
This document describes the functionality, API and configuration of the AUTOSAR BSW module ICU.
The figure below depicts the AUTOSAR layered architecture as 3 distinct layers,
The BSW is further divided into 4 layers:
MCAL is the lowest abstraction layer of the Basic Software. It contains internal drivers that are software modules that interact with the Microcontroller and its internal peripherals directly. ICU driver will use ECAP (Enhanced Capture) hardware IP for demodulation of a PWM signal, counting pulses, measuring of frequency and duty cycle and generating simple interrupts.
The Icu driver uses ECAP module to capture events. There are three ECAP instances available to work with (ECAP0 - ECAP2) on J721E and J7200. The Icu driver provides the following features:
The hardware ECAP module includes the following features:
Please note that this is just for reference purpose, for other details please refer to technical reference manual. Note that not all feature available in ECAP hardware IP are currently supported by ICU driver.
Diagrams are from device TRM.
Icu
Sl No | Specification | Comment / Link |
---|---|---|
1 | AUTOSAR 4.3.1 | AUTOSAR Specification for Icu Driver Internet Link |
2 | TDA4x TRM | Technical Reference Manual, TDA4X |
3 | BSW General Requirements / Coding guidelines | Intranet Link |
4 | Software Product Specification (SPS) | Intranet Link Requirements are derived from 1 |
The Icu Driver implements a standardized interface specified in the AUTOSAR_SWS_ICUDriver document, specified in: 4, 1 and 3. It’s recommended to refer 1 for clarification.
Hardware does not support wakeup capability. Hence, the below features are not supported. - Controlling Wakeup interrupts. - Icu_SetMode() - Icu_DisableWakeup() - Icu_EnableWakeup() - Icu_CheckWakeup()
Below listed points are assumed to be valid for this design/implementation, exceptions and other deviations are listed for each explicitly. Care should be taken to ensure these assumptions are addressed.
The Icu driver follows the code sequence outlined by the Autosar Spec for Icu Module. Please refer to 1 for more details.
There are no hard requirements for resource allocation for Icu driver. Average Stack Size of ICU Driver is around 2 kilo bytes.
An interrupt can be generated on capture events 1 through 4. In ICU driver module, interrupt will be generated for every single capture event - so all 4 capture events are triggered for edge counting, edge detection, timestamp calculation and signal measurements.
When a capture event occurs and capture register reads value, an interrupt flag will be raised for that event. The ISR in ICU module will recognize the the capture event and perform required steps based on the measurement mode (Please refer to 1) selected in configurator. For example, if Timestamp measurement mode is selected, the timestamp specific ISR will be called, required values will be stored in module, and interrupts will be cleared from there.
Refer 1 specifically section 7.1.3 of the specification for more details
All time units used within the API services of the ICU module shall be of the unit ticks.
The ICU Module can have two states: IC_STATUS_UINIT (before the module had been initialized with Icu_Init) and ICU_STATUS_INIT (after module has been initialized).
The ICU State (logical input state of ICU Channel) can be ICU_ACTIVE or ICU_IDLE. ICU_ACTIVE - Input state of an ICU Channel, and activation edge has been detected. ICU_IDLE - Input state of an ICU Channel, no activation edge had been detected since last call of Icu_GetInputState() or Icu_Init().
Design ID | DES_ICU_001 |
Requirements Covered | MCAL-4591 |
The diagram below shows the overall files structure for the Icu driver.
Icu Directory Structure
Driver Implemented by
Example Application
Design ID | DES_ICU_002 |
Requirements Covered | MCAL-4569, MCAL-4570, MCAL-4571, MCAL-4572, MCAL-4573, MCAL-4574, MCAL-4575, MCAL-4576, MCAL-4577, MCAL-4578, MCAL-4579 |
The AUTOSAR Icu Driver Specification details mandatory parameters that shall be configurable via the configurator. Please refer section 10 1 Error Checks are common for variants of devices and we can do this in xdm or generator code.
Design ID | DES_ICU_003 |
Requirements Covered | MCAL-4534, MCAL-4535, MCAL-4536, MCAL-4538, MCAL-4539, MCAL-4541, MCAL-4542, MCAL-4544, MCAL-4545, MCAL-4546, MCAL-4547, MCAL-4549, MCAL-4550, MCAL-4552, MCAL-4553, MCAL-4554, MCAL-4555, MCAL-4557, MCAL-4558, MCAL-4559, MCAL-4560, MCAL-4561, MCAL-4562, MCAL-4563, MCAL-4566, MCAL-4567 |
The design's specific configurable parameters are as follows:
Parameter | Usage comment |
---|---|
IcuFunctionalClock | This is the value of the System Clock freq |
IcuDeviceVariant | This shall allow integrators to select the device variant for which integration is being performed. This parameter shall be used by driver to impose device specific constraints. The user guide shall detail the device specific constraints |
IcuClkPrescaler | This parameter allows the selection of pre-scalar value.The prescaler stage is clocked with the ICU clock and acts as a clock divider for the time-base clock. |
Design ID | DES_ICU_004 |
Requirements Covered | MCAL-5168, MCAL-5169, MCAL-5170 |
The driver shall support both VARIANT-PRE-COMPILE & VARIANT-POST-BUILD.
There are two types of errors in Icu module - Developement Erros and RunTime Errors.
AUTOSAR requires that API functions check the validity of their parameters and module status. The checks in table are internal parameter checks of the API functions. These checks are for development error reporting and can be enabled or disabled.
Design ID | DES_ICU_005 |
Requirements Covered | MCAL-4585, MCAL-4586 |
Development Error Reporting
The detection of development errors is configurable (ON / OFF) at pre-compile time. The switch ICU_DEV_ERROR_DETECT will activate or deactivate the detection of all development errors.
By default, development errors are reported to the DET using the service Det_ReportError(), if development error detection and reporting are enabled (i.e. checkboxes Development Mode and Development Error Reporting are checked).
Type of Error | Related Error code | Value (Hex) |
API is called with invalid pointer | ICU_E_PARAM_POINTER | 0x0A |
API service used with an invalid channel identifier or channel was not configured for the functionality of the called API | ICU_E_PARAM_CHANNEL | 0x0B |
API service used with an invalid or not feasible activation | ICU_E_PARAM_ACTIVATION | 0x0C |
Init Function Failed | ICU_E_INIT_FAILED | 0x0D |
API service used with an invalid bugger size | ICU_E_PARAM_BUFFER_SIZE | 0x0E |
API serice Icu_SetMode used with an invalid mode | ICU_E_PARAM_MODE | 0x0F |
API service used without module initialization | ICU_E_UNINIT | 0x14 |
API serice Icu_SetMode is called while in running operation | ICU_E_BUSY_OPERATION | 0x16 |
API Icu_Init ervice is called and when the ICU driver and the Hardware are already Initialized | ICU_E_ALREADY_INITIALIZED | 0x17 |
API Icu_StartTimeStamp is called and the parameter NotifyInterval is Invalid | ICU_E_PARAM_NOTIFY_INTERVAL | 0x18 |
API Icu_GetVersionInfo is called and the parameter versioninfo is invalid | ICU_E_PARAM_VINFO | 0x19 |
Runtime Errors
Type of Error | Related Error code | Value (Hex) |
API service Icu_StopTimestamp called on a channel which was not started or already stopped | ICU_E_NOT_STARTED | 0x15 |
Icu driver makes driver status available for debugging. The input channel status can be probed using the Icu_GetInputState() API.
The detailed API and interface description is available as part of 1 & 4. This section describes the API supported by the MCAL driver and the requirements covered by each of the API.
The sections below lists some of key data structures that shall be implemented and used in driver implementation.
Type | Identifier | Comments |
---|---|---|
uint32 | ICU_MAX_NUM_CHANNELS | Defines the maximum number of instances available in ICU module. This is specific to SoC being used (3 for J721E and J7200). |
Used to allow enabling/disabling of all interrupts which are not required for the ECU wakeup. This will only be set to ICU_MODE_NORMAL as wakeup capability is not supported by hardware. Please refer section 8.2.1 of 1.
Numeric identifier of an ICU Channel. Please refer section 8.2.2 of 1.
Input state of an ICU channel. Please refer section 8.2.3 of 1.
This type contains initialization data. Please refer section 8.2.4 of 1.
Definition of the type of activation of an ICU channel. Please refer section 8.2.5 of 1.
Width of the buffer for timestamp ticks and measured elapsed timeticks. This will be 32-bit to match the hardware timer. Please refer section 8.2.6 of 1.
Type which shall contain the values, needed for calculating duty cycle. Please refer section 8.2.7 of 1.
Icu Index time to abstract the reutn value of service Icu_GetTimestampIndex() Please refer section 8.2.8 of 1.
Type to abstract the return value of the service Icu_GetEdgeNumbers(). Please refer section 8.2.9 of 1.
Definition of the measurement mode type. Please refer section 8.2.10 of 1.
Definition of the measurement property type. Please refer section 8.2.11 of 1.
Definition of the timestamp measurement property type. Please refer section 8.2.12 of 1.
For the standard APIs please refer 8.3 of 1. Sections below highlight other design considerations for the implementation.
Refer section 8.3.1 of 1
Design ID | DES_ICU_006 |
Requirements Covered | MCAL-4610, MCAL-4611, MCAL-4612, MCAL-4613, MCAL-4614, MCAL-4616, MCAL-4617, MCAL-4618, MCAL-4619, MCAL-4620 |
Refer section 8.3.2 of 1
Design ID | DES_ICU_007 |
Requirements Covered | MCAL-4621, MCAL-4622, MCAL-4623, MCAL-4624, MCAL-4625, MCAL-4626, MCAL-4627, MCAL-4628, MCAL-4629, MCAL-4630 |
Refer 8.3.7 of 1
Design ID | DES_ICU_008 |
Requirements Covered | MCAL-4659, MCAL-4660, MCAL-4661, MCAL-4662, MCAL-4663, MCAL-4664 |
Refer section 8.3.8 of 1
Design ID | DES_ICU_009 |
Requirements Covered | MCAL-4665, MCAL-4666, MCAL-4667, MCAL-4668 |
Refer section 8.3.9 of 1
Design ID | DES_ICU_010 |
Requirements Covered | MCAL-4669, MCAL-4670, MCAL-4671, MCAL-4672 |
Refer section 8.3.10 of 1
Design ID | DES_ICU_011 |
Requirements Covered | MCAL-4673, MCAL-4674, MCAL-4675, MCAL-4676, MCAL-4677, MCAL-4678, MCAL-4679, MCAL-4680, MCAL-4681, MCAL-4682, MCAL-4683 |
Refer section 8.3.11 of 1
Design ID | DES_ICU_012 |
Requirements Covered | MCAL-4684, MCAL-4685, MCAL-4686, MCAL-4687, MCAL-4688, MCAL-4689, MCAL-4690, MCAL-4691, MCAL-4692, MCAL-4693, MCAL-4694, MCAL-4695, MCAL-4696, MCAL-4697, MCAL-4198, MCAL-4199 |
Refer section 8.3.12 of 1
Design ID | DES_ICU_013 |
Requirements Covered | MCAL-4700, MCAL-4701, MCAL-4702, MCAL-4703, MCAL-4704, MCAL-4705, MCAL-4706, MCAL-4707 |
Refer section 8.3.13 of 1
Design ID | DES_ICU_014 |
Requirements Covered | MCAL-4708, MCAL-4709, MCAL-4710, MCAL-4710, MCAL-4711, MCAL-4712, MCAL-4713, MCAL-47104, MCAL-4715, MCAL-4716 |
Refer section 8.3.14 of 1
Design ID | DES_ICU_015 |
Requirements Covered | MCAL-4717, MCAL-4719, MCAL-4720, MCAL-4718, MCAL-4721, MCAL-4722 |
Refer section 8.3.15 of 1
Design ID | DES_ICU_016 |
Requirements Covered | MCAL-4723, MCAL-4724, MCAL-4725, MCAL-4726, MCAL-4727, MCAL-4728, MCAL-4729, MCAL-4730 |
Refer section 8.3.16 of 1
Design ID | DES_ICU_017 |
Requirements Covered | MCAL-4731, MCAL-4732, MCAL-4733, MCAL-4734, MCAL-4735, MCAL-4736, MCAL-4737, MCAL-4738 |
Refer section 8.3.17 of 1
Design ID | DES_ICU_018 |
Requirements Covered | MCAL-4739, MCAL-4740, MCAL-4741, MCAL-4742, MCAL-4743, MCAL-4744 |
Refer section 8.3.18 of 1
Design ID | DES_ICU_019 |
Requirements Covered | MCAL-4745, MCAL-4746, MCAL-4747, MCAL-4748, MCAL-4749, MCAL-4750 |
Refer section 8.3.19 of 1
Design ID | DES_ICU_020 |
Requirements Covered | MCAL-4751, MCAL-4752, MCAL-4753, MCAL-4754, MCAL-4755, MCAL-4756, MCAL-4757 |
Refer section 8.3.20 of 1
Design ID | DES_ICU_021 |
Requirements Covered | MCAL-4758, MCAL-4759, MCAL-4760, MCAL-4761, MCAL-4762, MCAL-4763, MCAL-4764, MCAL-4765 |
Refer section 8.3.21 of 1
Design ID | DES_ICU_022 |
Requirements Covered | MCAL-4766, MCAL-4767, MCAL-4768, MCAL-4769, MCAL-4770, MCAL-4771, MCAL-4772 |
Refer section 8.3.22 of 1
Design ID | DES_ICU_023 |
Requirements Covered | MCAL-4773, MCAL-4774, MCAL-4775, MCAL-4776, MCAL-4777, MCAL-4778, MCAL-4779, MCAL-4780, MCAL-4781, MCAL-4782, MCAL-4783, MCAL-4784 |
Refer section 8.3.23 of 1
Design ID | DES_ICU_024 |
Requirements Covered | MCAL-4785, MCAL-4786, MCAL-4787, MCAL-4788, MCAL-4789, MCAL-4790, MCAL-4791, MCAL-4792, MCAL-4793, MCAL-4794 |
Refer section 8.3.24 of 1
Design ID | DES_ICU_025 |
Requirements Covered | MCAL-4795, MCAL-4796 |
This design expects that implementation will require to use following global variables.
Variable | Type | Description | Default Value |
---|---|---|---|
Icu_DrvObj | Icu_DriverObjType | Icu driver object | - |
Icu_DrvStatus | uint8 | Driver Status | ICU_STATUS_UNINIT |
Sections below list some of the important design decisions and rational behind those decision.
Signal Measurements API could be implemented using either interrupt based or non-interrupt based functionality.
The most efficient(least time delay) method shall be chosen. Also, the method which complies best with AUTOSAR specification will be analyzed.
Option 2 is selected as it gives best runtime performance. Most importantly, it complies best with AUTOSAR specified functionality.
ECAP module has the ability to generate interrupts at each or only at a particular capture event. There can be total of 4 capture event interrupts (one for each capture register, CAP1 - CAP4).
The design the best complies with AUTOSAR specification shall be chosen.
Option 2 is chosen as it will ensure that there are no deviation from AUTOSAR specification.
The sections below identify some of the aspects of design that would require emphasis during testing of this design implementation
The sections below identify some of the aspects of design that would require emphasis during testing of this design implementation
Revision | Date | Author | Description | Status |
---|---|---|---|---|
0.1 | 19 Jan 2021 | Nikki Shah | First version | Pending |
0.2 | 24 Feb 2021 | Nikki Shah | Review Comments Addressed | Approved |