MCUSW
|
This file contains generated pre compile configuration file for ICU MCAL driver.
Go to the source code of this file.
Macros | |
#define | ICU_PRE_COMPILE_VARIANT (STD_ON ) |
ICU Build Variant. Build variants.(i.e Pre-compile,Post-build or Link time) More... | |
#define | ICU_SAFETY_DIAGNOSTIC_API (STD_ON) |
Enable/Disable Icu Safety Diagnostic. More... | |
#define | ICU_DE_INIT_API (STD_ON) |
Enable/Disable Icu DeInit API. More... | |
#define | ICU_EDGE_COUNT_API (STD_ON) |
Enable/Disable Edge Count API. More... | |
#define | ICU_EDGE_DETECT_API (STD_ON) |
Enable/Disable Edge Detect API. More... | |
#define | ICU_GET_DUTY_CYCLE_VALUES_API (STD_ON) |
Enable/Disable Get Duty Cycle Values API. More... | |
#define | ICU_GET_INPUT_STATE_API (STD_ON) |
Enable/Disable Get Input State API. More... | |
#define | ICU_GET_TIME_ELAPSED_API (STD_ON) |
Enable/Disable Get Time Elapsed API. More... | |
#define | ICU_GET_VERSION_INFO_API (STD_ON) |
Enable/Disable Get Version Info API. More... | |
#define | ICU_SIGNAL_MEASUREMENT_API (STD_ON) |
Enable/Disable Signal Measurement API. More... | |
#define | ICU_TIMESTAMP_API (STD_ON) |
Enable/Disable Timestamp API. More... | |
#define | ICU_DEV_ERROR_DETECT (STD_ON) |
Enable/Disable Development error detet. More... | |
#define | IcuConf_IcuChannelConfiguration_IcuChannel_0 (1U) |
Channel ID Symbolic Names Configured channel ID(s) More... | |
#define | ICU_INIT_CONFIG_PC IcuConfigSet |
Pre Compile config macro name. More... | |
#define | ICU_ISR_TYPE (ICU_ISR_CAT1) |
ISR type. More... | |
#define | ICU_MAX_NUM_CHANNELS (3U) |
#define | ICU_CHANNEL1 (1U) |
ECAP Channel 1, in MAIN DOMAIN. More... | |
Functions | |
void | Icu_ch1Notify (void) |
ICU ISR. More... | |
Variables | |
const uint32 | Icu_HwUnitBaseAddr [ICU_MAX_NUM_CHANNELS] |
const struct Icu_ConfigType_PC_s | IcuConfigSet_PC |
ICU Configuration structure declaration. More... | |
const struct Icu_ConfigType_s | IcuConfigSet |