101 #define ICU_PRE_COMPILE_VARIANT (STD_ON ) 105 #define ICU_SAFETY_DIAGNOSTIC_API (STD_ON) 108 #define ICU_DE_INIT_API (STD_ON) 111 #define ICU_EDGE_COUNT_API (STD_ON) 114 #define ICU_EDGE_DETECT_API (STD_ON) 117 #define ICU_GET_DUTY_CYCLE_VALUES_API (STD_ON) 120 #define ICU_GET_INPUT_STATE_API (STD_ON) 123 #define ICU_GET_TIME_ELAPSED_API (STD_ON) 126 #define ICU_GET_VERSION_INFO_API (STD_ON) 129 #define ICU_SIGNAL_MEASUREMENT_API (STD_ON) 132 #define ICU_TIMESTAMP_API (STD_ON) 135 #define ICU_DEV_ERROR_DETECT (STD_ON) 140 #define IcuConf_IcuChannelConfiguration_IcuChannel_0 (1U) 146 #define ICU_INIT_CONFIG_PC IcuConfigSet 149 #define ICU_ISR_TYPE (ICU_ISR_CAT1) 151 #define ICU_MAX_NUM_CHANNELS (3U) 157 #define ICU_CHANNEL1 (1U) 160 extern CONST(uint32, ICU_CONST)
#define ICU_MAX_NUM_CHANNELS
Definition: Icu_Cfg.h:151
const struct Icu_ConfigType_s IcuConfigSet
const uint32 Icu_HwUnitBaseAddr[ICU_MAX_NUM_CHANNELS]
const struct Icu_ConfigType_PC_s IcuConfigSet_PC
ICU Configuration structure declaration.
void Icu_ch1Notify(void)
ICU ISR.