MCUSW
|
This file contains interface header for Fls MCAL driver.
Go to the source code of this file.
Data Structures | |
struct | Fls_SectorType |
FLS Module Flashable Sectors and pages. More... | |
struct | Fls_ConfigType |
FLS Module Configuration Structure. More... | |
Macros | |
FLS Driver Module SW Version Info | |
Defines for FLS Driver version used for compatibility checks | |
#define | FLS_SW_MAJOR_VERSION (2U) |
Driver Implementation Major Version. More... | |
#define | FLS_SW_MINOR_VERSION (0U) |
Driver Implementation Minor Version. More... | |
#define | FLS_SW_PATCH_VERSION (0U) |
Driver Implementation Patch Version. More... | |
FLS Driver Module AUTOSAR Version Info | |
Defines for FLS Driver AUTOSAR version used for compatibility checks | |
#define | FLS_AR_RELEASE_MAJOR_VERSION (4U) |
AUTOSAR Major version specification implemented by FLS Driver. More... | |
#define | FLS_AR_RELEASE_MINOR_VERSION (3U) |
AUTOSAR Minor version specification implemented by FLS Driver. More... | |
#define | FLS_AR_RELEASE_REVISION_VERSION (1U) |
AUTOSAR Patch version specification implemented by FLS Driver. More... | |
FLS Driver ID Info | |
#define | FLS_VENDOR_ID ((uint16) 44U) |
Texas Instruments Vendor ID. More... | |
#define | FLS_MODULE_ID ((uint16) 92U) |
FLS Driver Module ID. More... | |
#define | FLS_INSTANCE_ID ((uint8) 0U) |
FLS Driver Instance ID. More... | |
FLS Error Codes | |
Error codes returned by FLS functions | |
#define | FLS_E_PARAM_CONFIG ((uint8) 0x01U) |
API service called with wrong parameter. More... | |
#define | FLS_E_PARAM_ADDRESS ((uint8) 0x02U) |
API service called with wrong parameter. More... | |
#define | FLS_E_PARAM_LENGTH ((uint8) 0x03U) |
API service called with wrong parameter. More... | |
#define | FLS_E_PARAM_DATA ((uint8) 0x04U) |
API service called with wrong parameter. More... | |
#define | FLS_E_UNINIT ((uint8) 0x05U) |
API service used without module initiali-zation. More... | |
#define | FLS_E_BUSY ((uint8) 0x06U) |
APIs called when module is busy. More... | |
#define | FLS_E_PARAM_POINTER ((uint8) 0x0AU) |
APIs called with a Null Pointer. More... | |
#define | FLS_E_VERIFY_ERASE_FAILED ((uint8) 0x07U) |
APIs service Erase Verification (BlankCheck) failed. More... | |
#define | FLS_E_VERIFY_WRITE_FAILED ((uint8) 0x08U) |
APIs serice Write Verification (Compare) failed. More... | |
#define | FLS_E_TIMEOUT ((uint8) 0x09U) |
APIs Timeout Exceeded. More... | |
#define | FLS_E_ERASE_FAILED ((uint8) 0x01U) |
Flash Erase Failed in HW. More... | |
#define | FLS_E_WRITE_FAILED ((uint8) 0x02U) |
Flash Write Failed in HW. More... | |
#define | FLS_E_READ_FAILED ((uint8) 0x03U) |
Flash Read Failed in HW. More... | |
#define | FLS_E_COMPARE_FAILED ((uint8) 0x04U) |
Flash Compare Failediin HW. More... | |
#define | FLS_E_UNEXPECTED_FLASH_ID ((uint8) 0x05U) |
Expected HW ID not matched. More... | |
FLS Service Ids | |
The Service Id is one of the argument to Det_ReportError function and is used to identify the source of the error | |
#define | FLS_SID_INIT ((uint8) 0x00U) |
FLS_Init() API Service ID. More... | |
#define | FLS_SID_ERASE ((uint8) 0x01U) |
FLS_Erase() API Service ID. More... | |
#define | FLS_SID_WRITE ((uint8) 0x02U) |
FLS_Write() API Service ID. More... | |
#define | FLS_SID_CANCEL ((uint8) 0x03U) |
FLS_Cancel() API Service ID. More... | |
#define | FLS_SID_GET_STATUS ((uint8) 0x04U) |
FLS_GetStatus() API Service ID. More... | |
#define | FLS_SID_GET_JOB_RESULT ((uint8) 0x05U) |
Fls_GetJobResult() API Service ID. More... | |
#define | FLS_SID_READ ((uint8) 0x07U) |
FLS_Read() API Service ID. More... | |
#define | FLS_SID_COMPARE ((uint8) 0x08U) |
FLS_Compare() API Service ID. More... | |
#define | FLS_SID_SET_MODE ((uint8) 0x09U) |
FLS_SetMode() API Service ID. More... | |
#define | FLS_SID_GET_VERSION_INFO ((uint8) 0x10U) |
Fls_GetVersionInfo() API Service ID. More... | |
#define | FLS_SID_BLANK_CHECK ((uint8) 0x0AU) |
FLS_BlankCheck() API Service ID. More... | |
#define | FLS_SID_MAIN_FUNCTION ((uint8) 0x06U) |
FLS_MainFunction() API Service ID. More... | |
Typedefs | |
typedef uint32 | Fls_AddressType |
Type of address type. More... | |
typedef uint32 | Fls_LengthType |
Enumerations | |
enum | OSPI_xferLines { OSPI_XFER_LINES_SINGLE = 0U, OSPI_XFER_LINES_DUAL, OSPI_XFER_LINES_QUAD, OSPI_XFER_LINES_OCTAL } |
Number of lines used for OSPI read/write transaction. More... | |
Functions | |
void | Fls_SwitchMode (boolean dacEnable, boolean xipEnable) |
Switch Mode of the OSPI Driver Parameters (in) : boolean dacEnable - should DAC mode be enaled or disabled Parameters (in) : boolean xipEnable - should XIP mode be enaled or disabled Mode : Supervisor Mode (Privileged Mode) More... | |
void | Fls_Init (const Fls_ConfigType *ConfigPtr) |
Initializes the Flash Driver. More... | |
Std_ReturnType | Fls_Erase (Fls_AddressType TargetAddress, Fls_LengthType Length) |
Erases flash sector(s). More... | |
Std_ReturnType | Fls_Write (Fls_AddressType TargetAddress, const uint8 *SourceAddressPtr, Fls_LengthType Length) |
Writes one or more complete flash pages. More... | |
Std_ReturnType | Fls_Read (Fls_AddressType SourceAddress, uint8 *TargetAddressPtr, Fls_LengthType Length) |
Reads from flash memory.. More... | |
Std_ReturnType | Fls_Compare (Fls_AddressType SourceAddress, const uint8 *TargetAddressPtr, Fls_LengthType Length) |
Compares the contents of an area of flash memory with that of an application data buffer. More... | |
Std_ReturnType | Fls_BlankCheck (Fls_AddressType Address, Fls_LengthType Length) |
The function Fls_BlankCheck shall verify, whether a given memory area has been erased but not (yet) programmed. More... | |
MemIf_StatusType | Fls_GetStatus (void) |
Returns the driver state. More... | |
Std_ReturnType | Fls_GetVersionInfo (Std_VersionInfoType *versioninfo) |
This service returns the version information of this module. More... | |
MemIf_JobResultType | Fls_GetJobResult (void) |
Returns the result of the last job. More... | |
void | Fls_MainFunction (void) |
Performs the processing of jobs. More... | |
void | Fls_Cancel (void) |
Cancels an ongoing job. More... | |