MCUSW
|
FLS Module Configuration Structure.
Data Fields | |
Fls_JobEndNotifyType | Fls_JobEndNotification |
Fls_JobErrorNotifyType | Fls_JobErrorNotification |
uint32 | maxReadNormalMode |
uint32 | maxWriteNormalMode |
Fls_SectorType | sectorList [1] |
boolean | dacEnable |
boolean | xipEnable |
uint64 | ospiClkSpeed |
boolean | dtrEnable |
boolean | phyEnable |
OSPI_xferLines | ospixferlines |
uint32 | flsBaudRateDiv |
uint32 | blockSize |
Fls_JobEndNotifyType Fls_ConfigType::Fls_JobEndNotification |
Mapped to the job end notification routine provided by some upper layer module, typically the Fee module.
Fls_JobErrorNotifyType Fls_ConfigType::Fls_JobErrorNotification |
Mapped to the job error notification routine provided by some upper layer module, typically the Fee module.
uint32 Fls_ConfigType::maxReadNormalMode |
The maximum number of bytes to read or compare in one cycle of the flash driver's job processing function in normal mode.
uint32 Fls_ConfigType::maxWriteNormalMode |
The maximum number of bytes to write in one cycle of the flash driver's job processing function in normal mode.
Fls_SectorType Fls_ConfigType::sectorList[1] |
The maximum number of bytes to write in one cycle of the flash driver's job processing function in normal mode. Using Fls Info Structure instead of this for now.
boolean Fls_ConfigType::dacEnable |
Enable Direct Access Mode of Transfer in OSPI Flash
boolean Fls_ConfigType::xipEnable |
Enable XIP mode in OSPI Flash
uint64 Fls_ConfigType::ospiClkSpeed |
OSPI Clock Speed
boolean Fls_ConfigType::dtrEnable |
Enable Double transfer rate protocol for OSPI.
boolean Fls_ConfigType::phyEnable |
Enable PHY high-speed mode for DAC mode
OSPI_xferLines Fls_ConfigType::ospixferlines |
Select the OSPI read/write transaction Lines
uint32 Fls_ConfigType::flsBaudRateDiv |
To select the FLS baudrate Divider value
uint32 Fls_ConfigType::blockSize |
To select OSPI block size based on variants