![]() |
SDL API Guide for J7200
|
ESM init configuration.
Data Fields | |
SDL_ESM_ErrorConfig_t | esmErrorConfig |
uint32_t | enableBitmap [SDL_ESM_MAX_EVENT_MAP_NUM_WORDS] |
uint32_t | priorityBitmap [SDL_ESM_MAX_EVENT_MAP_NUM_WORDS] |
uint32_t | errorpinBitmap [SDL_ESM_MAX_EVENT_MAP_NUM_WORDS] |
uint32_t | pinmininterval |
SDL_ESM_ErrorConfig_t SDL_ESM_config::esmErrorConfig |
Error event to be used for self test
uint32_t SDL_ESM_config::enableBitmap[SDL_ESM_MAX_EVENT_MAP_NUM_WORDS] |
ESM Event bitmap
uint32_t SDL_ESM_config::priorityBitmap[SDL_ESM_MAX_EVENT_MAP_NUM_WORDS] |
ESM Event Priority bitmap
uint32_t SDL_ESM_config::errorpinBitmap[SDL_ESM_MAX_EVENT_MAP_NUM_WORDS] |
ESM bitmap for driving error pin: When selected error event occurs the error output pin will be asserted It is the application responsibility to reset the error if the system did not crash or lockup
uint32_t SDL_ESM_config::pinmininterval |