SDL API Guide for J7200
|
Header file contains enumerations, structure definitions and function declarations for SDL Error Signaling Module interface.
The SDL ESM enumerations include:
The SDL ESM function macros include:
The SDL ESM data structures include:
The SDL ESM APIs include:
Go to the source code of this file.
ESM ECC Error source type | |
#define | SDL_ESM_ECC_PARAM_MCU_CPU0_SEC_ERROR (1u) |
MCU CPU0 detected 1-bit ECC error source. More... | |
#define | SDL_ESM_ECC_PARAM_MCU_CPU0_DED_ERROR (2u) |
MCU CPU0 detected 2-bit ECC error source. More... | |
#define | SDL_ESM_ECC_PARAM_MCU_CPU1_SEC_ERROR (3u) |
MCU CPU1 detected 1-bit ECC error source. More... | |
#define | SDL_ESM_ECC_PARAM_MCU_CPU1_DED_ERROR (4u) |
MCU CPU1 detected 2-bit ECC error source. More... | |
#define | SDL_ESM_ECC_PARAM_MCU_CBASS_SEC_ERROR (5u) |
MCU CBASS detected 1-bit ECC error source. More... | |
#define | SDL_ESM_ECC_PARAM_MCU_CBASS_DED_ERROR (6u) |
MCU CBASS detected 2-bit ECC error source. More... | |
typedef uint32_t | sdlEsmEccErrorSource_t |
Source of the ECC error which maps to the ESM interrupt source. More... | |
Data Structures | |
struct | SDL_ESM_ErrorConfig_t |
ESM error configuration. More... | |
struct | SDL_ESM_config |
ESM init configuration. More... | |
Macros | |
#define | SDL_ESM_INTNUMBER_INVALID (0xffffffffu) |
Invalid interrupt number. More... | |
#define | SDL_ESM_INST_INVALID (0xfffffffeu) |
Invalid Esm Instance. More... | |
#define | SDL_ESM_ERRORADDR_INVALID (0xffffffffu) |
Address field: Error Address invalid. More... | |
#define | SDL_ESM_ERRORRAMID_INVALID (0xffffffffu) |
Address field: Error RAM ID invalid. More... | |
#define | SDL_ESM_ERRORBITOFFSET_INVALID (0xffffffffffffffffu) |
Address field: Error Bit Error Offset invalid. More... | |
#define | SDL_ESM_ERRORBITGROUP_INVALID (0xffffffffu) |
Address field: Error Bit Error Group invalid. More... | |
#define | SDL_ESM_MAX_EVENT_MAP_NUM_WORDS (32u) |
Maximum number of EVENT words. More... | |
#define | SDL_ESM_ECC_PARAM_MAIN_MSMC_AGGR0_SEC_ERROR (10001u) |
Main MSMC ECC AGGR0 detected 1-bit ECC error source. More... | |
#define | SDL_ESM_ECC_PARAM_MAIN_MSMC_AGGR0_DED_ERROR (10002u) |
Main MSMC ECC AGGR0 detected 2-bit ECC error source. More... | |
#define | SDL_ESM_ECC_PARAM_MAIN_A72_AGGR0_SEC_ERROR (10003u) |
Main A72 ECC AGGR0 detected 1-bit ECC error source. More... | |
#define | SDL_ESM_ECC_PARAM_MAIN_A72_AGGR0_DED_ERROR (10004u) |
Main A72 ECC AGGR0 detected 2-bit ECC error source. More... | |
Typedefs | |
typedef int32_t | SDL_Result |
This enumerator defines the values for ESM interrupt typesMore... | |
typedef int32_t(* | SDL_ESM_applicationCallback) (SDL_ESM_Inst instance, SDL_ESM_IntType intrType, uint32_t grpChannel, uint32_t index, uint32_t intSrc, void *arg) |
Enumerations | |
enum | SDL_ESM_IntType { SDL_ESM_INT_TYPE_HI = 1, SDL_ESM_INT_TYPE_LO = 2, SDL_ESM_INT_TYPE_CFG = 3, SDL_ESM_INT_TYPE_MAX = 4 } |
enum | SDL_ESM_CCM_IntSrc { SDL_ESM_CCM_OUTPUT_COMPARE_BLOCK_INT = 1, SDL_ESM_CCM_VIM_ERR_INT = 2, SDL_ESM_CCM_INACTIVITY_MONITOR_INT = 3, SDL_ESM_CCM_SELF_TEST_ERR_INT = 4, SDL_ESM_CCM_STAT_ERR_INT = 5 } |
Defines the different SDL ESM interrupt sourcesMore... | |
enum | SDL_ESM_WDT_IntSrc { SDL_ESM_TIMER_ID_0 = 1, SDL_ESM_TIMER_ID_1 = 2 } |
Defines the different Timer id eventsMore... | |
enum | SDL_ESM_Inst { SDL_ESM_INST_WKUP_ESM0 = 1, SDL_ESM_INST_MCU_ESM0 = 2, SDL_ESM_INST_MAIN_ESM0 = 3, SDL_ESM_INSTANCE_MAX =0xFFFF } |
Defines the different ESM instance typesMore... | |
Functions | |
void | SDL_ESM_hiInterruptHandler_MCU (uintptr_t arg) |
Esm Hi Interrupt Handler for MCU Esm Instance. More... | |
void | SDL_ESM_hiInterruptHandler_WKUP (uintptr_t arg) |
Esm Hi Interrupt Handler for WKUP Esm Instance. More... | |
void | SDL_ESM_hiInterruptHandler_MAIN (uintptr_t arg) |
Esm Hi Interrupt Handler for MAIN Esm Instance. More... | |
void | SDL_ESM_loInterruptHandler_MCU (uintptr_t arg) |
Esm Lo Interrupt Handler for MCU Esm Instance. More... | |
void | SDL_ESM_loInterruptHandler_WKUP (uintptr_t arg) |
Esm Lo Interrupt Handler for WKUP Esm Instance. More... | |
void | SDL_ESM_loInterruptHandler_MAIN (uintptr_t arg) |
Esm Lo Interrupt Handler for MAIN Esm Instance. More... | |
void | SDL_ESM_configInterruptHandler_MCU (uintptr_t arg) |
Esm Config Interrupt Handler for MCU Instance. More... | |
void | SDL_ESM_configInterruptHandler_WKUP (uintptr_t arg) |
Esm Config Interrupt Handler for WKUP Instance. More... | |
void | SDL_ESM_configInterruptHandler_MAIN (uintptr_t arg) |
Esm Config Interrupt Handler for MAIN Instance. More... | |
int32_t | SDL_ESM_getIntNumber (SDL_ESM_Inst esmInstType, SDL_ESM_IntType esmIntType) |
Esm get Interrupt Number corresponding to the input interrupt type. More... | |