![]() |
SDL API Guide for J7200
|
Functions | |
int32_t | SDL_VTM_initVd (SDL_VTM_InstVd instance, const SDL_VTM_configVd *pConfig) |
VTM Voltage Domain initialization. More... | |
int32_t | SDL_VTM_initTs (SDL_VTM_InstTs instance, const SDL_VTM_configTs *pConfig) |
VTM Temperature sensor initialization. More... | |
int32_t | SDL_VTM_getTemp (SDL_VTM_InstTs instance, uint32_t *pTempVal) |
Read VTM Temperature sensor values in degree celcius. More... | |
int32_t | SDL_VTM_getSensorStatus (SDL_VTM_InstTs instance, const SDL_VTM_Stat_read_ctrl *pCtrl, SDL_VTM_Stat_val *pStat_val) |
Read VTM Temperature sensor status. More... | |
int32_t | SDL_VTM_intrCntrl (SDL_VTM_InstVd instance, SDL_VTM_intrCtrl intrCtrl) |
Set maximum Threshold values of VTM Temperature sensor. More... | |
int32_t | SDL_VTM_verifyConfigVd (SDL_VTM_InstVd instance, const SDL_VTM_configVd *pConfig) |
VTM Voltage Domain configures verification. More... | |
int32_t | SDL_VTM_verifyConfigTs (SDL_VTM_InstTs instance, const SDL_VTM_configTs *pConfig) |
VTM Temperature sensor configures verification. More... | |
int32_t | SDL_VTM_getStaticRegistersVd (SDL_VTM_InstVd instance, SDL_VTM_staticRegsVd *pStaticRegs) |
VTM Voltage Domain readback Static configuration registers. More... | |
int32_t | SDL_VTM_getStaticRegistersTs (SDL_VTM_InstTs instance, SDL_VTM_staticRegsTs *pStaticRegs) |
VTM Temperature sensor readback Static configuration registers. More... | |
int32_t SDL_VTM_initVd | ( | SDL_VTM_InstVd | instance, |
const SDL_VTM_configVd * | pConfig | ||
) |
VTM Voltage Domain initialization.
This function executes a VTM Voltage Domain initialization of the specified type for a specific VTM VD instance. VTM is a feature that is used to set OPP VID, event selection, global configuration
instance | [IN] VTM Voltage Domain instance |
pConfig | [IN] Pointer to VTM VD configuration (optional) |
int32_t SDL_VTM_initTs | ( | SDL_VTM_InstTs | instance, |
const SDL_VTM_configTs * | pConfig | ||
) |
VTM Temperature sensor initialization.
This function executes a VTM Temperature sensor initialization of the specified type for a specific VTM TS instance. VTM is a feature that is used to set control register, thermal shutdown range, Threshold values and interrupts
instance | [IN] VTM Temperature sensor instance |
pConfig | [IN] Pointer to VTM TS configuration (optional) |
int32_t SDL_VTM_getTemp | ( | SDL_VTM_InstTs | instance, |
uint32_t * | pTempVal | ||
) |
Read VTM Temperature sensor values in degree celcius.
instance | [IN] VTM Temperature sensor instance |
pTempVal | [OUT] Pointer to Temperature sensor values |
int32_t SDL_VTM_getSensorStatus | ( | SDL_VTM_InstTs | instance, |
const SDL_VTM_Stat_read_ctrl * | pCtrl, | ||
SDL_VTM_Stat_val * | pStat_val | ||
) |
Read VTM Temperature sensor status.
instance | [IN] VTM Temperature sensor instance |
pCtrl | [IN] Pointer to VTM interrupt control |
pStat_val | [OUT] Pointer to Temperature sensor status |
int32_t SDL_VTM_intrCntrl | ( | SDL_VTM_InstVd | instance, |
SDL_VTM_intrCtrl | intrCtrl | ||
) |
Set maximum Threshold values of VTM Temperature sensor.
instance | [IN] VTM Temperature sensor instance |
intrCtrl | [IN] VTM interrupt control |
int32_t SDL_VTM_verifyConfigVd | ( | SDL_VTM_InstVd | instance, |
const SDL_VTM_configVd * | pConfig | ||
) |
VTM Voltage Domain configures verification.
instance | [IN] VTM Voltage Domain instance |
pConfig | [IN] Pointer to VTM VD configuration (optional) |
int32_t SDL_VTM_verifyConfigTs | ( | SDL_VTM_InstTs | instance, |
const SDL_VTM_configTs * | pConfig | ||
) |
VTM Temperature sensor configures verification.
instance | [IN] VTM Temperature sensor instance |
pConfig | [IN] Pointer to VTM VD configuration (optional) |
int32_t SDL_VTM_getStaticRegistersVd | ( | SDL_VTM_InstVd | instance, |
SDL_VTM_staticRegsVd * | pStaticRegs | ||
) |
VTM Voltage Domain readback Static configuration registers.
instance | [IN] VTM Voltage Domain instance |
pStaticRegs | [OUT] Pointer to VTM VD static register |
int32_t SDL_VTM_getStaticRegistersTs | ( | SDL_VTM_InstTs | instance, |
SDL_VTM_staticRegsTs * | pStaticRegs | ||
) |
VTM Temperature sensor readback Static configuration registers.
instance | [IN] VTM Temperature sensor instance |
pStaticRegs | [OUT] Pointer to VTM TS static register |