![]() |
SDL API Guide for J7200
|
VTM temperature sensor Stat values.
This structure contains VTM temperature sensor Stat values
Data Fields | |
SDL_VTM_ts_stat_vd_map | vd_map |
uint8_t | maxt_outrg_alert |
uint8_t | lt_th0_alert |
uint8_t | gt_th1_alert |
uint8_t | gt_th2_alert |
uint8_t | soc_fc_update |
uint8_t | data_valid |
SDL_VTM_adc_code | data_out |
SDL_VTM_ts_stat_vd_map SDL_VTM_Stat_val::vd_map |
Indicates the core voltage domain placement of the temperature sensor. Device specific field. This field indicates in which core voltage domain, cVD, has been physically placed the temp-monitor. Valid values: 0x0 to 0xE where: 0x0 = VD_RTC, not present is some SOCs, 0x1 = VD_WKUP, 0x2 = VD_MCU, 0x3 = VD_CORE etc
uint8_t SDL_VTM_Stat_val::maxt_outrg_alert |
This bit will be driven to a level 1 for a given temperature monitor if it has its corresponding bit maxt_outrg_en = 1, and the temperature reading is reporting to be outside the max temperature supported, temp > programmed value
uint8_t SDL_VTM_Stat_val::lt_th0_alert |
reflects the status of the lt_th0_alert comparator result.
uint8_t SDL_VTM_Stat_val::gt_th1_alert |
reflects the status of the gt_th1_alert comparator result
uint8_t SDL_VTM_Stat_val::gt_th2_alert |
reflects the status of the gt_th2_alert comparator result
uint8_t SDL_VTM_Stat_val::soc_fc_update |
ADC conversion status
uint8_t SDL_VTM_Stat_val::data_valid |
Data valid bit after the adc is done
SDL_VTM_adc_code SDL_VTM_Stat_val::data_out |
Data_out signal value from sensor: Temperature data from the ADC in monitor.