![]() |
SDL API Guide for J7200
|
Functions | |
int32_t | SDL_RAT_isRegionTranslationEnabled (const SDL_ratRegs *pRatRegs, uint32_t regionIndex) |
This function returns the enable status of the specified region address translation. More... | |
uint32_t | SDL_RAT_getMaxRegions (const SDL_ratRegs *pRatRegs) |
int32_t | SDL_RAT_setErrMsgDestId (SDL_ratRegs *pRatRegs, uint32_t destId) |
This function is used to set the destination ID for error messages. More... | |
int32_t | SDL_RAT_getErrMsgDestId (const SDL_ratRegs *pRatRegs, uint32_t *pDestId) |
This function is used to read the destination ID for error messages. More... | |
int32_t | SDL_RAT_enableExceptionLog (SDL_ratRegs *pRatRegs) |
This function enables the exception logging capability. It also enables exception interrupt generation. The module's exception interrupt signal is asserted if the exception logging capability is enabled and the exception interrupt source is enabled by calling the. More... | |
int32_t | SDL_RAT_disableExceptionLog (SDL_ratRegs *pRatRegs) |
This function disables the exception logging capability. It also disables the module's exception interrupt signal generation, regardless of whether the exception interrupt source is enabled or disabled. More... | |
int32_t | SDL_RAT_isIntrPending (const SDL_ratRegs *pRatRegs, SDL_RAT_intrSrcTypes intrSrc) |
This function returns the pending interrupt status of the specified interrupt source. More... | |
int32_t | SDL_RAT_setIntrPending (SDL_ratRegs *pRatRegs, SDL_RAT_intrSrcTypes intrSrc) |
This function is used to forceably set the pending status of the specified interrupt source. More... | |
int32_t | SDL_RAT_clrIntrPending (SDL_ratRegs *pRatRegs, SDL_RAT_intrSrcTypes intrSrc) |
This function is used to clear the pending status of the specified interrupt source. More... | |
int32_t | SDL_RAT_ackIntr (SDL_ratRegs *pRatRegs, SDL_RAT_intrSrcTypes intrSrc) |
This function is used to acknowledge the specified interrupt source. More... | |
int32_t | SDL_RAT_enableIntr (SDL_ratRegs *pRatRegs, SDL_RAT_intrSrcTypes intrSrc) |
This function enables the specified interrupt source. It also calls SDL_RAT_enableExceptionLog to enable exception logging as there is no valid reason to enable the exception interrupt source and not log the exception information and assert the module's exception interrupt signal. More... | |
int32_t | SDL_RAT_disableIntr (SDL_ratRegs *pRatRegs, SDL_RAT_intrSrcTypes intrSrc) |
This function disables the specified interrupt source. This prevents the module's exception interrupt signal from being asserted. Note that software can still call SDL_RAT_isIntrPending to poll for an exception event and call SDL_RAT_getExceptionInfo to read exception event information if exception logging is enabled. More... | |
int32_t | SDL_RAT_getExceptionInfo (SDL_ratRegs *pRatRegs, SDL_ratExceptionInfo *pExceptionInfo) |
This function is used to get information for the last boundary crossing transaction exception captured. The log is automatically cleared by this function so that a future exception can be captured. More... | |
int32_t | SDL_RAT_enableRegionTranslation (SDL_ratRegs *pRatRegs, uint32_t regionIndex) |
This function enables address translation for the specified region. More... | |
int32_t | SDL_RAT_disableRegionTranslation (SDL_ratRegs *pRatRegs, uint32_t regionIndex) |
This function disables address translation for the specified region. More... | |
int32_t | SDL_RAT_configRegionTranslation (SDL_ratRegs *pRatRegs, uint32_t regionIndex, SDL_ratTranslationCfgInfo *pTranslationCfg) |
This function is used to configure a region address translation for the specified region index. The translation is automatically enabled after it is configured. More... | |
int32_t | SDL_RAT_verifyConfigRegionTranslation (const SDL_ratRegs *pRatRegs, uint32_t regionIndex, SDL_ratTranslationCfgInfo *pTranslationCfg) |
This function is used to configure a region address translation for the specified region index. The translation is automatically enabled after it is configured. More... | |
int32_t | SDL_RAT_getStaticRegs (SDL_ratRegs *pRatRegs, uint32_t regionIndex, SDL_ratStaticRegs *pStaticRegs) |
This function returns the enable status of the specified region address translation. More... | |
int32_t SDL_RAT_isRegionTranslationEnabled | ( | const SDL_ratRegs * | pRatRegs, |
uint32_t | regionIndex | ||
) |
This function returns the enable status of the specified region address translation.
SDL_RAT_isRegionTranslationEnabled
Description
This function returns the enable status of the specified region address translation
Arguments
pRatRegs - A pointer (of type SDL_ratRegs*) to the base address of the RAT module
regionIndex - The index of the region to configure. This value must be in the range 0..(SDL_RAT_getMaxRegions()-1) inclusive.
Return Value
true - The specified region address translation is enabled
false - The specified region address translation is not enabled
Pre Condition
None
Post Condition
None
Reads
SDL_RAT_CTRL
Example
SDL_ratRegs *pRatRegs = (SDL_ratRegs *)RAT_BASE_ADDRESS; uint32_t regionIndex = 0; bool bIsEnabled; bIsEnabled = SDL_ratIsRegionTranslationEnabled(pRatRegs,regionIndex); printf("Address translation for region %u is %s\n", regionIndex, bIsEnabled ? "enabled" : "not enabled" );
pRatRegs | - A pointer (of type SDL_ratRegs*) to the base address of the RAT module |
regionIndex | - The index of the region to configure. This value must be in the range 0..(SDL_RAT_getMaxRegions()-1) inclusive. |
uint32_t SDL_RAT_getMaxRegions | ( | const SDL_ratRegs * | pRatRegs | ) |
SDL_RAT_getMaxRegions
Description
This function returns the maximum number of regions that can be configured.
Arguments
pRatRegs - A pointer (of type SDL_ratRegs*) to the base address of the RAT module
Return Value
The the maximum number of regions that can be configured in this RAT
Pre Condition
None
Post Condition
None
Reads
None
Example
SDL_ratRegs *pRatRegs = (SDL_ratRegs *)RAT_BASE_ADDRESS; uint32_t maxRegions; maxRegions = SDL_ratGetMaxRegions(pRatRegs);
int32_t SDL_RAT_setErrMsgDestId | ( | SDL_ratRegs * | pRatRegs, |
uint32_t | destId | ||
) |
This function is used to set the destination ID for error messages.
pRatRegs | - A pointer (of type SDL_ratRegs*) to the base address of the RAT module |
destId | - The destination ID for future error messages |
int32_t SDL_RAT_getErrMsgDestId | ( | const SDL_ratRegs * | pRatRegs, |
uint32_t * | pDestId | ||
) |
This function is used to read the destination ID for error messages.
pRatRegs | - A pointer (of type SDL_ratRegs*) to the base address of the RAT module |
pDestId | - A pointer to hold the destination ID register value |
int32_t SDL_RAT_enableExceptionLog | ( | SDL_ratRegs * | pRatRegs | ) |
This function enables the exception logging capability. It also enables exception interrupt generation. The module's exception interrupt signal is asserted if the exception logging capability is enabled and the exception interrupt source is enabled by calling the.
pRatRegs | - A pointer (of type SDL_ratRegs*) to the base address of the RAT module |
int32_t SDL_RAT_disableExceptionLog | ( | SDL_ratRegs * | pRatRegs | ) |
This function disables the exception logging capability. It also disables the module's exception interrupt signal generation, regardless of whether the exception interrupt source is enabled or disabled.
pRatRegs | - A pointer (of type SDL_ratRegs*) to the base address of the RAT module |
int32_t SDL_RAT_isIntrPending | ( | const SDL_ratRegs * | pRatRegs, |
SDL_RAT_intrSrcTypes | intrSrc | ||
) |
This function returns the pending interrupt status of the specified interrupt source.
pRatRegs | - A pointer (of type SDL_ratRegs*) to the base address of the RAT module |
intrSrc | - The interrupt source of type SDL_RAT_intrSrcTypes |
int32_t SDL_RAT_setIntrPending | ( | SDL_ratRegs * | pRatRegs, |
SDL_RAT_intrSrcTypes | intrSrc | ||
) |
This function is used to forceably set the pending status of the specified interrupt source.
pRatRegs | - A pointer (of type SDL_ratRegs*) to the base address of the RAT module |
intrSrc | - The interrupt source of type SDL_RAT_intrSrcTypes |
int32_t SDL_RAT_clrIntrPending | ( | SDL_ratRegs * | pRatRegs, |
SDL_RAT_intrSrcTypes | intrSrc | ||
) |
This function is used to clear the pending status of the specified interrupt source.
pRatRegs | - A pointer (of type SDL_ratRegs*) to the base address of the RAT module |
intrSrc | - The interrupt source of type SDL_RAT_intrSrcTypes |
int32_t SDL_RAT_ackIntr | ( | SDL_ratRegs * | pRatRegs, |
SDL_RAT_intrSrcTypes | intrSrc | ||
) |
This function is used to acknowledge the specified interrupt source.
pRatRegs | - A pointer (of type SDL_ratRegs*) to the base address of the RAT module |
intrSrc | - The interrupt source of type SDL_RAT_intrSrcTypes |
int32_t SDL_RAT_enableIntr | ( | SDL_ratRegs * | pRatRegs, |
SDL_RAT_intrSrcTypes | intrSrc | ||
) |
This function enables the specified interrupt source. It also calls SDL_RAT_enableExceptionLog to enable exception logging as there is no valid reason to enable the exception interrupt source and not log the exception information and assert the module's exception interrupt signal.
pRatRegs | - A pointer (of type SDL_ratRegs*) to the base address of the RAT module |
intrSrc | - The interrupt source of type SDL_RAT_intrSrcTypes |
int32_t SDL_RAT_disableIntr | ( | SDL_ratRegs * | pRatRegs, |
SDL_RAT_intrSrcTypes | intrSrc | ||
) |
This function disables the specified interrupt source. This prevents the module's exception interrupt signal from being asserted. Note that software can still call SDL_RAT_isIntrPending to poll for an exception event and call SDL_RAT_getExceptionInfo to read exception event information if exception logging is enabled.
pRatRegs | - A pointer (of type SDL_ratRegs*) to the base address of the RAT module |
intrSrc | - The interrupt source of type SDL_RAT_intrSrcTypes |
int32_t SDL_RAT_getExceptionInfo | ( | SDL_ratRegs * | pRatRegs, |
SDL_ratExceptionInfo * | pExceptionInfo | ||
) |
This function is used to get information for the last boundary crossing transaction exception captured. The log is automatically cleared by this function so that a future exception can be captured.
pRatRegs | - A pointer (of type SDL_ratRegs*) to the base address of the RAT module |
pExceptionInfo | - A pointer to a SDL_ratExceptionInfo structure containing returned exception information |
int32_t SDL_RAT_enableRegionTranslation | ( | SDL_ratRegs * | pRatRegs, |
uint32_t | regionIndex | ||
) |
This function enables address translation for the specified region.
pRatRegs | - A pointer (of type SDL_ratRegs*) to the base address of the RAT module |
regionIndex | - The index of the region to configure. This value must be in the range 0..(SDL_RAT_getMaxRegions()-1) inclusive. |
int32_t SDL_RAT_disableRegionTranslation | ( | SDL_ratRegs * | pRatRegs, |
uint32_t | regionIndex | ||
) |
This function disables address translation for the specified region.
pRatRegs | - A pointer (of type SDL_ratRegs*) to the base address of the RAT module |
regionIndex | - The index of the region to configure. This value must be in the range 0..(SDL_RAT_getMaxRegions()-1) inclusive. |
int32_t SDL_RAT_configRegionTranslation | ( | SDL_ratRegs * | pRatRegs, |
uint32_t | regionIndex, | ||
SDL_ratTranslationCfgInfo * | pTranslationCfg | ||
) |
This function is used to configure a region address translation for the specified region index. The translation is automatically enabled after it is configured.
pRatRegs | - A pointer (of type SDL_ratRegs*) to the base address of the RAT module |
regionIndex | - The index of the region to configure. This value must be in the range 0..(SDL_RAT_getMaxRegions()-1) inclusive. |
pTranslationCfg | - A pointer of type SDL_ratTranslationCfgInfo containing configuration information |
int32_t SDL_RAT_verifyConfigRegionTranslation | ( | const SDL_ratRegs * | pRatRegs, |
uint32_t | regionIndex, | ||
SDL_ratTranslationCfgInfo * | pTranslationCfg | ||
) |
This function is used to configure a region address translation for the specified region index. The translation is automatically enabled after it is configured.
pRatRegs | - A pointer (of type SDL_ratRegs*) to the base address of the RAT module |
regionIndex | - The index of the region to configure. This value must be in the range 0..(SDL_RAT_getMaxRegions()-1) inclusive. |
pTranslationCfg | - A pointer of type SDL_ratTranslationCfgInfo containing configuration information |
int32_t SDL_RAT_getStaticRegs | ( | SDL_ratRegs * | pRatRegs, |
uint32_t | regionIndex, | ||
SDL_ratStaticRegs * | pStaticRegs | ||
) |
This function returns the enable status of the specified region address translation.
pRatRegs | - A pointer (of type SDL_ratRegs*) to the base address of the RAT module |
regionIndex | - The index of the region to configure. This value must be in the range 0..(SDL_RAT_getMaxRegions()-1) inclusive. |
pStaticRegs | - A pointer to the static registers structure. |