![]() |
SDL API Guide for J7200
|
This structure contains exception status information returned by the SDL_RAT_getExceptionInfo function.
Data Fields | |
uint32_t | type |
uint64_t | address |
uint32_t | group |
uint32_t | code |
uint32_t | srcId |
uint32_t | destId |
uint32_t | routeId |
uint32_t | privId |
uint32_t | byteCnt |
bool | bWrite |
bool | bRead |
bool | bDebug |
bool | bCacheable |
bool | bPriv |
bool | bSecure |
uint32_t SDL_ratExceptionInfo::type |
Identifies the exception type (for the RAT, this field should equal 4)
uint64_t SDL_ratExceptionInfo::address |
Address
uint32_t SDL_ratExceptionInfo::group |
Group
uint32_t SDL_ratExceptionInfo::code |
Code
uint32_t SDL_ratExceptionInfo::srcId |
Source ID
uint32_t SDL_ratExceptionInfo::destId |
Destination ID
uint32_t SDL_ratExceptionInfo::routeId |
Route ID
uint32_t SDL_ratExceptionInfo::privId |
Priv ID
uint32_t SDL_ratExceptionInfo::byteCnt |
Byte Count
bool SDL_ratExceptionInfo::bWrite |
Write
bool SDL_ratExceptionInfo::bRead |
Read
bool SDL_ratExceptionInfo::bDebug |
Debug
bool SDL_ratExceptionInfo::bCacheable |
Cacheable
bool SDL_ratExceptionInfo::bPriv |
Priv
bool SDL_ratExceptionInfo::bSecure |
Secure