![]() |
SDL API Guide for J7200
|
===========================================================================
Functions | |
int32_t | SDL_MTOG_init (SDL_MTOG_Inst instance, const SDL_MTOG_config *pConfig) |
Initialize Master TOG module with respect of instance. More... | |
int32_t | SDL_MTOG_verifyConfig (SDL_MTOG_Inst instance, const SDL_MTOG_config *pConfig) |
Verifying written configuration with Master TOG module. More... | |
int32_t | SDL_MTOG_start (SDL_MTOG_Inst instance) |
Start the timeout function. More... | |
int32_t | SDL_MTOG_stop (SDL_MTOG_Inst instance) |
Stop the timeout function. More... | |
int32_t | SDL_MTOG_forceTimeout (SDL_MTOG_Inst instance) |
Force a timeout. More... | |
int32_t | SDL_MTOG_reset (SDL_MTOG_Inst instance) |
Reset the timeout functionality. More... | |
int32_t | SDL_MTOG_getStaticRegisters (SDL_MTOG_Inst instance, SDL_MTOG_staticRegs *pStaticRegs) |
Readback Static configuration register. More... | |
int32_t SDL_MTOG_init | ( | SDL_MTOG_Inst | instance, |
const SDL_MTOG_config * | pConfig | ||
) |
Initialize Master TOG module with respect of instance.
This function allows software to initialize MTOG module
The pConfig contains the timeout value
instance | [IN] MTOG instance |
pConfig | [IN] Pointer to store the configuration |
int32_t SDL_MTOG_verifyConfig | ( | SDL_MTOG_Inst | instance, |
const SDL_MTOG_config * | pConfig | ||
) |
Verifying written configuration with Master TOG module.
This function allows software to verifying MTOG module
The pConfig contains the timeout value
instance | [IN] MTOG instance |
pConfig | [IN] Pointer to store the configuration |
int32_t SDL_MTOG_start | ( | SDL_MTOG_Inst | instance | ) |
Start the timeout function.
This function starts the timeout counter functionality.
instance | [IN] MTOG instance |
int32_t SDL_MTOG_stop | ( | SDL_MTOG_Inst | instance | ) |
Stop the timeout function.
This function stops the timeout counter functionality.
instance | [IN] MTOG instance |
int32_t SDL_MTOG_forceTimeout | ( | SDL_MTOG_Inst | instance | ) |
Force a timeout.
This function enables software to force a timeout and flush of the interface transactions.
instance | [IN] MTOG instance |
int32_t SDL_MTOG_reset | ( | SDL_MTOG_Inst | instance | ) |
Reset the timeout functionality.
This function resets the timeout functionality by clearing the timeout interrupt and timeout counter. It should be called after servicing a timeout interrupt and before re-enabling the timeout counter via the SDL_MTOG_start function.
Note that the timeout value set via the SDL_MTOG_setTimeoutVal function is unaffected.
instance | [IN] MTOG instance |
int32_t SDL_MTOG_getStaticRegisters | ( | SDL_MTOG_Inst | instance, |
SDL_MTOG_staticRegs * | pStaticRegs | ||
) |
Readback Static configuration register.
This function reads back configuration registers that are static. Note that this is just one register master TOG
instance | [IN] MTOG instance |
pStaticRegs | [OUT] Pointer to store the read static registers |