![]() |
SDL API Guide for J7200
|
This is the SDL-FL API documentation for the VBUSM Master Timeout Gasket module.
The following procedure describes how to properly use this SDL-FL API:
Whenever a read return or write status return is pending without being accepted, an internal timer increments by 1. Whenever the counter value meets or exceeds the programmed value, the gasket is in a timed out state and the following actions are taken:
Following servicing of the timeout interrupt, software should...
Sub Modules | |
MTOG Data Structures | |
MTOG Enumerated Data Types | |
MTOG Functions | |