![]() |
SDL API Guide for J7200
|
Provides the APIs for POK.
Sub Modules | |
POK Data Structures | |
POK Enum Data defines | |
POK Functions | |
Files | |
file | sdl_pok_def.h |
Header file containing various enumerations, structure definitions and function declarations for the Power System modules such as POK/POR IP. | |
Data Structures | |
struct | SDL_pokShiftsAndMasks_t |
struct | SDL_pokPRGInfo_t |
Functions | |
int32_t | SDL_pok_getPRGInfo (SDL_wkupCtrlRegsBase_t *pBaseAddress, SDL_PRG_Inst instance, SDL_pokPRGInfo_t *pPRGInfo) |
void | sdlGetErrSig (uint32_t id, SDL_POK_Inst *instance, uint32_t *esm_err_sig_ov, uint32_t *esm_err_sig_uv, bool *usePorCfgFlag) |
int32_t SDL_pok_getPRGInfo | ( | SDL_wkupCtrlRegsBase_t * | pBaseAddress, |
SDL_PRG_Inst | instance, | ||
SDL_pokPRGInfo_t * | pPRGInfo | ||
) |
void sdlGetErrSig | ( | uint32_t | id, |
SDL_POK_Inst * | instance, | ||
uint32_t * | esm_err_sig_ov, | ||
uint32_t * | esm_err_sig_uv, | ||
bool * | usePorCfgFlag | ||
) |