Important

This developer note only applies when using ETHFW based networking, such as io-pkt based CPSW5G/9G on SDP 7.1.

11.8. VLAN Configuration using ETHFW

As of PSDK RTOS release 10.01.00, static VLAN configurations have been added to ETHFW. In previous releases ETHFW would forward all VLAN traffic to all registered clients. As of the PSDK RTOS 10.01.00 release, by default ETHFW will only forward VLAN traffic of VLAN id 1024. For more details on how to configure ETHFW to forward more VLANs, please refer to the “VLAN Support” section of the ETHFW user guide (LINK).