UDMA channel object. More...
#include <udma_ch.h>
Data Fields | |
| uint32_t | chType |
| Udma_ChPrms | chPrms |
| Udma_DrvHandle | drvHandle |
| uint32_t | txChNum |
| uint32_t | rxChNum |
| uint32_t | extChNum |
| uint32_t | pdmaChNum |
| uint32_t | peerThreadId |
| Udma_RingHandle | fqRing |
| Udma_RingHandle | cqRing |
| Udma_RingHandle | tdCqRing |
| struct Udma_RingObj | fqRingObj |
| struct Udma_RingObj | cqRingObj |
| struct Udma_RingObj | tdCqRingObj |
| Udma_FlowHandle | defaultFlow |
| struct Udma_FlowObj | defaultFlowObj |
| Udma_ChTxPrms | txPrms |
| Udma_ChRxPrms | rxPrms |
| Udma_ChUtcPrms | utcPrms |
| uint32_t | chInitDone |
| uint32_t | chOesAllocDone |
| uint32_t | trigger |
UDMA channel object.
UDMA channel handle.
Note: This is an internal/private driver structure and should not be used or modified by caller.