UDMA RX channel parameters. More...
#include <udma_ch.h>
Data Fields | |
| uint8_t | pauseOnError |
| uint8_t | addrType |
| uint8_t | chanType |
| uint16_t | fetchWordSize |
| uint8_t | busPriority |
| uint8_t | busQos |
| uint8_t | busOrderId |
| uint8_t | dmaPriority |
| uint16_t | flowIdFwRangeStart |
| uint16_t | flowIdFwRangeCnt |
| uint8_t | flowEInfoPresent |
| uint8_t | flowPsInfoPresent |
| uint8_t | flowErrorHandling |
| uint8_t | flowSopOffset |
| uint8_t | ignoreShortPkts |
| uint8_t | ignoreLongPkts |
| uint32_t | configDefaultFlow |
| uint8_t | burstSize |
UDMA RX channel parameters.