Files | |
| file | udma_flow.h |
| UDMA flow related parameters and API. | |
Data Structures | |
| struct | Udma_FlowPrms |
| UDMA RX channel flow parameters. More... | |
| struct | Udma_FlowAllocMappedPrms |
| UDMA RX channel mapped flow alloc parameters. More... | |
| struct | Udma_FlowHandle |
| UDMA flow object. More... | |
Macros | |
| #define | UDMA_DEFAULT_FLOW_ID (0x3FFFU) |
| Default flow ID. More... | |
| #define | UDMA_FLOW_INVALID ((uint32_t) 0xFFFF0000U) |
| Macro used to specify that flow ID is invalid. More... | |
Functions | |
| int32_t | Udma_flowAlloc (Udma_DrvHandle drvHandle, Udma_FlowHandle flowHandle, uint32_t flowCnt) |
| UDMA flow allocation API. More... | |
| int32_t | Udma_flowAllocMapped (Udma_DrvHandle drvHandle, Udma_FlowHandle flowHandle, const Udma_FlowAllocMappedPrms *flowAllocMappedPrms) |
| UDMA mapped flow allocation API. In devices like AM64x, flows are tied to channels. This API is used to allocate a single flow from the mapped free flows which are dedicated for a particular channel. More... | |
| int32_t | Udma_flowFree (Udma_FlowHandle flowHandle) |
| UDMA free flows. More... | |
| int32_t | Udma_flowAttach (Udma_DrvHandle drvHandle, Udma_FlowHandle flowHandle, uint32_t flowStart, uint32_t flowCnt) |
| UDMA flow attach API. This API is used to attach to an already allocated flow. This API differs from flow alloc API in this aspect - it doesn't allocate resource from RM. Once the flow is attached to, Udma_flowConfig API can be used to configure the flow through sciclient/DMSC API. More... | |
| int32_t | Udma_flowAttachMapped (Udma_DrvHandle drvHandle, Udma_FlowHandle flowHandle, uint32_t mappepdFlowNum, const Udma_FlowAllocMappedPrms *flowAllocMappedPrms) |
| UDMA mapped flow attach API. This API is used to attach to an already allocated mapped flow. This API differs from mapped flow alloc API in this aspect - it doesn't allocate resource from RM. Once the flow is attached to, Udma_flowConfig API can be used to configure the flow through sciclient/DMSC API. More... | |
| int32_t | Udma_flowDetach (Udma_FlowHandle flowHandle) |
| UDMA flow detach API. More... | |
| int32_t | Udma_flowConfig (Udma_FlowHandle flowHandle, uint32_t flowIdx, const Udma_FlowPrms *flowPrms) |
| This API configures the flow configurations. More... | |
| uint32_t | Udma_flowGetNum (Udma_FlowHandle flowHandle) |
| Returns the start flow number managed by this flow handle. More... | |
| uint32_t | Udma_flowGetCount (Udma_FlowHandle flowHandle) |
| Returns the number of flows managed by this flow handle. More... | |
| int32_t | UdmaFlowPrms_init (Udma_FlowPrms *flowPrms, uint32_t chType) |
| Udma_FlowPrms structure init function. More... | |
This is UDMA driver RX flow related configuration parameters and API
| #define UDMA_DEFAULT_FLOW_ID (0x3FFFU) |
Default flow ID.
| #define UDMA_FLOW_INVALID ((uint32_t) 0xFFFF0000U) |
Macro used to specify that flow ID is invalid.
| int32_t Udma_flowAlloc | ( | Udma_DrvHandle | drvHandle, |
| Udma_FlowHandle | flowHandle, | ||
| uint32_t | flowCnt | ||
| ) |
UDMA flow allocation API.
| drvHandle | [IN] UDMA driver handle pointer passed during Udma_init |
| flowHandle | [IN/OUT] UDMA flow handle. The caller need to allocate memory for this object and pass this pointer to all further APIs. The caller should not change any parameters as this is owned and maintained by the driver. |
| flowCnt | [IN] Flow count. The driver will allocate this many flows contiguously. |
| int32_t Udma_flowAllocMapped | ( | Udma_DrvHandle | drvHandle, |
| Udma_FlowHandle | flowHandle, | ||
| const Udma_FlowAllocMappedPrms * | flowAllocMappedPrms | ||
| ) |
UDMA mapped flow allocation API. In devices like AM64x, flows are tied to channels. This API is used to allocate a single flow from the mapped free flows which are dedicated for a particular channel.
Note: Allocation of mapped flows have to be done after Udma_chOpen, Since the mapped flow have to be allocated from the dedicated flows for the particular channel.
| drvHandle | [IN] UDMA driver handle pointer passed during Udma_init |
| flowHandle | [IN/OUT] UDMA flow handle. The caller need to allocate memory for this object and pass this pointer to all further APIs. The caller should not change any parameters as this is owned and maintained by the driver. |
| flowAllocMappedPrms | [IN] UDMA mapped flow alloc parameters. This parameter can't be NULL. |
| int32_t Udma_flowFree | ( | Udma_FlowHandle | flowHandle | ) |
UDMA free flows.
Freeup the flow resources.
Note: This API can be used to free mapped flow also, which are allocated using Udma_flowAllocMapped.
Requirement: TODO
| flowHandle | [IN] UDMA flow handle. This parameter can't be NULL. |
| int32_t Udma_flowAttach | ( | Udma_DrvHandle | drvHandle, |
| Udma_FlowHandle | flowHandle, | ||
| uint32_t | flowStart, | ||
| uint32_t | flowCnt | ||
| ) |
UDMA flow attach API. This API is used to attach to an already allocated flow. This API differs from flow alloc API in this aspect - it doesn't allocate resource from RM. Once the flow is attached to, Udma_flowConfig API can be used to configure the flow through sciclient/DMSC API.
Requirement: DOX_REQ_TAG(PDK-3418)
| drvHandle | [IN] UDMA driver handle pointer passed during Udma_init |
| flowHandle | [IN/OUT] UDMA flow handle. The caller need to allocate memory for this object and pass this pointer to all further APIs. The caller should not change any parameters as this is owned and maintained by the driver. |
| flowStart | [IN] Flow index to attach to. This paramter should be a valid flow number allowed to be used by a core. The driver doesn't check the validity of this field at the time of attach. But the flow config API may fail if wrong flow index is used or when the core doesn't own the flow as per DMSC board config. |
| flowCnt | [IN] Flow count - to attach to more than 1 flow which is contiguous from flow start. This is provided to allow a single handle to manage multiple contiguous flows similar to how Udma_flowAlloc and Udma_flowConfig API are implemented. |
| int32_t Udma_flowAttachMapped | ( | Udma_DrvHandle | drvHandle, |
| Udma_FlowHandle | flowHandle, | ||
| uint32_t | mappepdFlowNum, | ||
| const Udma_FlowAllocMappedPrms * | flowAllocMappedPrms | ||
| ) |
UDMA mapped flow attach API. This API is used to attach to an already allocated mapped flow. This API differs from mapped flow alloc API in this aspect - it doesn't allocate resource from RM. Once the flow is attached to, Udma_flowConfig API can be used to configure the flow through sciclient/DMSC API.
Requirement: DOX_REQ_TAG(PDK-3418)
| drvHandle | [IN] UDMA driver handle pointer passed during Udma_init |
| flowHandle | [IN/OUT] UDMA flow handle. The caller need to allocate memory for this object and pass this pointer to all further APIs. The caller should not change any parameters as this is owned and maintained by the driver. |
| mappepdFlowNum | [IN] Mapped flow index to attach to. This paramter should be a valid mapped flow number allowed to be used by a core and by the mapped channel. The driver doesn't check the validity of this field at the time of attach. But the flow config API may fail if wrong mapped flow index is used or when the core doesn't own the mapped flow as per DMSC board config or if the mapped flow dosen't belong to the deicated flows for the particular channel. |
| flowAllocMappedPrms | [IN] UDMA mapped flow alloc parameters. This parameter can't be NULL. |
| int32_t Udma_flowDetach | ( | Udma_FlowHandle | flowHandle | ) |
UDMA flow detach API.
Since no allocation is done in attach, this API just clears up the flow handle.
Note: This API can be used to detach mapped flow also, which are attached using Udma_flowAttachMapped.
Requirement: DOX_REQ_TAG(PDK-3418)
| flowHandle | [IN] UDMA flow handle. This parameter can't be NULL. |
| int32_t Udma_flowConfig | ( | Udma_FlowHandle | flowHandle, |
| uint32_t | flowIdx, | ||
| const Udma_FlowPrms * | flowPrms | ||
| ) |
This API configures the flow configurations.
Requirement: DOX_REQ_TAG(PDK-2599)
| flowHandle | [IN] UDMA flow handle pointer |
| flowIdx | [IN] Since multiple flows are allocated and also contiguously, all the flows needs to be configured one after the other. This is the relative index from the start of the flow allocated. If the index goes beyond what is allocated, then the function returns error. Note: In case of configuring the default flow and mapped flow(in devices like AM64x), this should be set to "zero". |
| flowPrms | [IN] Pointer to flow configuration. |
| uint32_t Udma_flowGetNum | ( | Udma_FlowHandle | flowHandle | ) |
Returns the start flow number managed by this flow handle.
Note: In case off mapped flow(in devices like AM64x), this returns the mapped flow number.
Requirement: TODO
| flowHandle | [IN] UDMA flow handle. This parameter can't be NULL. |
| uint32_t Udma_flowGetCount | ( | Udma_FlowHandle | flowHandle | ) |
Returns the number of flows managed by this flow handle.
Note: In case of mapped flow(in devices like AM64x), this always returns 1, since only one mapped flow is managed by a flow handle.
Requirement: DOX_REQ_TAG(PDK-3718)
| flowHandle | [IN] UDMA flow handle. This parameter can't be NULL. |
| int32_t UdmaFlowPrms_init | ( | Udma_FlowPrms * | flowPrms, |
| uint32_t | chType | ||
| ) |
Udma_FlowPrms structure init function.
| flowPrms | [IN] Pointer to Udma_FlowPrms structure. |
| chType | [IN] UDMA channel type. Refer Udma_ChType. |
| Udma_ChHandle Udma_FlowPrms::rxChHandle |
[IN] Deprecated member. Not used any more.
| uint8_t Udma_FlowPrms::einfoPresent |
[IN] Set to 1 if extended packet info is present in the descriptor
| uint8_t Udma_FlowPrms::psInfoPresent |
[IN] Set to 1 if protocol-specific info is present in the descriptor
| uint8_t Udma_FlowPrms::errorHandling |
[IN] Determines how starvation errors are handled. 0=drop packet, 1=retry
| uint8_t Udma_FlowPrms::descType |
[IN] Descriptor type - see tisci_msg_rm_udmap_flow_cfg_req::rx_desc_type
| uint8_t Udma_FlowPrms::psLocation |
[IN] Protocol-specific info location. TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_PS_END_PD TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_PS_BEGIN_DB
| uint16_t Udma_FlowPrms::sopOffset |
[IN] Start of rx packet data (byte offset from the start of the SOP buffer)
| uint16_t Udma_FlowPrms::defaultRxCQ |
[IN] Rx destination queue
| uint8_t Udma_FlowPrms::srcTagHi |
[IN] UDMAP receive flow source tag high byte constant configuration to be programmed into the rx_src_tag_hi field of the flow's RFLOW_RFB register.
| uint8_t Udma_FlowPrms::srcTagLo |
[IN] UDMAP receive flow source tag low byte constant configuration to be programmed into the rx_src_tag_lo field of the flow's RFLOW_RFB register.
| uint8_t Udma_FlowPrms::srcTagHiSel |
[IN] UDMAP receive flow source tag high byte selector configuration to be programmed into the rx_src_tag_hi_sel field of the RFLOW_RFC register. Refer tisci_msg_rm_udmap_flow_cfg_req::rx_dest_tag_hi_sel.
| uint8_t Udma_FlowPrms::srcTagLoSel |
[IN] UDMAP receive flow source tag low byte selector configuration to be programmed into the rx_src_tag_low_sel field of the RFLOW_RFC register. Refer tisci_msg_rm_udmap_flow_cfg_req::rx_dest_tag_lo_sel.
| uint8_t Udma_FlowPrms::destTagHi |
[IN] UDMAP receive flow destination tag high byte constant configuration to be programmed into the rx_dest_tag_hi field of the flow's RFLOW_RFB register.
| uint8_t Udma_FlowPrms::destTagLo |
[IN] UDMAP receive flow destination tag low byte constant configuration to be programmed into the rx_dest_tag_lo field of the flow's RFLOW_RFB register.
| uint8_t Udma_FlowPrms::destTagHiSel |
[IN] UDMAP receive flow destination tag high byte selector configuration to be programmed into the rx_dest_tag_hi_sel field of the RFLOW_RFC register. Refer tisci_msg_rm_udmap_flow_cfg_req::rx_dest_tag_hi_sel.
| uint8_t Udma_FlowPrms::destTagLoSel |
[IN] UDMAP receive flow destination tag low byte selector configuration to be programmed into the rx_dest_tag_low_sel field of the RFLOW_RFC register. Refer tisci_msg_rm_udmap_flow_cfg_req::rx_dest_tag_lo_sel.
| uint8_t Udma_FlowPrms::sizeThreshEn |
[IN] UDMAP receive flow packet size based free buffer queue enable configuration to be programmed into the rx_size_thresh_en field of the RFLOW_RFC register. See the UDMAP section of the TRM for more information on this setting. Configuration of the optional size thresholds when this configuration is enabled is done by sending the tisci_msg_rm_udmap_flow_size_thresh_cfg_req message to System Firmware for the receive flow allocated by this request. This parameter can be no greater than TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_SIZE_THRESH_MAX
| uint16_t Udma_FlowPrms::fdq0Sz0Qnum |
[IN] UDMAP receive flow free descriptor queue 0 configuration to be programmed into the rx_fdq0_sz0_qnum field of the flow's RFLOW_RFD register. See the UDMAP section of the TRM for more information on this setting. The specified free queue must be valid within the Navigator Subsystem and must be owned by the host, or a subordinate of the host, requesting allocation and configuration of the receive flow.
| uint16_t Udma_FlowPrms::fdq1Qnum |
[IN] UDMAP receive flow free descriptor queue 1 configuration to be programmed into the rx_fdq1_qnum field of the flow's RFLOW_RFD register. See the UDMAP section of the TRM for more information on this setting. The specified free queue must be valid within the Navigator Subsystem and must be owned by the host, or a subordinate of the host, requesting allocation and configuration of the receive flow.
| uint16_t Udma_FlowPrms::fdq2Qnum |
[IN] UDMAP receive flow free descriptor queue 2 configuration to be programmed into the rx_fdq2_qnum field of the flow's RFLOW_RFE register. See the UDMAP section of the TRM for more information on this setting. The specified free queue must be valid within the Navigator Subsystem and must be owned by the host, or a subordinate of the host, requesting allocation and configuration of the receive flow.
| uint16_t Udma_FlowPrms::fdq3Qnum |
[IN] UDMAP receive flow free descriptor queue 3 configuration to be programmed into the rx_fdq3_qnum field of the flow's RFLOW_RFE register. See the UDMAP section of the TRM for more information on this setting. The specified free queue must be valid within the Navigator Subsystem and must be owned by the host, or a subordinate of the host, requesting allocation and configuration of the receive flow.
| uint16_t Udma_FlowPrms::sizeThresh0 |
[IN] UDMAP receive flow packet size threshold 0 configuration to be programmed into the rx_size_thresh0 field of the flow's RFLOW_RFF register. See the UDMAP section of the TRM for more information on this setting.
| uint16_t Udma_FlowPrms::sizeThresh1 |
[IN] UDMAP receive flow packet size threshold 1 configuration to be programmed into the rx_size_thresh1 field of the flow's RFLOW_RFF register. See the UDMAP section of the TRM for more information on this setting.
| uint16_t Udma_FlowPrms::sizeThresh2 |
[IN] UDMAP receive flow packet size threshold 2 configuration to be programmed into the rx_size_thresh2 field of the flow's RFLOW_RFG register. See the UDMAP section of the TRM for more information on this setting.
| uint16_t Udma_FlowPrms::fdq0Sz1Qnum |
[IN] UDMAP receive flow free descriptor queue for size threshold 1 configuration to be programmed into the rx_fdq0_sz1_qnum field of the flow's RFLOW_RFG register. See the UDMAP section of the TRM for more information on this setting. The specified free queue must be valid within the Navigator Subsystem and must be owned by the host, or a subordinate of the host, who owns the receive flow index and who is making the optional configuration request.
| uint16_t Udma_FlowPrms::fdq0Sz2Qnum |
[IN] UDMAP receive flow free descriptor queue for size threshold 2 configuration to be programmed into the rx_fdq0_sz2_qnum field of the flow's RFLOW_RFH register. See the UDMAP section of the TRM for more information on this setting. The specified free queue must be valid within the Navigator Subsystem and must be owned by the host, or a subordinate of the host, who owns the receive flow index and who is making the optional configuration request.
| uint16_t Udma_FlowPrms::fdq0Sz3Qnum |
[IN] UDMAP receive flow free descriptor queue for size threshold 3 configuration to be programmed into the rx_fdq0_sz3_qnum field of the flow's RFLOW_RFH register. See the UDMAP section of the TRM for more information on this setting. The specified free queue must be valid within the Navigator Subsystem and must be owned by the host, or a subordinate of the host, who owns the receive flow index and who is making the optional configuration request.
| uint32_t Udma_FlowAllocMappedPrms::mappedFlowGrp |
The Mapped flow group to use when channel type is UDMA_CH_TYPE_RX_MAPPED.
The driver will allocate mapped flows from this group. Refer Udma_MappedRxGrpSoc macro for details about mapped RX flow groups.
| uint32_t Udma_FlowAllocMappedPrms::mappedChNum |
The assigned mapped channel number when channel type is UDMA_CH_TYPE_RX_MAPPED.
This is used to allocate the corresponding mapped flow for the particular channel. The driver will allocate from the mapped flows which are dedicated for this particular channel.
| Udma_DrvHandle Udma_FlowHandle::drvHandle |
Pointer to global driver handle.
| uint32_t Udma_FlowHandle::flowStart |
Flow ID start number.
Note: In case of mapped flow(in devices like AM64x), this indicates the mapped flow idx managed by this flow handle.
| uint32_t Udma_FlowHandle::flowCnt |
Number of flow IDs allocated - Contiguos flows are allocated
Note: In case of mapped flow(in devices like AM64x), this will be 1 since only one mapped flow is managed by a flow handle.
| uint32_t Udma_FlowHandle::flowInitDone |
Flag to set the flow object is init.
| uint32_t Udma_FlowHandle::mappedFlowGrp |
The allocated mapped flow group when channel type is UDMA_CH_TYPE_RX_MAPPED.
This is needed to free the mapped flow.
Refer Udma_MappedRxGrpSoc macro for details about mapped RX flow groups.
For unmapped case, this will be UDMA_MAPPED_GROUP_INVALID
| uint32_t Udma_FlowHandle::mappedChNum |
The assigned mapped channel number when channel type is UDMA_CH_TYPE_RX_MAPPED.
This is needed to free the mapped flow.
For unmapped case, this will be UDMA_DMA_CH_INVALID.