3.2.2.10.3.3.2.1. PTP
3.2.2.10.3.3.2.1.1. Introduction
The Common Platform Time Sync (CPTS) module is used to facilitate host control of time sync operations. It enables compliance with the IEEE 1588-2008 standard for a precision clock synchronization protocol.
The support for CPTS module can be enabled by Kconfig option CONFIG_TI_AM65_CPTS or through menuconfig tool.
When CPTS module is enabled it will exports a kernel interface for specific clock drivers and a PTP clock API user space interface and enable support for SIOCSHWTSTAMP and SIOCGHWTSTAMP socket ioctls. The PTP exposes the PHC as a character device with standardized ioctls which usually can be found at path:
/dev/ptpN
Supported PTP hardware clock functionality:
Basic clock operations
- Set time
- Get time
- Shift the clock by a given offset atomically
- Adjust clock frequency
Ancillary clock features
- Time stamp external events
- Periodic output signals configurable from user space
- Synchronization of the Linux system time via the PPS subsystem
Supported parameters for SIOCSHWTSTAMP and SIOCGHWTSTAMP:
SIOCSHWTSTAMP
hwtstamp_config.flags = 0
hwtstamp_config.tx_type
HWTSTAMP_TX_ON - enables hardware time stamping for outgoing packets
HWTSTAMP_TX_OFF - no outgoing packet will need hardware time stamping
hwtstamp_config.rx_filter
HWTSTAMP_FILTER_NONE - time stamp no incoming packet at all
HWTSTAMP_FILTER_ALL - time stamp any incoming packet
CPTS PTP packet timestamping default configuration when enabled (SIOCSHWTSTAMP):
CPSW_PN_TS_CTL_REG
TS_MSG_TYPE_EN = 0xF (Sync, Delay_Req, Pdelay_Req, and Pdelay_Resp.)
TS_TX_ANNEX_F_EN = 1
TS_TX_ANNEX_E_EN = 1
TS_TX_ANNEX_D_EN = 1
TS_TX_VLAN_LTYPE1_E = 1
CPSW_PN_TS_CTL_LTYPE2_REG
TS_TTL_NONZERO = 1
TS_320 = 1
TS_319 = 1
TS_132 = 1
TS_131 = 1
TS_130 = 1
TS_129 = 1
TS_107 = 1
TS_LTYPE1 = 0x88F7 (ETH_P_1588)
CPSW_PN_TS_SEQ_LTYPE_REG
TS_SEQ_ID_OFFSET = 0x1e
TS_LTYPE1 = 0x88F7 (ETH_P_1588)
CPSW_PN_TS_VLAN_LTYPE_REG
TS_VLAN_LTYPE1 = 0x8100 (ETH_P_8021Q)
For more information about PTP clock API and Network timestamping see Linux kernel documentation
To check the ptp clock adjustment with PTP protocol, a PTP slave (client) and a PTP master (server) applications are needed to run on separate devices (EVM or PC). Open source application package linuxptp can be used as slave and as well as master. Hence TX timestamp generation can be delayed (especially with low speed links) the ptp4l “tx_timestamp_timeout” parameter needs to be set for ptp4l to work.
create file ptp.cfg with content as below:
[global]
tx_timestamp_timeout 400
pass configuration file to ptp4l using “-f” option:
ptp4l -E -2 -H -i eth0 -l 6 -m -q -p /dev/ptpN -f ptp.cfg
Slave Side Examples
The following command can be used to run a ptp-over-L4 client on the evm in slave mode
./ptp4l -E -4 -H -i eth0 -s -l 7 -m -q -p /dev/ptpN
For ptp-over-L2 client, use the command
./ptp4l -E -2 -H -i eth0 -s -l 7 -m -q -p /dev/ptpN
Master Side Examples
ptp4l can also be run in master mode. For example, the following command starts a ptp4l-over-L2 master on an EVM using hardware timestamping,
./ptp4l -E -2 -H -i eth0 -l 7 -m -q -p /dev/ptpN
On a Linux PC which does not support hardware timestamping, the following command starts a ptp4l-over-L2 master using software timestamping.
./ptp4l -E -2 -S -i eth0 -l 7 -m -q
Testing using testptp tool from Linux kernel
get the ptp clock time
# testptp -d /dev/ptpN -g
clock time: 1493255613.608918429 or Thu Apr 27 01:13:33 2017
query the ptp clock’s capabilities
# testptp -d /dev/ptpN -c
capabilities:
10000000 maximum frequency adjustment (ppb)
0 programmable alarms
4 external time stamp channels
2 programmable periodic signals
1 pulse per second
0 programmable pins
0 cross timestamping
Sanity testing of cpts ref frequency
Time difference between to testptp -g calls should be equal sleep time
# testptp -g -d /dev/ptpN && sleep 5 && testptp -g -d /dev/ptpN
clock time: 1493255884.565859901 or Thu Apr 27 01:18:04 2017
clock time: 1493255889.611065421 or Thu Apr 27 01:18:09 2017
shift the ptp clock time by ‘val’ seconds
# testptp -g -d /dev/ptpN && testptp -t 100 && testptp -g -d /dev/ptpN
clock time: 1493256107.640649117 or Thu Apr 27 01:21:47 2017
time shift okay
clock time: 1493256207.678819093 or Thu Apr 27 01:23:27 2017
set the ptp clock time to ‘val’ seconds
# testptp -g -d /dev/ptpN && testptp -T 1000000 && testptp -g -d /dev/ptpN
clock time: 1493256277.568238925 or Thu Apr 27 01:24:37 2017
set time okay
clock time: 100.018944504 or Thu Jan 1 00:01:40 1970
adjust the ptp clock frequency by ‘val’ ppb
# testptp -g -d /dev/ptpN && testptp -f 1000000 && testptp -g -d /dev/ptpN
clock time: 151.347795184 or Thu Jan 1 00:02:31 1970
frequency adjustment okay
clock time: 151.386187454 or Thu Jan 1 00:02:31 1970
Time stamping external events
External events can be timestamped by the CPTS module. The CPTS module loads a hardware timestamp event to the Event FIFO, whenever the HWx_TS_PUSH inputs are set. Thus, it is possible to timestamp events by using the HWx_TS_PUSH inputs to the CPTS module.
The following example illustrates the process of timestamping an external event. The external event in the example corresponds to the rising edge of GENF0 (Timestamp Generator Function). This involves using the output of CPSWxG CPTS GENF0 as an input to one of the HWx_TS_PUSH inputs.
The process of routing the CPSWxG CPTS GENF0 output to any of the HWx_TS_PUSH inputs is achieved through the Time Sync Router. The procedure to route the CPSWxG CPTS GENF0 output to HW4_TS_PUSH input for example, involves modifying the device-tree node of the Time Sync Router, to map the CPWSxG CPTS GENF0 output to HW4_TS_PUSH input.
The following block shows the Time Sync Router device-tree node with the mapping from CPSWxG CPTS GENF0 to HW4_TS_PUSH added.
#define TS_OFFSET(pa, val) (0x4+(pa)*4) (0x10000 | val)
×ync_router {
pinctrl-names = "default";
pinctrl-0 = <&cpsw_cpts>;
/* Example of the timesync routing */
cpsw_cpts: cpsw-cpts {
pinctrl-single,pins = <
/* pps [cpsw cpts genf0] in16 -> out25 [cpsw cpts hw4_push] */
TS_OFFSET(25, 16)
>;
};
};
Similar approach can be used for routing the outputs of other timestamp generator functions (GENFy) as inputs to other Hardware Timestamping push inputs (HWx_TS_PUSH).
The Input Sources and their indices, along with the Output Destinations and their indices for the Time Sync Router are obtained from the documentation as mentioned below.
The Input Sources for the Time Sync Router are documented at:
Time Sync Router Input Sources for J721E
The Output Destinations for the Time Sync Router are documented at:
Time Sync Router Output Destinations for J721E
To test that the timestamping feature works with the above changes, execute the following
# testptp -d /dev/ptpN -p 500000000 -i 0
# testptp -d /dev/ptpN -e 5 -i 3
event index 2 at 384.250000025
event index 2 at 384.750000025
event index 2 at 385.250000025
event index 2 at 385.750000025
event index 2 at 386.250000025
The first command is used to specify that /dev/ptpN has to be used as the clock, with the output period (‘p’) being 500000000 nanoseconds (500 milliseconds) and the event index ‘i’ being 0 (corresponding to GENF0).
The second command is used to specify that /dev/ptpN has to be used as the clock, with the first 5 events to be output (‘e’) , corresponding to the event index 3 (‘i’). Event index starts from 0, due to which, the 3 here corresponds to HW4_TS_PUSH.
PPS Pulse Per Second support
The PPS support for TDA4VM can be enabled with the following steps:
Route the output of the CPSWxG CPTS timestamp generator function (GENFy) to one of the CPSWxG CPTS timestamp generator inputs (HWx_TS_PUSH) using the Time Sync Router, by modifying the device-tree node corresponding to the Time Sync Router:
For example, route CPSWxG CPTS GENF1 output to HW3_TS_PUSH input
#define TS_OFFSET(pa, val) (0x4+(pa)*4) (0x10000 | val)
×ync_router {
pinctrl-names = "default";
pinctrl-0 = <&cpsw_cpts>;
/* Example of timesync routing */
cpsw_cpts: cpsw-cpts {
pinctrl-single,pins = <
/* pps [cpsw cpts genf1] in17 -> out24 [cpsw cpts hw3_push] */
TS_OFFSET(24, 17)
>;
};
};
Inform the mapping to the CPSWxG driver, by using the “ti,pps” device-tree property in the cpts device-tree node present within the CPSWxG device-tree node:
&cpswx {
cpts@3d000 {
ti,pps = <2 1>;
};
};
The property “ti,pps” is of the form <x-1 y>, where x and y correspond to the choice of HWx_TS_PUSH and GENFy.
PPS can now be tested using testptp and ppstest tools:
# ./testptp -d /dev/ptpX -P 1
pps for system time request okay
# ./ppstest /dev/pps0
trying PPS source "/dev/pps0"
found PPS source "/dev/pps0"
ok, found 1 source(s), now start fetching data...
source 0 - assert 198.000000700, sequence: 7 - clear 0.000000000, sequence: 0
source 0 - assert 199.000000700, sequence: 8 - clear 0.000000000, sequence: 0
Note
When using PPS signal along with PTP, the ptp4l application has to be rerun before enabling the PPS signal. This is required in order to ensure that the PPS signal remains in sync with the PHC which in turn is synchronized with the PTP master clock via the ptp4l application. If the ptp4l application is run after enabling the PPS signal, then the PPS signal will not be in sync with the PHC. Additionally, if the ptp4l application is stopped and rerun at any point in time, then the command to generate the PPS signal also has to be rerurn accordingly.
3.2.2.10.3.3.2.1.2. Setup
1. In both J7VCL and AM625-SK, create a config file named ptp.cfg whose contents are as follows:
[global]
tx_timestamp_timeout 400
Install ptp4l if it is not already present on the boards.
3.2.2.10.3.3.2.1.3. PTP with Ordinary Clock (MAC mode)
3.2.2.10.3.3.2.1.3.1. J7VCL as master clock and AM625-SK as slave clock
Assuming that eth1 is the interface on J7VCL that is connected to eth0 on AM625-SK, the following commands have to be run. The commands can be modified for different interface connections.
Steps:
Run the following on J7VCL:
ptp4l -E -2 -H -i eth1 -l 6 -m -q -f ptp.cfg
Run the following on AM625-SK:
ptp4l -E -2 -H -i eth0 -s -l 6 -m -q -f ptp.cfg
Observed Outputs:
On J7VCL:
root@j7200-evm:~/TSN-PTP4L# ptp4l -E -2 -H -i eth1 -l 6 -m -q -f ptp.cfg
ptp4l[1827.484]: selected /dev/ptp2 as PTP clock
ptp4l[1827.561]: port 1 (eth1): INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[1827.561]: port 0 (/var/run/ptp4l): INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[1834.569]: port 1: announce timeout
ptp4l[1834.569]: port 1 (eth1): LISTENING to MASTER on ANNOUNCE_RECEIPT_TIMEOUT_EXPIRES
ptp4l[1834.569]: selected best master clock 70ff76.fffe.1d8c08
ptp4l[1834.569]: selected local clock 70ff76.fffe.1d8c08 as best master
ptp4l[1834.569]: port 1: assuming the grand master role
On AM625-SK:
root@am62xx-evm:~# ptp4l -E -2 -H -i eth0 -s -l 6 -m -q -f ptp.cfg
ptp4l[1874.715]: selected /dev/ptp0 as PTP clock
ptp4l[1874.763]: port 1 (eth0): INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[1874.763]: port 0 (/var/run/ptp4l): INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[1875.717]: port 1: new foreign master 70ff76.fffe.1d8c08-1
ptp4l[1879.717]: selected best master clock 70ff76.fffe.1d8c08 on port 1
ptp4l[1879.717]: selected best master clock 70ff76.fffe.1d8c08
ptp4l[1879.717]: port 1 (eth0): LISTENING to UNCALIBRATED on RS_SLAVE
ptp4l[1881.717]: master offset 1146408914 s0 freq +0 path delay -1582
ptp4l[1882.717]: master offset 1146420591 s1 freq +11677 path delay -2965
ptp4l[1883.717]: master offset -4307 s2 freq +7370 path delay -2965
ptp4l[1883.717]: port 1 (eth0): UNCALIBRATED to SLAVE on MASTER_CLOCK_SELECTED
ptp4l[1884.717]: master offset -1385 s2 freq +9000 path delay -2965
ptp4l[1885.717]: master offset -1480 s2 freq +8489 path delay -1582
ptp4l[1886.717]: master offset -405 s2 freq +9120 path delay -851
ptp4l[1887.717]: master offset 48 s2 freq +9452 path delay -121
ptp4l[1888.717]: master offset 888 s2 freq +10306 path delay -121
ptp4l[1889.717]: master offset 758 s2 freq +10442 path delay 3
ptp4l[1890.718]: master offset 614 s2 freq +10526 path delay 3
ptp4l[1891.717]: master offset -96 s2 freq +10000 path delay 479
ptp4l[1892.718]: master offset 199 s2 freq +10266 path delay 479
ptp4l[1893.718]: master offset 221 s2 freq +10348 path delay 497
ptp4l[1894.718]: master offset 145 s2 freq +10338 path delay 519
ptp4l[1895.718]: master offset 103 s2 freq +10340 path delay 519
ptp4l[1896.718]: master offset 43 s2 freq +10311 path delay 529
ptp4l[1897.718]: master offset 17 s2 freq +10297 path delay 529
ptp4l[1898.718]: master offset 12 s2 freq +10298 path delay 529
ptp4l[1899.718]: master offset 3 s2 freq +10292 path delay 529
ptp4l[1900.718]: master offset -3 s2 freq +10287 path delay 529
ptp4l[1901.718]: master offset 2 s2 freq +10291 path delay 529
ptp4l[1902.718]: master offset -7 s2 freq +10283 path delay 529
ptp4l[1903.718]: master offset 0 s2 freq +10288 path delay 528
ptp4l[1904.718]: master offset -3 s2 freq +10285 path delay 528
ptp4l[1905.718]: master offset -9 s2 freq +10278 path delay 526
ptp4l[1906.718]: master offset 0 s2 freq +10284 path delay 525
ptp4l[1907.718]: master offset 8 s2 freq +10292 path delay 524
ptp4l[1908.718]: master offset 2 s2 freq +10288 path delay 524
ptp4l[1909.718]: master offset 6 s2 freq +10293 path delay 524
ptp4l[1910.718]: master offset -6 s2 freq +10283 path delay 524
ptp4l[1911.718]: master offset 3 s2 freq +10290 path delay 523
ptp4l[1912.718]: master offset 3 s2 freq +10291 path delay 523
ptp4l[1913.718]: master offset 4 s2 freq +10293 path delay 523
ptp4l[1914.719]: master offset -3 s2 freq +10287 path delay 523
ptp4l[1915.719]: master offset 9 s2 freq +10298 path delay 522
ptp4l[1916.718]: master offset 1 s2 freq +10293 path delay 523
ptp4l[1917.719]: master offset 2 s2 freq +10294 path delay 523
ptp4l[1918.719]: master offset -12 s2 freq +10281 path delay 523
3.2.2.10.3.3.2.1.3.2. AM625-SK as master clock and J7VCL as slave clock
Assuming that eth1 is the interface on J7VCL that is connected to eth0 on AM625-SK, the following commands have to be run. The commands can be modified for different interface connections.
Steps:
Run the following on AM625-SK:
ptp4l -E -2 -H -i eth0 -l 6 -m -q -f ptp.cfg
Run the following on J7VCL:
ptp4l -E -2 -H -i eth1 -s -l 6 -m -q -f ptp.cfg
Observed Outputs:
On AM625-SK:
root@am62xx-evm:~# ptp4l -E -2 -H -i eth0 -l 6 -m -q -f ptp.cfg
ptp4l[2647.841]: selected /dev/ptp0 as PTP clock
ptp4l[2647.895]: port 1 (eth0): INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[2647.895]: port 0 (/var/run/ptp4l): INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[2655.009]: port 1: announce timeout
ptp4l[2655.010]: port 1 (eth0): LISTENING to MASTER on ANNOUNCE_RECEIPT_TIMEOUT_EXPIRES
ptp4l[2655.010]: selected best master clock f4844c.fffe.fc1151
ptp4l[2655.010]: selected local clock f4844c.fffe.fc1151 as best master
ptp4l[2655.010]: port 1: assuming the grand master role
On J7VCL:
root@j7200-evm:~/TSN-PTP4L# ptp4l -E -2 -H -i eth1 -s -l 6 -m -q -f ptp.cfg
ptp4l[2215.575]: selected /dev/ptp2 as PTP clock
ptp4l[2215.657]: port 1 (eth1): INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[2215.657]: port 0 (/var/run/ptp4l): INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[2215.787]: port 1: new foreign master f4844c.fffe.fc1151-1
ptp4l[2219.787]: selected best master clock f4844c.fffe.fc1151 on port 1
ptp4l[2219.787]: selected best master clock f4844c.fffe.fc1151
ptp4l[2219.787]: port 1 (eth1): LISTENING to UNCALIBRATED on RS_SLAVE
ptp4l[2221.786]: master offset 15033 s0 freq +0 path delay -38
ptp4l[2222.787]: master offset 16404 s2 freq +1371 path delay -38
ptp4l[2222.787]: port 1 (eth1): UNCALIBRATED to SLAVE on MASTER_CLOCK_SELECTED
ptp4l[2223.787]: master offset 15861 s2 freq +17232 path delay 523
ptp4l[2224.786]: master offset 27 s2 freq +6156 path delay 523
ptp4l[2225.787]: master offset -4768 s2 freq +1369 path delay 523
ptp4l[2226.787]: master offset -4758 s2 freq -51 path delay 523
ptp4l[2227.787]: master offset -3322 s2 freq -43 path delay 520
ptp4l[2228.787]: master offset -1895 s2 freq +388 path delay 520
ptp4l[2229.787]: master offset -725 s2 freq +989 path delay 344
ptp4l[2230.787]: master offset -334 s2 freq +1163 path delay 344
ptp4l[2231.787]: master offset -253 s2 freq +1144 path delay 482
ptp4l[2232.787]: master offset -11 s2 freq +1310 path delay 477
ptp4l[2233.787]: master offset 39 s2 freq +1356 path delay 490
ptp4l[2234.787]: master offset 43 s2 freq +1372 path delay 490
ptp4l[2235.787]: master offset 39 s2 freq +1381 path delay 490
ptp4l[2236.787]: master offset 31 s2 freq +1385 path delay 490
ptp4l[2237.787]: master offset 13 s2 freq +1376 path delay 490
ptp4l[2238.787]: master offset -3 s2 freq +1364 path delay 490
ptp4l[2239.787]: master offset -3 s2 freq +1363 path delay 490
ptp4l[2240.787]: master offset -10 s2 freq +1355 path delay 500
ptp4l[2241.787]: master offset -26 s2 freq +1336 path delay 521
ptp4l[2242.787]: master offset -14 s2 freq +1340 path delay 521
ptp4l[2243.788]: master offset 18 s2 freq +1368 path delay 521
ptp4l[2244.788]: master offset 13 s2 freq +1369 path delay 524
ptp4l[2245.788]: master offset 17 s2 freq +1376 path delay 524
ptp4l[2246.788]: master offset -6 s2 freq +1359 path delay 524
ptp4l[2247.788]: master offset -19 s2 freq +1344 path delay 524
ptp4l[2248.788]: master offset -6 s2 freq +1351 path delay 524
3.2.2.10.3.3.2.1.4. PTP with Transparent Clock (Switch mode)
Use the following ptp config file on the device that acts as the transparent clock:
tc-ptp.cfg
[global]
tx_timestamp_timeout 400
clock_type E2E_TC
On other devices, the existing ptp.cfg file can be used.
3.2.2.10.3.3.2.1.4.1. J7VCL as transparent clock, PC as master clock and AM625-SK as slave clock
Switch mode is enabled on J7VCL, with the CPSW5G ports in QSGMII mode acting as switch ports. A PC (Personal Computer) with Software Timestamping capability is used (PC with Hardware Timestamping capability or another board is preferred) as the master clock. The setup is as follows:
PC is connected to eth1 of J7VCL’s CPSW5G ports while AM625-SK’s eth0 is connected to J7VCL’s eth2.
Note
Since the PC uses Software Timestamping, the offset is relatively large when compared to the previous section where only boards with Hardware Timestamping capabilities were used.
Steps:
Enable switch mode on J7VCL by running the following commands:
devlink dev param set platform/c000000.ethernet name switch_mode value true cmode runtime
ip link add name br0 type bridge
ip link set dev br0 type bridge ageing_time 1000
ip link set dev eth1 up
ip link set dev eth2 up
ip link set dev eth1 master br0
ip link set dev eth2 master br0
ip link set dev br0 up
ip link set dev br0 type bridge vlan_filtering 1
bridge vlan add dev br0 vid 1 self
bridge vlan add dev br0 vid 1 pvid untagged self
# Ensure that multicast flooding is off
bridge link set dev eth1 mcast_flood off
bridge link set dev eth2 mcast_flood off
On the PC, create the same ptp.cfg file mentioned earlier and run:
sudo ptp4l -E -2 -S -i enp2s0 -l 6 -m -q -f ptp.cfg
enp2s0 is assumed to be the ethernet interface. Replace -S with -H if PC supports Hardware Timestamping.
On J7VCL, run:
ptp4l -E -2 -H -i eth1 -i eth2 -s -f tc-ptp.cfg --step_threshold=1 -m -q
On AM625-SK, run:
ptp4l -E -2 -H -i eth0 -s -l 6 -m -q -f ptp.cfg
Observed Outputs:
On PC:
user@pc:~/TSN-PTP4L$ sudo ptp4l -E -2 -S -i enp2s0 -l 6 -m -q -f p.cfg
ptp4l[16750.478]: port 1: INITIALIZING to LISTENING on INITIALIZE
ptp4l[16750.478]: port 0: INITIALIZING to LISTENING on INITIALIZE
ptp4l[16750.478]: port 1: link up
ptp4l[16757.189]: port 1: LISTENING to MASTER on ANNOUNCE_RECEIPT_TIMEOUT_EXPIRES
ptp4l[16757.189]: selected best master clock b0227a.fffe.d8b7e3
ptp4l[16757.189]: assuming the grand master role
On J7VCL:
root@j7200-evm:~/PTP# ptp4l -E -2 -H -i eth1 -i eth2 -s -f ptp.cfg --step_threshold=1 -q -m
ptp4l[602.896]: selected /dev/ptp2 as PTP clock
ptp4l[602.936]: port 1 (eth1): INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[602.968]: port 2 (eth2): INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[602.968]: port 0 (/var/run/ptp4l): INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[604.014]: port 1: new foreign master b0227a.fffe.d8b7e3-1
ptp4l[608.014]: selected best master clock b0227a.fffe.d8b7e3 on port 1
ptp4l[608.014]: selected best master clock b0227a.fffe.d8b7e3
ptp4l[608.014]: foreign master not using PTP timescale
ptp4l[608.014]: running in a temporal vortex
ptp4l[608.014]: port 1 (eth1): LISTENING to UNCALIBRATED on RS_SLAVE
ptp4l[609.182]: selected best master clock b0227a.fffe.d8b7e3 on port 1
ptp4l[609.182]: selected best master clock b0227a.fffe.d8b7e3
ptp4l[609.182]: foreign master not using PTP timescale
ptp4l[609.182]: running in a temporal vortex
ptp4l[610.015]: master offset 4240878 s0 freq -29261 path delay 411528
ptp4l[611.015]: master offset 4420049 s1 freq +149852 path delay 411528
ptp4l[612.015]: master offset -217741 s2 freq -67889 path delay 411528
ptp4l[612.015]: port 1 (eth1): UNCALIBRATED to SLAVE on MASTER_CLOCK_SELECTED
ptp4l[613.015]: master offset 19010 s2 freq +103540 path delay 411528
ptp4l[614.015]: master offset -169233 s2 freq -79000 path delay 432761
ptp4l[615.015]: master offset 74375 s2 freq +113838 path delay 432761
ptp4l[615.965]: selected best master clock b0227a.fffe.d8b7e3 on port 1
ptp4l[615.965]: selected best master clock b0227a.fffe.d8b7e3
ptp4l[615.965]: foreign master not using PTP timescale
ptp4l[615.965]: running in a temporal vortex
ptp4l[616.015]: master offset -249811 s2 freq -188035 path delay 447928
ptp4l[617.016]: master offset 255527 s2 freq +195312 path delay 429728
ptp4l[618.016]: master offset -92188 s2 freq -105356 path delay 447928
ptp4l[619.016]: master offset 279496 s2 freq +195312 path delay 429728
ptp4l[620.016]: master offset -53619 s2 freq -94443 path delay 447928
ptp4l[621.016]: master offset 258016 s2 freq +195312 path delay 447928
ptp4l[622.016]: master offset -143222 s2 freq -195312 path delay 453994
ptp4l[623.016]: master offset 355710 s2 freq +195312 path delay 453994
ptp4l[623.037]: selected best master clock b0227a.fffe.d8b7e3 on port 1
ptp4l[623.037]: selected best master clock b0227a.fffe.d8b7e3
ptp4l[623.037]: foreign master not using PTP timescale
ptp4l[623.037]: running in a temporal vortex
ptp4l[624.016]: master offset -81029 s2 freq -137939 path delay 456066
ptp4l[625.017]: master offset 399612 s2 freq +195312 path delay 456066
ptp4l[626.017]: master offset -59174 s2 freq -140392 path delay 456066
ptp4l[627.017]: master offset 535534 s2 freq +195312 path delay 372817
ptp4l[628.017]: master offset 68957 s2 freq -30014 path delay 372817
ptp4l[629.017]: master offset 469268 s2 freq +195312 path delay 372817
ptp4l[630.017]: master offset 227264 s2 freq +148980 path delay 465639
ptp4l[630.879]: selected best master clock b0227a.fffe.d8b7e3 on port 1
ptp4l[630.879]: selected best master clock b0227a.fffe.d8b7e3
ptp4l[630.879]: foreign master not using PTP timescale
ptp4l[630.879]: running in a temporal vortex
ptp4l[631.018]: master offset 188501 s2 freq +178397 path delay 416485
ptp4l[632.017]: master offset -292192 s2 freq -195312 path delay 416485
ptp4l[633.018]: master offset 392634 s2 freq +195312 path delay 322010
ptp4l[634.017]: master offset -61040 s2 freq -14594 path delay 322010
ptp4l[635.018]: master offset 318688 s2 freq +195312 path delay 322010
ptp4l[636.018]: master offset -177868 s2 freq -149734 path delay 322010
ptp4l[637.018]: master offset 371574 s2 freq +195312 path delay 320475
ptp4l[637.827]: selected best master clock b0227a.fffe.d8b7e3 on port 1
ptp4l[637.827]: selected best master clock b0227a.fffe.d8b7e3
ptp4l[637.827]: foreign master not using PTP timescale
ptp4l[637.827]: running in a temporal vortex
ptp4l[638.018]: master offset 129834 s2 freq +104608 path delay 420138
ptp4l[639.018]: master offset 71472 s2 freq +85196 path delay 420138
ptp4l[640.019]: master offset 45549 s2 freq +80714 path delay 411496
ptp4l[641.019]: master offset 15511 s2 freq +64341 path delay 411496
ptp4l[642.019]: master offset -41550 s2 freq +11933 path delay 451793
ptp4l[643.019]: master offset 3387 s2 freq +44405 path delay 441161
ptp4l[644.019]: master offset 6207 s2 freq +48241 path delay 441161
ptp4l[644.259]: selected best master clock b0227a.fffe.d8b7e3 on port 1
ptp4l[644.259]: selected best master clock b0227a.fffe.d8b7e3
ptp4l[644.259]: foreign master not using PTP timescale
ptp4l[644.259]: running in a temporal vortex
ptp4l[645.019]: master offset 11684 s2 freq +55581 path delay 437299
ptp4l[646.019]: master offset 1653 s2 freq +49055 path delay 443743
ptp4l[647.019]: master offset -6190 s2 freq +41708 path delay 447606
ptp4l[648.019]: master offset 3011 s2 freq +49052 path delay 444569
ptp4l[649.020]: master offset 3506 s2 freq +50450 path delay 447606
ptp4l[650.020]: master offset -6195 s2 freq +41801 path delay 447606
ptp4l[650.630]: selected best master clock b0227a.fffe.d8b7e3 on port 1
ptp4l[650.630]: selected best master clock b0227a.fffe.d8b7e3
ptp4l[650.630]: foreign master not using PTP timescale
ptp4l[650.630]: running in a temporal vortex
ptp4l[651.020]: master offset 3461 s2 freq +49598 path delay 442913
ptp4l[652.020]: master offset 2104 s2 freq +49280 path delay 442913
On AM625-SK:
root@am62xx-evm:~# ptp4l -E -2 -H -i eth0 -s -l 6 -m -q -f ptp.cfg
ptp4l[618.874]: selected /dev/ptp0 as PTP clock
ptp4l[618.927]: port 1 (eth0): INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[618.927]: port 0 (/var/run/ptp4l): INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[619.431]: port 1: new foreign master b0227a.fffe.d8b7e3-1
ptp4l[623.431]: selected best master clock b0227a.fffe.d8b7e3 on port 1
ptp4l[623.431]: selected best master clock b0227a.fffe.d8b7e3
ptp4l[623.431]: foreign master not using PTP timescale
ptp4l[623.431]: running in a temporal vortex
ptp4l[623.431]: port 1 (eth0): LISTENING to UNCALIBRATED on RS_SLAVE
ptp4l[625.432]: master offset 4167996 s0 freq -15185 path delay 414520
ptp4l[626.432]: master offset 4365478 s1 freq +182227 path delay 414520
ptp4l[627.432]: master offset -235340 s2 freq -53113 path delay 414520
ptp4l[627.432]: port 1 (eth0): UNCALIBRATED to SLAVE on MASTER_CLOCK_SELECTED
ptp4l[628.432]: master offset 33747 s2 freq +145372 path delay 376516
ptp4l[629.432]: master offset -293346 s2 freq -171597 path delay 376516
ptp4l[630.432]: master offset 228692 s2 freq +262438 path delay 338513
ptp4l[631.432]: master offset -192552 s2 freq -90199 path delay 376516
ptp4l[632.433]: master offset 159142 s2 freq +203730 path delay 376516
ptp4l[633.433]: master offset -188770 s2 freq -96440 path delay 414520
ptp4l[634.433]: master offset 176253 s2 freq +211952 path delay 376516
ptp4l[635.433]: master offset -222145 s2 freq -133570 path delay 376516
ptp4l[636.433]: master offset 306349 s2 freq +328281 path delay 298604
ptp4l[637.433]: master offset -247846 s2 freq -134010 path delay 298604
ptp4l[638.433]: master offset 242133 s2 freq +281616 path delay 298604
ptp4l[639.433]: master offset -289587 s2 freq -177465 path delay 298604
ptp4l[640.434]: master offset 291214 s2 freq +316460 path delay 279683
ptp4l[641.434]: master offset -283245 s2 freq -170634 path delay 279683
ptp4l[642.434]: master offset 294661 s2 freq +322298 path delay 256129
ptp4l[643.434]: master offset 31931 s2 freq +147966 path delay 256129
ptp4l[644.434]: master offset -41547 s2 freq +84068 path delay 256129
ptp4l[645.434]: master offset -414538 s2 freq -301387 path delay 256129
ptp4l[646.435]: master offset 299758 s2 freq +288547 path delay 251884
ptp4l[647.434]: master offset -233796 s2 freq -155079 path delay 251884
ptp4l[648.435]: master offset 282743 s2 freq +291321 path delay 268964
ptp4l[649.435]: master offset -296428 s2 freq -203027 path delay 268964
ptp4l[650.435]: master offset 318129 s2 freq +322601 path delay 268964
ptp4l[651.435]: master offset 54329 s2 freq +154240 path delay 276656
ptp4l[652.436]: master offset -40272 s2 freq +75938 path delay 276656
ptp4l[653.436]: master offset -52185 s2 freq +51943 path delay 276656
ptp4l[654.436]: master offset -124449 s2 freq -35976 path delay 361074
ptp4l[655.436]: master offset -90327 s2 freq -39189 path delay 423913
ptp4l[656.436]: master offset 8536 s2 freq +32576 path delay 423913
ptp4l[657.436]: master offset 37342 s2 freq +63943 path delay 423175
ptp4l[658.436]: master offset 15742 s2 freq +53545 path delay 444110
ptp4l[659.436]: master offset 27596 s2 freq +70122 path delay 444110
ptp4l[660.436]: master offset 13826 s2 freq +64631 path delay 446241
ptp4l[661.437]: master offset 10467 s2 freq +65419 path delay 446241
ptp4l[662.437]: master offset 11032 s2 freq +69124 path delay 446241
ptp4l[663.437]: master offset -3933 s2 freq +57469 path delay 446241
ptp4l[664.437]: master offset 735 s2 freq +60957 path delay 444278
3.2.2.10.3.3.2.1.4.2. AM625-SK as transparent clock, PC as master clock and J7VCL as slave clock
Switch mode is enabled on AM625-SK, with the CPSW3G ports in RGMII mode acting as switch ports. A PC (Personal Computer) with Software Timestamping capability is used (PC with Hardware Timestamping capability or another board is preferred) as the master clock. The setup is as follows:
PC is connected to eth0 of AM625-SK’s CPSW3G ports while J7VCL’s eth1 is connected to AM625-SK’s eth1.
Steps:
Enable switch mode on AM625-SK by running the following commands:
devlink dev param set platform/8000000.ethernet name switch_mode value true cmode runtime
ip link add name br0 type bridge
ip link set dev br0 type bridge ageing_time 1000
ip link set dev eth0 up
ip link set dev eth1 up
ip link set dev eth0 master br0
ip link set dev eth1 master br0
ip link set dev br0 up
ip link set dev br0 type bridge vlan_filtering 1
bridge vlan add dev br0 vid 1 self
bridge vlan add dev br0 vid 1 pvid untagged self
# Ensure that multicast flooding is off
bridge link set dev eth0 mcast_flood off
bridge link set dev eth1 mcast_flood off
On the PC, create the same ptp.cfg file mentioned earlier and run:
sudo ptp4l -E -2 -S -i enp2s0 -l 6 -m -q -f ptp.cfg
enp2s0 is assumed to be the ethernet interface. Replace -S with -H if PC supports Hardware Timestamping.
On AM625-SK, run:
ptp4l -E -2 -H -i eth0 -i eth1 -s -f tc-ptp.cfg --step_threshold=1 -m -q
On J7VCL, run:
ptp4l -E -2 -H -i eth1 -s -l 6 -m -q -f ptp.cfg
Observed Outputs:
On PC:
user@pc:~/TSN-PTP4L$ sudo ptp4l -E -2 -S -i enp2s0 -l 6 -m -q -f ptp.cfg
ptp4l[18640.121]: port 1: INITIALIZING to LISTENING on INITIALIZE
ptp4l[18640.121]: port 0: INITIALIZING to LISTENING on INITIALIZE
ptp4l[18640.122]: port 1: link up
ptp4l[18647.795]: port 1: LISTENING to MASTER on ANNOUNCE_RECEIPT_TIMEOUT_EXPIRES
ptp4l[18647.795]: selected best master clock b0227a.fffe.d8b7e3
ptp4l[18647.796]: assuming the grand master role
On AM625-SK:
root@am62xx-evm:~# ptp4l -E -2 -H -i eth0 -i eth1 -s -f ptp.cfg --step_threshold=1 -m -q
ptp4l[508.734]: selected /dev/ptp0 as PTP clock
ptp4l[508.768]: port 1 (eth0): INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[508.808]: port 2 (eth1): INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[508.808]: port 0 (/var/run/ptp4l): INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[510.134]: port 1: new foreign master b0227a.fffe.d8b7e3-1
ptp4l[514.135]: selected best master clock b0227a.fffe.d8b7e3 on port 1
ptp4l[514.135]: selected best master clock b0227a.fffe.d8b7e3
ptp4l[514.135]: foreign master not using PTP timescale
ptp4l[514.135]: port 1 (eth0): LISTENING to UNCALIBRATED on RS_SLAVE
ptp4l[515.135]: master offset -1660108720858304691 s0 freq +0 path delay 145597
ptp4l[515.404]: selected best master clock b0227a.fffe.d8b7e3 on port 1
ptp4l[515.404]: selected best master clock b0227a.fffe.d8b7e3
ptp4l[515.404]: foreign master not using PTP timescale
ptp4l[516.135]: master offset -1660108720858311656 s1 freq -6965 path delay 145597
ptp4l[517.135]: master offset -2379 s2 freq -9344 path delay 145597
ptp4l[517.135]: port 1 (eth0): UNCALIBRATED to SLAVE on MASTER_CLOCK_SELECTED
ptp4l[518.136]: master offset -12603 s2 freq -20282 path delay 145597
ptp4l[519.136]: master offset 49256 s2 freq +37796 path delay 110374
ptp4l[520.136]: master offset -59315 s2 freq -55998 path delay 173739
ptp4l[521.136]: master offset -9282 s2 freq -23759 path delay 173739
ptp4l[522.136]: master offset -34935 s2 freq -52197 path delay 215742
ptp4l[523.136]: master offset 59415 s2 freq +31673 path delay 167165
ptp4l[523.222]: selected best master clock b0227a.fffe.d8b7e3 on port 1
ptp4l[523.222]: selected best master clock b0227a.fffe.d8b7e3
ptp4l[523.222]: foreign master not using PTP timescale
ptp4l[524.136]: master offset 69431 s2 freq +59513 path delay 118589
ptp4l[525.136]: master offset -34194 s2 freq -23283 path delay 156913
ptp4l[526.136]: master offset -56535 s2 freq -55882 path delay 195237
ptp4l[527.137]: master offset 24678 s2 freq +8371 path delay 163169
ptp4l[528.137]: master offset 9448 s2 freq +544 path delay 163169
ptp4l[529.137]: master offset 25778 s2 freq +19708 path delay 139827
ptp4l[529.242]: selected best master clock b0227a.fffe.d8b7e3 on port 1
ptp4l[529.242]: selected best master clock b0227a.fffe.d8b7e3
ptp4l[529.242]: foreign master not using PTP timescale
ptp4l[530.137]: master offset 3067 s2 freq +4731 path delay 135917
ptp4l[531.137]: master offset -8098 s2 freq -5514 path delay 135917
ptp4l[532.137]: master offset -18361 s2 freq -18206 path delay 144642
ptp4l[533.138]: master offset -6540 s2 freq -11894 path delay 144642
ptp4l[534.137]: master offset -1649 s2 freq -8965 path delay 144642
ptp4l[535.138]: master offset -13636 s2 freq -21446 path delay 159134
ptp4l[536.138]: master offset 789 s2 freq -11112 path delay 159134
ptp4l[536.208]: selected best master clock b0227a.fffe.d8b7e3 on port 1
ptp4l[536.208]: selected best master clock b0227a.fffe.d8b7e3
ptp4l[536.208]: foreign master not using PTP timescale
On J7VCL:
root@j7200-evm:~/PTP# ptp4l -E -2 -H -i eth1 -s -l 6 -m -q -f ptp.cfg
ptp4l[425.608]: selected /dev/ptp2 as PTP clock
ptp4l[425.677]: port 1 (eth1): INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[425.677]: port 0 (/var/run/ptp4l): INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[425.705]: port 1: new foreign master b0227a.fffe.d8b7e3-1
ptp4l[429.705]: selected best master clock b0227a.fffe.d8b7e3 on port 1
ptp4l[429.705]: selected best master clock b0227a.fffe.d8b7e3
ptp4l[429.705]: foreign master not using PTP timescale
ptp4l[429.705]: port 1 (eth1): LISTENING to UNCALIBRATED on RS_SLAVE
ptp4l[431.706]: master offset -1660108807288380986 s0 freq +0 path delay 168950
ptp4l[432.706]: master offset -1660108807288385730 s1 freq -4743 path delay 168950
ptp4l[433.706]: master offset -18439 s2 freq -23182 path delay 168950
ptp4l[433.706]: port 1 (eth1): UNCALIBRATED to SLAVE on MASTER_CLOCK_SELECTED
ptp4l[434.706]: master offset -12324 s2 freq -22598 path delay 168950
ptp4l[435.706]: master offset -36594 s2 freq -50565 path delay 197305
ptp4l[436.706]: master offset -17848 s2 freq -42798 path delay 211592
ptp4l[437.706]: master offset 6950 s2 freq -23354 path delay 211592
ptp4l[438.706]: master offset 34748 s2 freq +6529 path delay 190271
ptp4l[439.706]: master offset 9819 s2 freq -7976 path delay 190271
ptp4l[440.707]: master offset -12612 s2 freq -27461 path delay 202810
ptp4l[441.706]: master offset -6574 s2 freq -25207 path delay 206237
ptp4l[442.707]: master offset 4474 s2 freq -16131 path delay 202810
ptp4l[443.707]: master offset 18718 s2 freq -545 path delay 186632
ptp4l[444.707]: master offset -7992 s2 freq -21639 path delay 196330
ptp4l[445.707]: master offset -4577 s2 freq -20622 path delay 196330
ptp4l[446.707]: master offset -1473 s2 freq -18891 path delay 196330
ptp4l[447.707]: master offset 15459 s2 freq -2401 path delay 180152
ptp4l[448.707]: master offset 256 s2 freq -12966 path delay 180152
ptp4l[449.707]: master offset -4951 s2 freq -18096 path delay 180152