3.2.2.4. Crypto
Introduction
The Crypto API Driver is a set of Linux drivers that provide access to the hardware cryptographic accelerators available on AM335x/AM437x/AM57x/DRA7/AM65/J721E/J721S2/J784S4/AM62 devices. These drivers are available built-in in the kernel in the current SDK release.
Following are the Hardware accelerators supported on the following devices:
* AM335X : MD5, SHA1, SHA224, SHA256, AES, DES
* AM437X : MD5, SHA1, SAH224, SHA256, SHA384, SHA512, AES, DES, DES3DES
* AM57x/DRA7 : AES, DES, DES3DES
* AM65x/J721e : AES, DES3DES, SHA1, SHA256, SHA512
* J721S2/J784S4 : AES, DES3DES, SHA1, SHA256, SHA512
* AM64X/AM62X/J722S : AES, SHA256, SHA512
Building the Drivers
For devices with available cryptographic hardware accelerators, a Linux driver and additionally a Cryptodev kernel module (for OpenSSL) is used to access them. Other devices use the pure software implementation of these cryptographic operations.
TDA4VM SoCs support a hardware accelerator called Security Accelerator 2/3 Ultra Light (SA2UL/SA3UL) for crypto operations.
The kernel configuration has already been set up in the SDK and no further configuration is needed for the drivers to be built-in to the kernel.
For reference, the configuration details are shown below. The configuration of the cryptographic drivers is done under the Hardware crypto devices sub-menu of the Cryptographic API menu in the kernel configuration.
Symbol: CRYPTO_DEV_SA2UL [=m]
¦ Type : tristate
¦ Prompt: Support for TI security accelerator
¦ Location:
¦ -> Cryptographic API (CRYPTO [=y])
¦ (1) -> Hardware crypto devices (CRYPTO_HW [=y])
To check if sa2ul module is properly installed, run the below command from the Linux command prompt:
lsmod | grep sa2ul
Output should show something similar to below:
sa2ul 262144 0
Build the Cryptodev kernel module using SDK
For using OpenSSL to access the Crypto Hardware Accelerator Drivers above, the Cryptodev is required (can be built as module). The framework is not officially in the kernel and was ported to Linux under the name “cryptodev”. It is built as part of the SDK and no further configuration is needed.
Using Cryptographic Hardware Accelerators from OpenSSL
In order to use these drivers from OpenSSL, a special driver is available which abstracts the access to these accelerators through Cryprodev module.
Cryptodev is itself a special device driver which provides a general interface for higher level applications such as OpenSSL to access hardware accelerators.
The filesystem which comes with the SDK comes built with the Cryptodev kernel modules and the TI driver which directly accesses the hardware accelerators is built into the kernel.
The following shows the command used to query the system for the state of the cryptodev module.
root@evm:~# lsmod | grep cryptodev cryptodev 11962 0
The following example demonstrates the OpenSSL built-in speed test to demonstrate performance. The addition of the parameter -engine devcrypto tells OpenSSL to use the Cryptodev driver if it exists.
root@evm:~# openssl speed -evp aes-128-cbc -engine devcrypto
engine "devcrypto" set.
Doing aes-128-cbc for 3s on 16 size blocks: 108107 aes-128-cbc's in 0.16s
Doing aes-128-cbc for 3s on 64 size blocks: 103730 aes-128-cbc's in 0.20s
Doing aes-128-cbc for 3s on 256 size blocks: 15181 aes-128-cbc's in 0.03s
Doing aes-128-cbc for 3s on 1024 size blocks: 15879 aes-128-cbc's in 0.03s
Doing aes-128-cbc for 3s on 8192 size blocks: 4879 aes-128-cbc's in 0.02s
OpenSSL 1.0.0b 16 Nov 2010
built on: Thu Jan 20 10:23:44 CST 2011
options:bn(64,32) rc4(ptr,int) des(idx,risc1,2,long) aes(partial) idea(int) blowfish(idx)
compiler: arm-none-linux-gnueabi-gcc -march=armv7-a -mtune=cortex-a8 -mfpu=neon -mfloat-abi=softfp -mthumb-interwork -mno-thumb -fPS
The 'numbers' are in 1000s of bytes per second processed.
type 16 bytes 64 bytes 256 bytes 1024 bytes 8192 bytes
aes-128-cbc 10810.70k 33193.60k 129544.53k 542003.20k 1998438.40k
root@evm:~#
Using the Linux time -v function gives more information about CPU usage during the test.
root@evm:~# time -v openssl speed -evp aes-128-cbc -engine devcrypto
engine "devcrypto" set.
Doing aes-128-cbc for 3s on 16 size blocks: 108799 aes-128-cbc's in 0.17s
Doing aes-128-cbc for 3s on 64 size blocks: 102699 aes-128-cbc's in 0.18s
Doing aes-128-cbc for 3s on 256 size blocks: 16166 aes-128-cbc's in 0.03s
Doing aes-128-cbc for 3s on 1024 size blocks: 15080 aes-128-cbc's in 0.03s
Doing aes-128-cbc for 3s on 8192 size blocks: 4838 aes-128-cbc's in 0.03s
OpenSSL 1.0.0b 16 Nov 2010
built on: Thu Jan 20 10:23:44 CST 2011
options:bn(64,32) rc4(ptr,int) des(idx,risc1,2,long) aes(partial) idea(int) blowfish(idx)
compiler: arm-none-linux-gnueabi-gcc -march=armv7-a -mtune=cortex-a8 -mfpu=neon -mfloat-abi=softfp -mthumb-interwork -mno-thumb -fPS
The 'numbers' are in 1000s of bytes per second processed.
type 16 bytes 64 bytes 256 bytes 1024 bytes 8192 bytes
aes-128-cbc 10239.91k 36515.20k 137949.87k 514730.67k 1321096.53k
Command being timed: "openssl speed -evp aes-128-cbc -engine devcrypto"
User time (seconds): 0.46
System time (seconds): 5.89
Percent of CPU this job got: 42%
Elapsed (wall clock) time (h:mm:ss or m:ss): 0m 15.06s
Average shared text size (kbytes): 0
Average unshared data size (kbytes): 0
Average stack size (kbytes): 0
Average total size (kbytes): 0
Maximum resident set size (kbytes): 7104
Average resident set size (kbytes): 0
Major (requiring I/O) page faults: 0
Minor (reclaiming a frame) page faults: 479
Voluntary context switches: 36143
Involuntary context switches: 211570
Swaps: 0
File system inputs: 0
File system outputs: 0
Socket messages sent: 0
Socket messages received: 0
Signals delivered: 0
Page size (bytes): 4096
Exit status: 0
When the cryptodev driver is removed, OpenSSL reverts to the software implementation of the crypto algorithm. The performance using the software only implementation can be compared to the previous test.
root@evm:~# modprobe -r cryptodev
root@evm:~# time -v openssl speed -evp aes-128-cbc
Doing aes-128-cbc for 3s on 16 size blocks: 697674 aes-128-cbc's in 2.99s
Doing aes-128-cbc for 3s on 64 size blocks: 187556 aes-128-cbc's in 3.00s
Doing aes-128-cbc for 3s on 256 size blocks: 47922 aes-128-cbc's in 3.00s
Doing aes-128-cbc for 3s on 1024 size blocks: 12049 aes-128-cbc's in 3.00s
Doing aes-128-cbc for 3s on 8192 size blocks: 1509 aes-128-cbc's in 3.00s
OpenSSL 1.0.0b 16 Nov 2010
built on: Thu Jan 20 10:23:44 CST 2011
options:bn(64,32) rc4(ptr,int) des(idx,risc1,2,long) aes(partial) idea(int) blowfish(idx)
compiler: arm-none-linux-gnueabi-gcc -march=armv7-a -mtune=cortex-a8 -mfpu=neon -mfloat-abi=softfp -mthumb-interwork -mno-thumb -fPS
The 'numbers' are in 1000s of bytes per second processed.
type 16 bytes 64 bytes 256 bytes 1024 bytes 8192 bytes
aes-128-cbc 3733.37k 4001.19k 4089.34k 4112.73k 4120.58k
Command being timed: "openssl speed -evp aes-128-cbc"
User time (seconds): 15.03
System time (seconds): 0.00
Percent of CPU this job got: 99%
Elapsed (wall clock) time (h:mm:ss or m:ss): 0m 15.07s
Average shared text size (kbytes): 0
Average unshared data size (kbytes): 0
Average stack size (kbytes): 0
Average total size (kbytes): 0
Maximum resident set size (kbytes): 7216
Average resident set size (kbytes): 0
Major (requiring I/O) page faults: 1
Minor (reclaiming a frame) page faults: 484
Voluntary context switches: 13
Involuntary context switches: 35
Swaps: 0
File system inputs: 0
File system outputs: 0
Socket messages sent: 0
Socket messages received: 0
Signals delivered: 0
Page size (bytes): 4096
Exit status: 0
Using the TRNG Hardware Accelerator
The pre built kernel that come with the SDK already has the TRNG driver built into the kernel. No further configuration is required.
Check that the optee-rng driver is loaded:
root@evm:~# cat /sys/class/misc/hw_random/rng_current
optee-rng
The hwrng device should now show up in the filesystem.
root@evm:~# ls -l /dev/hwrng
crw------- 1 root root 10, 183 Jan 1 2000 /dev/hwrng
Use cat on this device to generate random numbers.
root@evm:~# cat /dev/hwrng | od -x
0000000 b2bd ae08 4477 be48 4836 bf64 5d92 01c9
0000020 0cb6 7ac5 16f9 8616 a483 7dfd 6bf4 3aa5
0000040 d693 db24 d917 5ee7 feb7 34c3 34e9 e7a5
0000060 36b7 ea85 fc17 0e66 555c 0934 7a0c 4c69
0000100 523b 9f21 1546 fddb d58b e5ed 142a 6712
0000120 8d76 8f80 a6d2 30d8 d107 32bc 7f45 f997
0000140 9d5d 0d0c f1f0 64f9 a77f 408f b0c1 f5a0
0000160 39c6 f0ae 4b59 1a76 84a7 a364 8964 f557
root@evm:~#
Test the random number generator on the target.
root@evm:~# cat /dev/hwrng | rngtest -c 1000
rngtest 3
Copyright (c) 2004 by Henrique de Moraes Holschuh
This is free software; see the source for copying conditions. There is NO warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
rngtest: starting FIPS tests...
rngtest: bits received from input: 20000032
rngtest: FIPS 140-2 successes: 999
rngtest: FIPS 140-2 failures: 1
rngtest: FIPS 140-2(2001-10-10) Monobit: 0
rngtest: FIPS 140-2(2001-10-10) Poker: 0
rngtest: FIPS 140-2(2001-10-10) Runs: 1
rngtest: FIPS 140-2(2001-10-10) Long run: 0
rngtest: FIPS 140-2(2001-10-10) Continuous run: 0
rngtest: input channel speed: (min=788.218; avg=4070.983; max=2790178.571)Kibits/s
rngtest: FIPS tests speed: (min=846.755; avg=15388.376; max=21920.595)Kibits/s
rngtest: Program run time: 6072670 microseconds
Note that the results may be slightly different on your system, since, after all, we’re dealing with a random number generator. Any appreciable number of errors typically indicates a bad random number generator.
If you’re satisfied the random number generator is working correctly, you can use rngd (the random number generator daemon) to feed the /dev/random entropy pool.
Hardware Accelerator testing
Testing using the tcrypt module:
# modprobe tcrypt mode=500 sec=1
[ 3006.234145] tcrypt:
[ 3006.234145] testing speed of async ecb(aes) (ecb-aes-sa2ul) encryption
[ 3006.242891] tcrypt: test 0 (128 bit key, 16 byte blocks): 87335 operations in 1 seconds (1397360 bytes)
[ 3007.251651] tcrypt: test 1 (128 bit key, 64 byte blocks): 87669 operations in 1 seconds (5610816 bytes)
[ 3008.259651] tcrypt: test 2 (128 bit key, 256 byte blocks): 87481 operations in 1 seconds (22395136 bytes)
[ 3009.267828] tcrypt: test 3 (128 bit key, 1024 byte blocks): 58076 operations in 1 seconds (59469824 bytes)
[ 3010.275914] tcrypt: test 4 (128 bit key, 8192 byte blocks): 22556 operations in 1 seconds (184778752 bytes)
[ 3011.284006] tcrypt: test 5 (192 bit key, 16 byte blocks): 80305 operations in 1 seconds (1284880 bytes)
[ 3012.291648] tcrypt: test 6 (192 bit key, 64 byte blocks): 84537 operations in 1 seconds (5410368 bytes)
[ 3013.299648] tcrypt: test 7 (192 bit key, 256 byte blocks): 90540 operations in 1 seconds (23178240 bytes)
[ 3014.307834] tcrypt: test 8 (192 bit key, 1024 byte blocks): 56054 operations in 1 seconds (57399296 bytes)
[ 3015.315915] tcrypt: test 9 (192 bit key, 8192 byte blocks): 20701 operations in 1 seconds (169582592 bytes)
[ 3016.324006] tcrypt: test 10 (256 bit key, 16 byte blocks): 81816 operations in 1 seconds (1309056 bytes)
[ 3017.331736] tcrypt: test 11 (256 bit key, 64 byte blocks): 82418 operations in 1 seconds (5274752 bytes)
[ 3018.339739] tcrypt: test 12 (256 bit key, 256 byte blocks): 87217 operations in 1 seconds (22327552 bytes)
[ 3019.347917] tcrypt: test 13 (256 bit key, 1024 byte blocks): 56534 operations in 1 seconds (57890816 bytes)
[ 3020.356012] tcrypt: test 14 (256 bit key, 8192 byte blocks): 20428 operations in 1 seconds (167346176 bytes)
[ 3021.364131] tcrypt:
[ 3021.364131] testing speed of async ecb(aes) (ecb-aes-sa2ul) decryption
[ 3021.373505] tcrypt: test 0 (128 bit key, 16 byte blocks): 81655 operations in 1 seconds (1306480 bytes)
[ 3022.379660] tcrypt: test 1 (128 bit key, 64 byte blocks): 87373 operations in 1 seconds (5591872 bytes)
[ 3023.387659] tcrypt: test 2 (128 bit key, 256 byte blocks): 81323 operations in 1 seconds (20818688 bytes)
[ 3024.395825] tcrypt: test 3 (128 bit key, 1024 byte blocks): 58990 operations in 1 seconds (60405760 bytes)
[ 3025.403928] tcrypt: test 4 (128 bit key, 8192 byte blocks): 22613 operations in 1 seconds (185245696 bytes)
[ 3026.411996] tcrypt: test 5 (192 bit key, 16 byte blocks): 79558 operations in 1 seconds (1272928 bytes)
[ 3027.419648] tcrypt: test 6 (192 bit key, 64 byte blocks): 86877 operations in 1 seconds (5560128 bytes)
[ 3028.427648] tcrypt: test 7 (192 bit key, 256 byte blocks): 80615 operations in 1 seconds (20637440 bytes)
[ 3029.435831] tcrypt: test 8 (192 bit key, 1024 byte blocks): 62007 operations in 1 seconds (63495168 bytes)
[ 3030.443907] tcrypt: test 9 (192 bit key, 8192 byte blocks): 21569 operations in 1 seconds (176693248 bytes)
[ 3031.452015] tcrypt: test 10 (256 bit key, 16 byte blocks): 86171 operations in 1 seconds (1378736 bytes)
[ 3032.459743] tcrypt: test 11 (256 bit key, 64 byte blocks): 79752 operations in 1 seconds (5104128 bytes)
[ 3033.467770] tcrypt: test 12 (256 bit key, 256 byte blocks): 84351 operations in 1 seconds (21593856 bytes)
[ 3034.475919] tcrypt: test 13 (256 bit key, 1024 byte blocks): 57082 operations in 1 seconds (58451968 bytes)
[ 3035.483995] tcrypt: test 14 (256 bit key, 8192 byte blocks): 20489 operations in 1 seconds (167845888 bytes)
[ 3036.492101] tcrypt:
...
IPSec Testing:
Server side
# iperf3 --server
Accepted connection from 192.168.1.1, port 41266
[ 5] local 192.168.1.1 port 5201 connected to 192.168.1.2 port 58177
[ ID] Interval Transfer Bandwidth Jitter Lost/Total Datagrams
[ 5] 0.00-1.00 sec 45.6 MBytes 382 Mbits/sec 0.021 ms 0/33017 (0%)
[ 5] 1.00-2.00 sec 47.7 MBytes 400 Mbits/sec 0.014 ms 0/34534 (0%)
[ 5] 2.00-3.00 sec 47.7 MBytes 400 Mbits/sec 0.013 ms 0/34527 (0%)
[ 5] 3.00-4.00 sec 47.7 MBytes 400 Mbits/sec 0.037 ms 0/34507 (0%)
[ 5] 4.00-5.00 sec 47.7 MBytes 400 Mbits/sec 0.021 ms 0/34540 (0%)
[ 5] 5.00-6.00 sec 47.7 MBytes 400 Mbits/sec 0.020 ms 0/34537 (0%)
[ 5] 6.00-7.00 sec 47.7 MBytes 400 Mbits/sec 0.013 ms 0/34511 (0%)
[ 5] 7.00-8.00 sec 47.7 MBytes 400 Mbits/sec 0.017 ms 0/34543 (0%)
[ 5] 8.00-9.00 sec 47.7 MBytes 400 Mbits/sec 0.012 ms 0/34518 (0%)
[ 5] 9.00-10.00 sec 47.7 MBytes 400 Mbits/sec 0.022 ms 0/34532 (0%)
[ 5] 10.00-10.04 sec 2.10 MBytes 403 Mbits/sec 0.014 ms 0/1518 (0%)
Client side
# iperf3 -c 192.168.1.1 -u -b 400.0M -t 10
Connecting to host 192.168.1.1, port 5201
[ 5] local 192.168.1.2 port 58177 connected to 192.168.1.1 port 5201
[ ID] Interval Transfer Bitrate Total Datagrams
[ 5] 0.00-1.00 sec 47.7 MBytes 400 Mbits/sec 34510
[ 5] 1.00-2.00 sec 47.7 MBytes 400 Mbits/sec 34531
[ 5] 2.00-3.00 sec ytes 400 Mbits/sec 34530
[ 5] 3.00-4.00 sec 47.7 MBytes 400 Mbits/sec 34531
[ 5] 4.00-5.00 sec 47.7 MBytes 400 Mbits/sec 34530
[ 5] 5.00-6.00 sec 47.7 MBytes 400 Mbits/sec 34530
[ 5] 6.00-7.00 sec 47.7 MBytes 400 Mbits/sec 34531
[ 5] 7.00-8.00 sec 47.7 MBytes 400 Mbits/sec 34530
[ 5] 8.00-9.00 sec 47.7 MBytes 400 Mbits/sec 34530
[ 5] 9.00-10.00 sec 47.7 MBytes 400 Mbits/sec 34531