3.6.7. Vulkan

The Vulkan® libraries are packaged with the Processor SDK Linux AM67A and can be used by graphics stacks such as Qt and GTK. The drivers run on an ARM core and programs the firmware running inside a GPU core with rendering commands submitted by the user applications.

Vulkan® is a relatively new API that focuses on increased verbosity and control over the device as opposed to OpenGL® ES, which was initially intended to abstract common processing functions for developers. As a result, it can be written by hand but it is usually advised to use an existing abstraction framework, such as the previously mentioned GTK or Qt widget based framework.

Like OpenCL™, Vulkan® has an Installable Client Driver (ICD) Loader to allow applications to query and pick the device it deems necessary instead of relying on a predefined mapping between a chosen display and backing vendor acceleration implementation. This means that typically an application that wants to use Vulkan® should link against an ICD loader library instead of directly using a vendor specific library.

A useful tool for debugging Vulkan® ICD Loaders and devices is vulkaninfo. This command, when run without any arguments will present a list of all supported devices, associated parameters, and supported extensions.

For more information about Vulkan® extensions see: