Capture Module Data Structure.
Contains the data objects required to use the tivxHwaCapture node
Data Fields | |
vx_node | node |
vx_user_data_object | config |
tivx_capture_params_t | params |
vx_object_array | raw_image_arr [APP_MODULES_MAX_BUFQ_DEPTH] |
vx_int32 | graph_parameter_index |
vx_int32 | en_out_capture_write |
vx_int32 | test_mode |
vx_node | write_node |
vx_array | file_path |
vx_array | file_prefix |
vx_user_data_object | write_cmd |
vx_char | output_file_path [TIVX_FILEIO_FILE_PATH_LENGTH] |
vx_char | objName [APP_MODULES_MAX_OBJ_NAME_SIZE] |
tivx_raw_image | error_frame_raw_image |
vx_uint8 | enable_error_detection |
vx_uint32 | capture_format |
vx_node CaptureObj::node |
Capture node object
vx_user_data_object CaptureObj::config |
User data object for config parameter, used as node parameter of Capture node
tivx_capture_params_t CaptureObj::params |
Capture node params structure to initialize config object
vx_object_array CaptureObj::raw_image_arr[APP_MODULES_MAX_BUFQ_DEPTH] |
Capture node object array output
vx_int32 CaptureObj::graph_parameter_index |
Capture node graph parameter index
vx_int32 CaptureObj::en_out_capture_write |
Flag to indicate whether or not the intermediate output is written
vx_int32 CaptureObj::test_mode |
Flag to enable test mode
vx_node CaptureObj::write_node |
Node used to write capture output
vx_array CaptureObj::file_path |
File path used to write capture node output
vx_array CaptureObj::file_prefix |
File path prefix used to write capture node output
vx_user_data_object CaptureObj::write_cmd |
User data object containing write cmd parameters
vx_char CaptureObj::output_file_path[TIVX_FILEIO_FILE_PATH_LENGTH] |
Output file path for capture node output
vx_char CaptureObj::objName[APP_MODULES_MAX_OBJ_NAME_SIZE] |
Name of capture module
tivx_raw_image CaptureObj::error_frame_raw_image |
Raw image used when camera gets disconnected
vx_uint8 CaptureObj::enable_error_detection |
Flag to enable detection of camera disconnection
vx_uint32 CaptureObj::capture_format |
Capture node format, taken from sensor_out_format