This section contains module APIs for the TIOVX Capture node tivxHwaCapture.
|
| vx_status | app_init_capture (vx_context context, CaptureObj *captureObj, SensorObj *sensorObj, char *objName, int32_t bufq_depth) |
| | Capture module init helper function. More...
|
| |
| void | app_deinit_capture (CaptureObj *captureObj, vx_int32 bufq_depth) |
| | Capture module deinit helper function. More...
|
| |
| void | app_delete_capture (CaptureObj *captureObj) |
| | Capture module delete helper function. More...
|
| |
| vx_status | app_create_graph_capture (vx_graph graph, CaptureObj *captureObj) |
| | Capture module create helper function. More...
|
| |
| vx_status | app_create_graph_capture_write_output (vx_graph graph, CaptureObj *captureObj) |
| | Capture module write output helper function. More...
|
| |
| vx_status | app_send_cmd_capture_write_node (CaptureObj *captureObj, vx_uint32 start_frame, vx_uint32 num_frames, vx_uint32 num_skip) |
| | Capture module write output helper function. More...
|
| |
| vx_status | app_send_error_frame (CaptureObj *captureObj) |
| | Capture module write output helper function. More...
|
| |
| tivx_raw_image | read_error_image_raw (vx_context context, IssSensor_Info *sensorInfo, char file_path[], vx_int32 *bytes_read) |
| | Capture module write output helper function. More...
|
| |
|
| #define | NUM_CAPT_CHANNELS (4u) |
| | Number of capture channels that are used by this module. Can be modified as needed. More...
|
| |
◆ NUM_CAPT_CHANNELS
| #define NUM_CAPT_CHANNELS (4u) |
Number of capture channels that are used by this module. Can be modified as needed.
◆ app_init_capture()
| vx_status app_init_capture |
( |
vx_context |
context, |
|
|
CaptureObj * |
captureObj, |
|
|
SensorObj * |
sensorObj, |
|
|
char * |
objName, |
|
|
int32_t |
bufq_depth |
|
) |
| |
Capture module init helper function.
This capture init helper function will create all the data objects required to create the capture node
- Parameters
-
| [in] | context | OpenVX context which must be created using vxCreateContext |
| [out] | captureObj | Capture Module object which gets populated with capture node data objects |
| [in] | sensorObj | Sensor Module object used to initialize capture data object parameters; must be initialized prior to passing to this function |
| [in] | objName | String of the name of this object |
| [in] | bufq_depth | Capture output buffer queue depth |
◆ app_deinit_capture()
| void app_deinit_capture |
( |
CaptureObj * |
captureObj, |
|
|
vx_int32 |
bufq_depth |
|
) |
| |
Capture module deinit helper function.
This capture deinit helper function will release all the data objects created during the app_init_capture call
- Parameters
-
| [in,out] | captureObj | Capture Module object which contains capture node data objects which are released in this function |
| [in] | bufq_depth | Capture output buffer queue depth |
◆ app_delete_capture()
| void app_delete_capture |
( |
CaptureObj * |
captureObj | ) |
|
Capture module delete helper function.
This capture delete helper function will delete the capture node and write node that is created during the app_create_graph_capture call
- Parameters
-
| [in,out] | captureObj | Capture Module object which contains capture node objects which are released in this function |
◆ app_create_graph_capture()
| vx_status app_create_graph_capture |
( |
vx_graph |
graph, |
|
|
CaptureObj * |
captureObj |
|
) |
| |
Capture module create helper function.
This capture create helper function will create the node using all the data objects created during the app_init_capture call. Internally calls app_create_graph_capture_write_output if en_out_capture_write is set
- Parameters
-
| [in] | graph | OpenVX graph that has been created using vxCreateGraph and where the capture node is created |
| [in,out] | captureObj | Capture Module object which contains capture node and write node which are created in this function |
◆ app_create_graph_capture_write_output()
| vx_status app_create_graph_capture_write_output |
( |
vx_graph |
graph, |
|
|
CaptureObj * |
captureObj |
|
) |
| |
Capture module write output helper function.
This capture create helper function will create the node for writing the capture output
- Parameters
-
| [in] | graph | OpenVX graph |
| [in,out] | captureObj | Capture Module object which contains capture node and write node which are created in this function |
◆ app_send_cmd_capture_write_node()
| vx_status app_send_cmd_capture_write_node |
( |
CaptureObj * |
captureObj, |
|
|
vx_uint32 |
start_frame, |
|
|
vx_uint32 |
num_frames, |
|
|
vx_uint32 |
num_skip |
|
) |
| |
Capture module write output helper function.
This capture create helper function will create the node for writing the capture output
- Parameters
-
| [in] | captureObj | Capture Module object which contains the write node used in this function |
| [in] | start_frame | Starting frame to write |
| [in] | num_frames | Total number of frames to write |
| [in] | num_skip | Number of capture frames to skip writing |
◆ app_send_error_frame()
| vx_status app_send_error_frame |
( |
CaptureObj * |
captureObj | ) |
|
Capture module write output helper function.
This capture helper function send the blank frame to the capture node over a control command. This frame is used as the output for when a camera is disconnected
- Parameters
-
| [in] | captureObj | Capture Module object which contains the error frame object for using as blank frame |
◆ read_error_image_raw()
| tivx_raw_image read_error_image_raw |
( |
vx_context |
context, |
|
|
IssSensor_Info * |
sensorInfo, |
|
|
char |
file_path[], |
|
|
vx_int32 * |
bytes_read |
|
) |
| |
Capture module write output helper function.
This capture helper function takes a raw_image that is unpopulated and populates it with the provided path
- Parameters
-
| [in] | context | OpenVX context which must be created using vxCreateContext |
| [in] | sensorInfo | Capture sensor information |
| [in] | file_path | Path to image |
| [out] | bytes_read | Number of bytes read from file |