Kernel for elementwise inverse hyperbolic tangent of an input vector. Supports float datatype.
|
| template<typename T > |
| MATHLIB_STATUS | MATHLIB_atanh (size_t length, T *pSrc, T *pDst) |
| | Performs the elementwise inverse hyperbolic tangent of an input vector. Function can be overloaded with float pointers, and the appropriate precision is employed to compute elementwise inverse hyperbolic tangent of the input vector. More...
|
| |
| MATHLIB_STATUS | MATHLIB_atanh_sp (size_t length, float *pSrc, float *pDst) |
| | This function is the C interface for MATHLIB_log10. Function accepts float pointers. More...
|
| |
◆ MATHLIB_atanh()
Performs the elementwise inverse hyperbolic tangent of an input vector. Function can be overloaded with float pointers, and the appropriate precision is employed to compute elementwise inverse hyperbolic tangent of the input vector.
- Template Parameters
-
| T | : implementation datatype |
- Parameters
-
| [in] | length | : length of input vector |
| [in] | pSrc | : pointer to buffer holding input vector |
| [out] | pDst | : pointer to buffer holding result vector |
- Returns
- Status of success.
◆ MATHLIB_atanh_sp()
| MATHLIB_STATUS MATHLIB_atanh_sp |
( |
size_t |
length, |
|
|
float * |
pSrc, |
|
|
float * |
pDst |
|
) |
| |
This function is the C interface for MATHLIB_log10. Function accepts float pointers.
- Template Parameters
-
| T | : implementation datatype |
- Parameters
-
| [in] | length | : length of input vector |
| [in] | pSrc | : pointer to buffer holding input vector |
| [out] | pDst | : pointer to buffer holding result vector |
- Returns
- Status of success.
Definition at line 439 of file MATHLIB_atanh.cpp.