MATHLIB User Guide
MATHLIB_log10

Introduction

Kernel for elementwise log base 10 of an input vector. Supports float and double datatype.

Functions

template<typename T >
MATHLIB_STATUS MATHLIB_log10 (size_t length, T *pSrc, T *pDst)
 Performs the elementwise log base 10 of an input vector. Function can be overloaded with float and double pointers, and the appropriate precision is employed to compute elementwise log base 10 of the input vector. More...
 
MATHLIB_STATUS MATHLIB_log10_sp (size_t length, float *pSrc, float *pDst)
 This function is the C interface for MATHLIB_log10. Function accepts float pointers. More...
 
MATHLIB_STATUS MATHLIB_log10_dp (size_t length, double *pSrc, double *pDst)
 This function is the C interface for MATHLIB_log10. Function accepts double pointers. More...
 

Function Documentation

◆ MATHLIB_log10()

template<typename T >
MATHLIB_STATUS MATHLIB_log10 ( size_t  length,
T *  pSrc,
T *  pDst 
)

Performs the elementwise log base 10 of an input vector. Function can be overloaded with float and double pointers, and the appropriate precision is employed to compute elementwise log base 10 of the input vector.

Template Parameters
T: implementation datatype
Parameters
[in]length: length of input vector
[in]pSrc: pointer to buffer holding input vector
[out]pDst: pointer to buffer holding result vector
Returns
Status of success.
Remarks
None

◆ MATHLIB_log10_sp()

MATHLIB_STATUS MATHLIB_log10_sp ( size_t  length,
float *  pSrc,
float *  pDst 
)

This function is the C interface for MATHLIB_log10. Function accepts float pointers.

Template Parameters
T: implementation datatype
Parameters
[in]length: length of input vector
[in]pSrc: pointer to buffer holding input vector
[out]pDst: pointer to buffer holding result vector
Returns
Status of success.
Remarks
None

Definition at line 604 of file MATHLIB_log10.cpp.

◆ MATHLIB_log10_dp()

MATHLIB_STATUS MATHLIB_log10_dp ( size_t  length,
double *  pSrc,
double *  pDst 
)

This function is the C interface for MATHLIB_log10. Function accepts double pointers.

Template Parameters
T: implementation datatype
Parameters
[in]length: length of input vector
[in]pSrc: pointer to buffer holding input vector
[out]pDst: pointer to buffer holding result vector
Returns
Status of success.
Remarks
None

Definition at line 611 of file MATHLIB_log10.cpp.