DSPLIB User Guide
DSPLIB_mat_submat_copy.h File Reference

Go to the source code of this file.

Data Structures

struct  DSPLIB_mat_submat_copyInitArgs
 Structure containing the parameters to initialize the kernel. More...
 

Functions

int32_t DSPLIB_mat_submat_copy_getHandleSize (DSPLIB_mat_submat_copyInitArgs *pKerInitArgs)
 This is a query function to calculate the size of internal handle. More...
 
DSPLIB_STATUS DSPLIB_mat_submat_copy_init (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsX, DSPLIB_bufParams2D_t *bufParamsY, const DSPLIB_mat_submat_copyInitArgs *pKerInitArgs)
 This function should be called before the DSPLIB_mat_submat_copy_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the streaming engine and streaming address generator. The results of these operations are stored in the handle. More...
 
DSPLIB_STATUS DSPLIB_mat_submat_copy_init_checkParams (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsX, const DSPLIB_bufParams2D_t *bufParamsY, const DSPLIB_mat_submat_copyInitArgs *pKerInitArgs)
 This function checks the validity of the parameters passed to DSPLIB_mat_submat_copy_init function. This function is called with the same parameters as the DSPLIB_mat_submat_copy_init, and this function must be called before the DSPLIB_mat_submat_copy_init is called. More...
 
DSPLIB_STATUS DSPLIB_mat_submat_copy_exec_checkParams (DSPLIB_kernelHandle handle, const void *restrict pX, const void *restrict pY)
 This function checks the validity of the parameters passed to DSPLIB_mat_submat_copy_exec function. This function is called with the same parameters as the DSPLIB_mat_submat_copy_exec, and this function must be called before the DSPLIB_mat_submat_copy_exec is called. More...
 
DSPLIB_STATUS DSPLIB_mat_submat_copy_exec (DSPLIB_kernelHandle handle, void *restrict pX, void *restrict pY)
 This function is the main kernel compute function. More...