DSPLIB User Guide
DSPLIB_mat_submat_copy

Introduction

Kernel for sub matrix copy.

Data Structures

struct  DSPLIB_mat_submat_copyInitArgs
 Structure containing the parameters to initialize the kernel. More...
 

Functions

int32_t DSPLIB_mat_submat_copy_getHandleSize (DSPLIB_mat_submat_copyInitArgs *pKerInitArgs)
 This is a query function to calculate the size of internal handle. More...
 
DSPLIB_STATUS DSPLIB_mat_submat_copy_init (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsX, DSPLIB_bufParams2D_t *bufParamsY, const DSPLIB_mat_submat_copyInitArgs *pKerInitArgs)
 This function should be called before the DSPLIB_mat_submat_copy_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the streaming engine and streaming address generator. The results of these operations are stored in the handle. More...
 
DSPLIB_STATUS DSPLIB_mat_submat_copy_init_checkParams (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsX, const DSPLIB_bufParams2D_t *bufParamsY, const DSPLIB_mat_submat_copyInitArgs *pKerInitArgs)
 This function checks the validity of the parameters passed to DSPLIB_mat_submat_copy_init function. This function is called with the same parameters as the DSPLIB_mat_submat_copy_init, and this function must be called before the DSPLIB_mat_submat_copy_init is called. More...
 
DSPLIB_STATUS DSPLIB_mat_submat_copy_exec_checkParams (DSPLIB_kernelHandle handle, const void *restrict pX, const void *restrict pY)
 This function checks the validity of the parameters passed to DSPLIB_mat_submat_copy_exec function. This function is called with the same parameters as the DSPLIB_mat_submat_copy_exec, and this function must be called before the DSPLIB_mat_submat_copy_exec is called. More...
 
DSPLIB_STATUS DSPLIB_mat_submat_copy_exec (DSPLIB_kernelHandle handle, void *restrict pX, void *restrict pY)
 This function is the main kernel compute function. More...
 

Function Documentation

◆ DSPLIB_mat_submat_copy_getHandleSize()

int32_t DSPLIB_mat_submat_copy_getHandleSize ( DSPLIB_mat_submat_copyInitArgs pKerInitArgs)

This is a query function to calculate the size of internal handle.

Parameters
[in]pKerInitArgs: Pointer to structure holding init parameters
Returns
Size of the buffer in bytes
Remarks
Application is expected to allocate buffer of the requested size and provide it as input to other functions requiring it.

Definition at line 25 of file DSPLIB_mat_submat_copy.cpp.

◆ DSPLIB_mat_submat_copy_init()

DSPLIB_STATUS DSPLIB_mat_submat_copy_init ( DSPLIB_kernelHandle  handle,
DSPLIB_bufParams2D_t bufParamsX,
DSPLIB_bufParams2D_t bufParamsY,
const DSPLIB_mat_submat_copyInitArgs pKerInitArgs 
)

This function should be called before the DSPLIB_mat_submat_copy_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the streaming engine and streaming address generator. The results of these operations are stored in the handle.

Parameters
[in]handle: Active handle to the kernel
[in]bufParamsX: Pointer to the structure containing dimensional information of X matrix
[out]bufParamsY: Pointer to the structure containing dimensional information of Y matrix
[in]pKerInitArgs: Pointer to the structure holding init parameters
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.
Remarks
Application is expected to provide a valid handle.

Definition at line 88 of file DSPLIB_mat_submat_copy.cpp.

◆ DSPLIB_mat_submat_copy_init_checkParams()

DSPLIB_STATUS DSPLIB_mat_submat_copy_init_checkParams ( DSPLIB_kernelHandle  handle,
const DSPLIB_bufParams2D_t bufParamsX,
const DSPLIB_bufParams2D_t bufParamsY,
const DSPLIB_mat_submat_copyInitArgs pKerInitArgs 
)

This function checks the validity of the parameters passed to DSPLIB_mat_submat_copy_init function. This function is called with the same parameters as the DSPLIB_mat_submat_copy_init, and this function must be called before the DSPLIB_mat_submat_copy_init is called.

Parameters
[in]handle: Active handle to the kernel
[in]bufParamsX: Pointer to the structure containing dimensional information of X matrix
[out]bufParamsY: Pointer to the structure containing dimensional information of Y matrix
[in]pKerInitArgs: Pointer to the structure holding init parameters
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.
Remarks
None

Definition at line 34 of file DSPLIB_mat_submat_copy.cpp.

◆ DSPLIB_mat_submat_copy_exec_checkParams()

DSPLIB_STATUS DSPLIB_mat_submat_copy_exec_checkParams ( DSPLIB_kernelHandle  handle,
const void *restrict  pX,
const void *restrict  pY 
)

This function checks the validity of the parameters passed to DSPLIB_mat_submat_copy_exec function. This function is called with the same parameters as the DSPLIB_mat_submat_copy_exec, and this function must be called before the DSPLIB_mat_submat_copy_exec is called.

Parameters
[in]handle: Active handle to the kernel
[in]pX: Pointer to buffer holding the X matrix
[out]pY: Pointer to buffer holding the Y matrix
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.
Remarks
None

Definition at line 71 of file DSPLIB_mat_submat_copy.cpp.

◆ DSPLIB_mat_submat_copy_exec()

DSPLIB_STATUS DSPLIB_mat_submat_copy_exec ( DSPLIB_kernelHandle  handle,
void *restrict  pX,
void *restrict  pY 
)

This function is the main kernel compute function.

Please refer to details under DSPLIB_mat_submat_copy_exec

Parameters
[in]handle: Active handle to the kernel
[in]pX: Pointer to buffer holding the X matrix
[out]pY: Pointer to buffer holding the Y matrix
Memory Requirements
Buffer dimY dimX Comments
pX M N X Matrix
pY nRows nCols Y Matrix
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.
Assumptions:
  • None
Performance Considerations:
For best performance,
  • The input and output data buffers are expected to be in L2 memory
  • The buffer pointers are assumed to be 64-byte aligned
  • Ensure that the starting point of adjacent rows in a 2-D matrix are allocated from different banks in L2 memory with the help of memory padding.
Remarks
Before calling this function, application is expected to call DSPLIB_mat_submat_copy_init and DSPLIB_mat_submat_copy_exec_checkParams functions. This ensures resource configuration and error checks are done only once for several invocations of this function.

Definition at line 211 of file DSPLIB_mat_submat_copy.cpp.