CC3200 Peripheral Driver Library User's Guide
1.2.0
|
Data Structures | |
struct | tDMAControlTable |
Functions | |
void | uDMAEnable (void) |
void | uDMADisable (void) |
unsigned long | uDMAErrorStatusGet (void) |
void | uDMAErrorStatusClear (void) |
void | uDMAChannelEnable (unsigned long ulChannelNum) |
void | uDMAChannelDisable (unsigned long ulChannelNum) |
tBoolean | uDMAChannelIsEnabled (unsigned long ulChannelNum) |
void | uDMAControlBaseSet (void *pControlTable) |
void * | uDMAControlBaseGet (void) |
void * | uDMAControlAlternateBaseGet (void) |
void | uDMAChannelRequest (unsigned long ulChannelNum) |
void | uDMAChannelAttributeEnable (unsigned long ulChannelNum, unsigned long ulAttr) |
void | uDMAChannelAttributeDisable (unsigned long ulChannelNum, unsigned long ulAttr) |
unsigned long | uDMAChannelAttributeGet (unsigned long ulChannelNum) |
void | uDMAChannelControlSet (unsigned long ulChannelStructIndex, unsigned long ulControl) |
void | uDMAChannelTransferSet (unsigned long ulChannelStructIndex, unsigned long ulMode, void *pvSrcAddr, void *pvDstAddr, unsigned long ulTransferSize) |
void | uDMAChannelScatterGatherSet (unsigned long ulChannelNum, unsigned ulTaskCount, void *pvTaskList, unsigned long ulIsPeriphSG) |
unsigned long | uDMAChannelSizeGet (unsigned long ulChannelStructIndex) |
unsigned long | uDMAChannelModeGet (unsigned long ulChannelStructIndex) |
void | uDMAIntRegister (unsigned long ulIntChannel, void(*pfnHandler)(void)) |
void | uDMAIntUnregister (unsigned long ulIntChannel) |
unsigned long | uDMAIntStatus (void) |
void | uDMAIntClear (unsigned long ulChanMask) |
void | uDMAChannelAssign (unsigned long ulMapping) |
void uDMAChannelAssign | ( | unsigned long | ulMapping | ) |
Assigns a peripheral mapping for a uDMA channel.
ulMapping | is a macro specifying the peripheral assignment for a channel. |
This function assigns a peripheral mapping to a uDMA channel. It is used to select which peripheral is used for a uDMA channel. The parameter ulMapping should be one of the macros named UDMA_CHn_tttt from the header file udma.h. For example, to assign uDMA channel 0 to the UART2 RX channel, the parameter should be the macro UDMA_CH0_UART2RX.
Please consult the data sheet for a table showing all the possible peripheral assignments for the uDMA channels for a particular device.
void uDMAChannelAttributeDisable | ( | unsigned long | ulChannelNum, |
unsigned long | ulAttr | ||
) |
Disables attributes of a uDMA channel.
ulChannelNum | is the channel to configure. |
ulAttr | is a combination of attributes for the channel. |
This function is used to disable attributes of a uDMA channel.
The ulAttr parameter is the logical OR of any of the following:
void uDMAChannelAttributeEnable | ( | unsigned long | ulChannelNum, |
unsigned long | ulAttr | ||
) |
Enables attributes of a uDMA channel.
ulChannelNum | is the channel to configure. |
ulAttr | is a combination of attributes for the channel. |
This function is used to enable attributes of a uDMA channel.
The ulAttr parameter is the logical OR of any of the following:
unsigned long uDMAChannelAttributeGet | ( | unsigned long | ulChannelNum | ) |
Gets the enabled attributes of a uDMA channel.
ulChannelNum | is the channel to configure. |
This function returns a combination of flags representing the attributes of the uDMA channel.
void uDMAChannelControlSet | ( | unsigned long | ulChannelStructIndex, |
unsigned long | ulControl | ||
) |
Sets the control parameters for a uDMA channel control structure.
ulChannelStructIndex | is the logical OR of the uDMA channel number with UDMA_PRI_SELECT or UDMA_ALT_SELECT. |
ulControl | is logical OR of several control values to set the control parameters for the channel. |
This function is used to set control parameters for a uDMA transfer. These parameters are typically not changed often.
The ulChannelStructIndex parameter should be the logical OR of the channel number with one of UDMA_PRI_SELECT or UDMA_ALT_SELECT to choose whether the primary or alternate data structure is used.
The ulControl parameter is the logical OR of five values: the data size, the source address increment, the destination address increment, the arbitration size, and the use burst flag. The choices available for each of these values is described below.
Choose the data size from one of UDMA_SIZE_8, UDMA_SIZE_16, or UDMA_SIZE_32 to select a data size of 8, 16, or 32 bits.
Choose the source address increment from one of UDMA_SRC_INC_8, UDMA_SRC_INC_16, UDMA_SRC_INC_32, or UDMA_SRC_INC_NONE to select an address increment of 8-bit bytes, 16-bit halfwords, 32-bit words, or to select non-incrementing.
Choose the destination address increment from one of UDMA_DST_INC_8, UDMA_DST_INC_16, UDMA_DST_INC_32, or UDMA_DST_INC_NONE to select an address increment of 8-bit bytes, 16-bit halfwords, 32-bit words, or to select non-incrementing.
The arbitration size determines how many items are transferred before the uDMA controller re-arbitrates for the bus. Choose the arbitration size from one of UDMA_ARB_1, UDMA_ARB_2, UDMA_ARB_4, UDMA_ARB_8, through UDMA_ARB_1024 to select the arbitration size from 1 to 1024 items, in powers of 2.
The value UDMA_NEXT_USEBURST is used to force the channel to only respond to burst requests at the tail end of a scatter-gather transfer.
void uDMAChannelDisable | ( | unsigned long | ulChannelNum | ) |
Disables a uDMA channel for operation.
ulChannelNum | is the channel number to disable. |
This function disables a specific uDMA channel. Once disabled, a channel cannot respond to uDMA transfer requests until re-enabled via uDMAChannelEnable().
void uDMAChannelEnable | ( | unsigned long | ulChannelNum | ) |
Enables a uDMA channel for operation.
ulChannelNum | is the channel number to enable. |
This function enables a specific uDMA channel for use. This function must be used to enable a channel before it can be used to perform a uDMA transfer.
When a uDMA transfer is completed, the channel is automatically disabled by the uDMA controller. Therefore, this function should be called prior to starting up any new transfer.
tBoolean uDMAChannelIsEnabled | ( | unsigned long | ulChannelNum | ) |
Checks if a uDMA channel is enabled for operation.
ulChannelNum | is the channel number to check. |
This function checks to see if a specific uDMA channel is enabled. This function can be used to check the status of a transfer, as the channel is automatically disabled at the end of a transfer.
unsigned long uDMAChannelModeGet | ( | unsigned long | ulChannelStructIndex | ) |
Gets the transfer mode for a uDMA channel control structure.
ulChannelStructIndex | is the logical OR of the uDMA channel number with either UDMA_PRI_SELECT or UDMA_ALT_SELECT. |
This function is used to get the transfer mode for the uDMA channel and to query the status of a transfer on a channel. When the transfer is complete the mode is UDMA_MODE_STOP.
void uDMAChannelRequest | ( | unsigned long | ulChannelNum | ) |
Requests a uDMA channel to start a transfer.
ulChannelNum | is the channel number on which to request a uDMA transfer. |
This function allows software to request a uDMA channel to begin a transfer. This function could be used for performing a memory-to-memory transfer or if for some reason, a transfer needs to be initiated by software instead of the peripheral associated with that channel.
void uDMAChannelScatterGatherSet | ( | unsigned long | ulChannelNum, |
unsigned | ulTaskCount, | ||
void * | pvTaskList, | ||
unsigned long | ulIsPeriphSG | ||
) |
Configures a uDMA channel for scatter-gather mode.
ulChannelNum | is the uDMA channel number. |
ulTaskCount | is the number of scatter-gather tasks to execute. |
pvTaskList | is a pointer to the beginning of the scatter-gather task list. |
ulIsPeriphSG | is a flag to indicate it is a peripheral scatter-gather transfer (else it is memory scatter-gather transfer) |
This function is used to configure a channel for scatter-gather mode. The caller must have already set up a task list and must pass a pointer to the start of the task list as the pvTaskList parameter. The ulTaskCount parameter is the count of tasks in the task list, not the size of the task list. The flag bIsPeriphSG should be used to indicate if scatter-gather should be configured for peripheral or memory operation.
unsigned long uDMAChannelSizeGet | ( | unsigned long | ulChannelStructIndex | ) |
Gets the current transfer size for a uDMA channel control structure.
ulChannelStructIndex | is the logical OR of the uDMA channel number with either UDMA_PRI_SELECT or UDMA_ALT_SELECT. |
This function is used to get the uDMA transfer size for a channel. The transfer size is the number of items to transfer, where the size of an item might be 8, 16, or 32 bits. If a partial transfer has already occurred, then the number of remaining items is returned. If the transfer is complete, then 0 is returned.
void uDMAChannelTransferSet | ( | unsigned long | ulChannelStructIndex, |
unsigned long | ulMode, | ||
void * | pvSrcAddr, | ||
void * | pvDstAddr, | ||
unsigned long | ulTransferSize | ||
) |
Sets the transfer parameters for a uDMA channel control structure.
ulChannelStructIndex | is the logical OR of the uDMA channel number with either UDMA_PRI_SELECT or UDMA_ALT_SELECT. |
ulMode | is the type of uDMA transfer. |
pvSrcAddr | is the source address for the transfer. |
pvDstAddr | is the destination address for the transfer. |
ulTransferSize | is the number of data items to transfer. |
This function is used to configure the parameters for a uDMA transfer. These parameters are typically changed often. The function uDMAChannelControlSet() MUST be called at least once for this channel prior to calling this function.
The ulChannelStructIndex parameter should be the logical OR of the channel number with one of UDMA_PRI_SELECT or UDMA_ALT_SELECT to choose whether the primary or alternate data structure is used.
The ulMode parameter should be one of the following values:
The pvSrcAddr and pvDstAddr parameters are pointers to the first location of the data to be transferred. These addresses should be aligned according to the item size. The compiler takes care of this alignment if the pointers are pointing to storage of the appropriate data type.
The ulTransferSize parameter is the number of data items, not the number of bytes. The value of this parameter should not exceed 1024.
The two scatter-gather modes, memory and peripheral, are actually different depending on whether the primary or alternate control structure is selected. This function looks for the UDMA_PRI_SELECT and UDMA_ALT_SELECT flag along with the channel number and sets the scatter-gather mode as appropriate for the primary or alternate control structure.
The channel must also be enabled using uDMAChannelEnable() after calling this function. The transfer does not begin until the channel has been configured and enabled. Note that the channel is automatically disabled after the transfer is completed, meaning that uDMAChannelEnable() must be called again after setting up the next transfer.
void* uDMAControlAlternateBaseGet | ( | void | ) |
Gets the base address for the channel control table alternate structures.
This function gets the base address of the second half of the channel control table that holds the alternate control structures for each channel.
void* uDMAControlBaseGet | ( | void | ) |
Gets the base address for the channel control table.
This function gets the base address of the channel control table. This table resides in system memory and holds control information for each uDMA channel.
void uDMAControlBaseSet | ( | void * | pControlTable | ) |
Sets the base address for the channel control table.
pControlTable | is a pointer to the 1024-byte-aligned base address of the uDMA channel control table. |
This function configures the base address of the channel control table. This table resides in system memory and holds control information for each uDMA channel. The table must be aligned on a 1024-byte boundary. The base address must be configured before any of the channel functions can be used.
The size of the channel control table depends on the number of uDMA channels and the transfer modes that are used. Refer to the introductory text and the microcontroller datasheet for more information about the channel control table.
void uDMADisable | ( | void | ) |
Disables the uDMA controller for use.
This function disables the uDMA controller. Once disabled, the uDMA controller cannot operate until re-enabled with uDMAEnable().
void uDMAEnable | ( | void | ) |
Enables the uDMA controller for use.
This function enables the uDMA controller. The uDMA controller must be enabled before it can be configured and used.
void uDMAErrorStatusClear | ( | void | ) |
Clears the uDMA error interrupt.
This function clears a pending uDMA error interrupt. This function should be called from within the uDMA error interrupt handler to clear the interrupt.
unsigned long uDMAErrorStatusGet | ( | void | ) |
Gets the uDMA error status.
This function returns the uDMA error status. It should be called from within the uDMA error interrupt handler to determine if a uDMA error occurred.
void uDMAIntClear | ( | unsigned long | ulChanMask | ) |
Clears uDMA interrupt status.
ulChanMask | is a 32-bit mask with one bit for each uDMA channel. |
This function clears bits in the uDMA interrupt status register according to which bits are set in ulChanMask. There is one bit for each channel. If a a bit is set in ulChanMask, then that corresponding channel's interrupt status is cleared (if it was set).
void uDMAIntRegister | ( | unsigned long | ulIntChannel, |
void(*)(void) | pfnHandler | ||
) |
Registers an interrupt handler for the uDMA controller.
ulIntChannel | identifies which uDMA interrupt is to be registered. |
pfnHandler | is a pointer to the function to be called when the interrupt is activated. |
This function registers and enables the handler to be called when the uDMA controller generates an interrupt. The ulIntChannel parameter should be one of the following:
unsigned long uDMAIntStatus | ( | void | ) |
Gets the uDMA controller channel interrupt status.
This function is used to get the interrupt status of the uDMA controller. The returned value is a 32-bit bit mask that indicates which channels are requesting an interrupt. This function can be used from within an interrupt handler to determine or confirm which uDMA channel has requested an interrupt.
void uDMAIntUnregister | ( | unsigned long | ulIntChannel | ) |
Unregisters an interrupt handler for the uDMA controller.
ulIntChannel | identifies which uDMA interrupt to unregister. |
This function disables and unregisters the handler to be called for the specified uDMA interrupt. The ulIntChannel parameter should be one of UDMA_INT_SW or UDMA_INT_ERR as documented for the function uDMAIntRegister().