![]() |
CC3200 Peripheral Driver Library User's Guide
1.2.0
|
Functions | |
| tBoolean | IntMasterEnable (void) |
| tBoolean | IntMasterDisable (void) |
| void | IntVTableBaseSet (unsigned long ulVtableBase) |
| void | IntRegister (unsigned long ulInterrupt, void(*pfnHandler)(void)) |
| void | IntUnregister (unsigned long ulInterrupt) |
| void | IntPriorityGroupingSet (unsigned long ulBits) |
| unsigned long | IntPriorityGroupingGet (void) |
| void | IntPrioritySet (unsigned long ulInterrupt, unsigned char ucPriority) |
| long | IntPriorityGet (unsigned long ulInterrupt) |
| void | IntEnable (unsigned long ulInterrupt) |
| void | IntDisable (unsigned long ulInterrupt) |
| void | IntPendSet (unsigned long ulInterrupt) |
| void | IntPendClear (unsigned long ulInterrupt) |
| void | IntPriorityMaskSet (unsigned long ulPriorityMask) |
| unsigned long | IntPriorityMaskGet (void) |
| void IntDisable | ( | unsigned long | ulInterrupt | ) |
Disables an interrupt.
| ulInterrupt | specifies the interrupt to be disabled. |
The specified interrupt is disabled in the interrupt controller. Other enables for the interrupt (such as at the peripheral level) are unaffected by this function.
| void IntEnable | ( | unsigned long | ulInterrupt | ) |
Enables an interrupt.
| ulInterrupt | specifies the interrupt to be enabled. |
The specified interrupt is enabled in the interrupt controller. Other enables for the interrupt (such as at the peripheral level) are unaffected by this function.
| tBoolean IntMasterDisable | ( | void | ) |
Disables the processor interrupt.
Prevents the processor from receiving interrupts. This does not affect the set of interrupts enabled in the interrupt controller; it just gates the single interrupt from the controller to the processor.
interrupt.h and call this function without having included hw_types.h. Now that the return is a tBoolean, a compiler error will occur in this case. The solution is to include hw_types.h before including interrupt.h.| tBoolean IntMasterEnable | ( | void | ) |
Enables the processor interrupt.
Allows the processor to respond to interrupts. This does not affect the set of interrupts enabled in the interrupt controller; it just gates the single interrupt from the controller to the processor.
interrupt.h and call this function without having included hw_types.h. Now that the return is a tBoolean, a compiler error will occur in this case. The solution is to include hw_types.h before including interrupt.h.| void IntPendClear | ( | unsigned long | ulInterrupt | ) |
Unpends an interrupt.
| ulInterrupt | specifies the interrupt to be unpended. |
The specified interrupt is unpended in the interrupt controller. This will cause any previously generated interrupts that have not been handled yet (due to higher priority interrupts or the interrupt no having been enabled yet) to be discarded.
| void IntPendSet | ( | unsigned long | ulInterrupt | ) |
Pends an interrupt.
| ulInterrupt | specifies the interrupt to be pended. |
The specified interrupt is pended in the interrupt controller. This will cause the interrupt controller to execute the corresponding interrupt handler at the next available time, based on the current interrupt state priorities. For example, if called by a higher priority interrupt handler, the specified interrupt handler will not be called until after the current interrupt handler has completed execution. The interrupt must have been enabled for it to be called.
| long IntPriorityGet | ( | unsigned long | ulInterrupt | ) |
Gets the priority of an interrupt.
| ulInterrupt | specifies the interrupt in question. |
This function gets the priority of an interrupt. See IntPrioritySet() for a definition of the priority value.
| unsigned long IntPriorityGroupingGet | ( | void | ) |
Gets the priority grouping of the interrupt controller.
This function returns the split between preemptable priority levels and subpriority levels in the interrupt priority specification.
| void IntPriorityGroupingSet | ( | unsigned long | ulBits | ) |
Sets the priority grouping of the interrupt controller.
| ulBits | specifies the number of bits of preemptable priority. |
This function specifies the split between preemptable priority levels and subpriority levels in the interrupt priority specification. The range of the grouping values are dependent upon the hardware implementation; on the CC3200 , three bits are available for hardware interrupt prioritization and therefore priority grouping values of three through seven have the same effect.
| unsigned long IntPriorityMaskGet | ( | void | ) |
Gets the priority masking level
This function gets the current setting of the interrupt priority masking level. The value returned is the priority level such that all interrupts of that and lesser priority are masked. A value of 0 means that priority masking is disabled.
Smaller numbers correspond to higher interrupt priorities. So for example a priority level mask of 4 will allow interrupts of priority level 0-3, and interrupts with a numerical priority of 4 and greater will be blocked.
The hardware priority mechanism will only look at the upper N bits of the priority level (where N is 3), so any prioritization must be performed in those bits.
| void IntPriorityMaskSet | ( | unsigned long | ulPriorityMask | ) |
Sets the priority masking level
| ulPriorityMask | is the priority level that will be masked. |
This function sets the interrupt priority masking level so that all interrupts at the specified or lesser priority level is masked. This can be used to globally disable a set of interrupts with priority below a predetermined threshold. A value of 0 disables priority masking.
Smaller numbers correspond to higher interrupt priorities. So for example a priority level mask of 4 will allow interrupts of priority level 0-3, and interrupts with a numerical priority of 4 and greater will be blocked.
The hardware priority mechanism will only look at the upper N bits of the priority level (where N is 3), so any prioritization must be performed in those bits.
| void IntPrioritySet | ( | unsigned long | ulInterrupt, |
| unsigned char | ucPriority | ||
| ) |
Sets the priority of an interrupt.
| ulInterrupt | specifies the interrupt in question. |
| ucPriority | specifies the priority of the interrupt. |
This function is used to set the priority of an interrupt. When multiple interrupts are asserted simultaneously, the ones with the highest priority are processed before the lower priority interrupts. Smaller numbers correspond to higher interrupt priorities; priority 0 is the highest interrupt priority.
The hardware priority mechanism will only look at the upper N bits of the priority level (where N is 3), so any prioritization must be performed in those bits. The remaining bits can be used to sub-prioritize the interrupt sources, and may be used by the hardware priority mechanism on a future part. This arrangement allows priorities to migrate to different NVIC implementations without changing the gross prioritization of the interrupts.
The parameter ucPriority can be any one of the following -INT_PRIORITY_LVL_0 -INT_PRIORITY_LVL_1 -INT_PRIORITY_LVL_2 -INT_PRIORITY_LVL_3 -INT_PRIORITY_LVL_4 -INT_PRIORITY_LVL_5 -INT_PRIORITY_LVL_6 -INT_PRIORITY_LVL_7
| void IntRegister | ( | unsigned long | ulInterrupt, |
| void(*)(void) | pfnHandler | ||
| ) |
Registers a function to be called when an interrupt occurs.
| ulInterrupt | specifies the interrupt in question. |
| pfnHandler | is a pointer to the function to be called. |
This function is used to specify the handler function to be called when the given interrupt is asserted to the processor. When the interrupt occurs, if it is enabled (via IntEnable()), the handler function will be called in interrupt context. Since the handler function can preempt other code, care must be taken to protect memory or peripherals that are accessed by the handler and other non-handler code.
| void IntUnregister | ( | unsigned long | ulInterrupt | ) |
Unregisters the function to be called when an interrupt occurs.
| ulInterrupt | specifies the interrupt in question. |
This function is used to indicate that no handler should be called when the given interrupt is asserted to the processor. The interrupt source will be automatically disabled (via IntDisable()) if necessary.
| void IntVTableBaseSet | ( | unsigned long | ulVtableBase | ) |
Sets the NVIC VTable base.
| ulVtableBase | specifies the new base address of VTable |
This function is used to specify a new base address for the VTable. This function must be called before using IntRegister() for registering any interrupt handler.