![]() |
CC3200 Peripheral Driver Library User's Guide
1.2.0
|
Functions | |
| void | FlashDisable () |
| long | FlashErase (unsigned long ulAddress) |
| void | FlashEraseNonBlocking (unsigned long ulAddress) |
| long | FlashMassErase () |
| void | FlashMassEraseNonBlocking () |
| long | FlashProgram (unsigned long *pulData, unsigned long ulAddress, unsigned long ulCount) |
| long | FlashProgramNonBlocking (unsigned long *pulData, unsigned long ulAddress, unsigned long ulCount) |
| tFlashProtection | FlashProtectGet (unsigned long ulAddress) |
| void | FlashIntRegister (void(*pfnHandler)(void)) |
| void | FlashIntUnregister (void) |
| void | FlashIntEnable (unsigned long ulIntFlags) |
| void | FlashIntDisable (unsigned long ulIntFlags) |
| unsigned long | FlashIntStatus (tBoolean bMasked) |
| void | FlashIntClear (unsigned long ulIntFlags) |
| void FlashDisable | ( | void | ) |
Flash Disable
This function Disables the internal Flash.
| long FlashErase | ( | unsigned long | ulAddress | ) |
Erases a block of flash.
| ulAddress | is the start address of the flash block to be erased. |
This function will erase a 2 kB block of the on-chip flash. After erasing, the block will be filled with 0xFF bytes. Read-only and execute-only blocks cannot be erased.
This function will not return until the block has been erased.
| void FlashEraseNonBlocking | ( | unsigned long | ulAddress | ) |
Erases a block of flash but does not wait for completion.
| ulAddress | is the start address of the flash block to be erased. |
This function will erase a 2 kB block of the on-chip flash. After erasing, the block will be filled with 0xFF bytes. Read-only and execute-only blocks cannot be erased.
This function will return immediately after commanding the erase operation. Applications making use of the function can determine completion state by using a flash interrupt handler or by polling FlashIntStatus.
| void FlashIntClear | ( | unsigned long | ulIntFlags | ) |
Clears flash controller interrupt sources.
| ulIntFlags | is the bit mask of the interrupt sources to be cleared. Can be any of the FLASH_CTRL_PROGRAM or FLASH_CTRL_AMISC values. |
The specified flash controller interrupt sources are cleared, so that they no longer assert. This must be done in the interrupt handler to keep it from being called again immediately upon exit.
| void FlashIntDisable | ( | unsigned long | ulIntFlags | ) |
Disables individual flash controller interrupt sources.
| ulIntFlags | is a bit mask of the interrupt sources to be disabled. Can be any of the FLASH_CTRL_PROGRAM or FLASH_CTRL_ACCESS values. |
Disables the indicated flash controller interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
| void FlashIntEnable | ( | unsigned long | ulIntFlags | ) |
Enables individual flash controller interrupt sources.
| ulIntFlags | is a bit mask of the interrupt sources to be enabled. Can be any of the FLASH_CTRL_PROGRAM or FLASH_CTRL_ACCESS values. |
Enables the indicated flash controller interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
| void FlashIntRegister | ( | void(*)(void) | pfnHandler | ) |
Registers an interrupt handler for the flash interrupt.
| pfnHandler | is a pointer to the function to be called when the flash interrupt occurs. |
This sets the handler to be called when the flash interrupt occurs. The flash controller can generate an interrupt when an invalid flash access occurs, such as trying to program or erase a read-only block, or trying to read from an execute-only block. It can also generate an interrupt when a program or erase operation has completed. The interrupt will be automatically enabled when the handler is registered.
| unsigned long FlashIntStatus | ( | tBoolean | bMasked | ) |
Gets the current interrupt status.
| bMasked | is false if the raw interrupt status is required and true if the masked interrupt status is required. |
This returns the interrupt status for the flash controller. Either the raw interrupt status or the status of interrupts that are allowed to reflect to the processor can be returned.
| void FlashIntUnregister | ( | void | ) |
Unregisters the interrupt handler for the flash interrupt.
This function will clear the handler to be called when the flash interrupt occurs. This will also mask off the interrupt in the interrupt controller so that the interrupt handler is no longer called.
| long FlashMassErase | ( | void | ) |
Erases a complele flash at shot.
This function erases a complele flash at shot
| void FlashMassEraseNonBlocking | ( | void | ) |
Erases a complele flash at shot but does not wait for completion.
This function will not return until the Flash has been erased.
| long FlashProgram | ( | unsigned long * | pulData, |
| unsigned long | ulAddress, | ||
| unsigned long | ulCount | ||
| ) |
Programs flash.
| pulData | is a pointer to the data to be programmed. |
| ulAddress | is the starting address in flash to be programmed. Must be a multiple of four. |
| ulCount | is the number of bytes to be programmed. Must be a multiple of four. |
This function will program a sequence of words into the on-chip flash. Each word in a page of flash can only be programmed one time between an erase of that page; programming a word multiple times will result in an unpredictable value in that word of flash.
Since the flash is programmed one word at a time, the starting address and byte count must both be multiples of four. It is up to the caller to verify the programmed contents, if such verification is required.
This function will not return until the data has been programmed.
| long FlashProgramNonBlocking | ( | unsigned long * | pulData, |
| unsigned long | ulAddress, | ||
| unsigned long | ulCount | ||
| ) |
Programs flash but does not poll for completion.
| pulData | is a pointer to the data to be programmed. |
| ulAddress | is the starting address in flash to be programmed. Must be a multiple of four. |
| ulCount | is the number of bytes to be programmed. Must be a multiple of four. |
This function will start programming one or more words into the on-chip flash and return immediately. The number of words that can be programmed in a single call depends the part on which the function is running. For parts without support for a flash write buffer, only a single word may be programmed on each call to this function (ulCount must be 1). If a write buffer is present, up to 32 words may be programmed on condition that the block being programmed does not straddle a 32 word address boundary. For example, wherease 32 words can be programmed if the address passed is 0x100 (a multiple of 128 bytes or 32 words), only 31 words could be programmed at 0x104 since attempting to write 32 would cross the 32 word boundary at 0x180.
Since the flash is programmed one word at a time, the starting address and byte count must both be multiples of four. It is up to the caller to verify the programmed contents, if such verification is required.
This function will return immediately after commanding the erase operation. Applications making use of the function can determine completion state by using a flash interrupt handler or by polling FlashIntStatus.
| tFlashProtection FlashProtectGet | ( | unsigned long | ulAddress | ) |
Gets the protection setting for a block of flash.
| ulAddress | is the start address of the flash block to be queried. |
This function gets the current protection for the specified 2-kB block of flash. Each block can be read/write, read-only, or execute-only. Read/write blocks can be read, executed, erased, and programmed. Read-only blocks can be read and executed. Execute-only blocks can only be executed; processor and debugger data reads are not allowed.