![]() |
SimpleLink CC3100/CC3200 Host Driver
Version 1.0.1.6
Simplifies the implementation of Internet connectivity
|
Data Fields | |
SlrxFilterHeaderArg_t | RuleHeaderArgs |
SlrxFilterCompareMask_t | RuleHeaderArgsMask [16] |
Definition at line 399 of file wlan_rx_filters.h.
SlrxFilterHeaderArg_t RuleHeaderArgs |
Argument for the comparison function
Definition at line 403 of file wlan_rx_filters.h.
SlrxFilterCompareMask_t RuleHeaderArgsMask[16] |
the mask is used in order to enable partial comparison, Use the 0xFFFFFFFF in case you don't want to use mask
Definition at line 409 of file wlan_rx_filters.h.