Data Structures | Macros | Typedefs | Enumerations
UART2CC32XX.h File Reference

Detailed Description

UART driver implementation for a CC32XX UART controller.

============================================================================

The UART header file should be included in an application as follows:

Refer to UART2.h for a complete description of APIs and examples of use.


#include <stddef.h>
#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/dpl/HwiP.h>
#include <ti/drivers/dpl/SemaphoreP.h>
#include <ti/drivers/power/PowerCC32XX.h>
#include <ti/drivers/UART2.h>
#include <ti/drivers/dma/UDMACC32XX.h>
#include <ti/drivers/Power.h>
Include dependency graph for UART2CC32XX.h:

Go to the source code of this file.

Data Structures

struct  UART2CC32XX_HWAttrs
 UART2CC32XX Hardware attributes. More...
 
struct  UART2CC32XX_Object
 UART2CC32XX Object. More...
 

Macros

#define UART2CC32XX_PIN_UNASSIGNED   0xFFF
 Indicates a pin is not being used. More...
 
#define UART2CC32XX_DMACH_UNASSIGNED   0xFF
 Indicates a DMA channel is not being used. More...
 
#define UART2CC32XX_PIN_01_UART1_TX   0x700
 
#define UART2CC32XX_PIN_02_UART1_RX   0x701
 
#define UART2CC32XX_PIN_03_UART0_TX   0x702
 
#define UART2CC32XX_PIN_04_UART0_RX   0x703
 
#define UART2CC32XX_PIN_07_UART1_TX   0x506
 
#define UART2CC32XX_PIN_08_UART1_RX   0x507
 
#define UART2CC32XX_PIN_16_UART1_TX   0x20F
 
#define UART2CC32XX_PIN_17_UART1_RX   0x210
 
#define UART2CC32XX_PIN_45_UART0_RX   0x92C
 
#define UART2CC32XX_PIN_45_UART1_RX   0x22C
 
#define UART2CC32XX_PIN_53_UART0_TX   0x934
 
#define UART2CC32XX_PIN_55_UART0_TX   0x336
 
#define UART2CC32XX_PIN_55_UART1_TX   0x636
 
#define UART2CC32XX_PIN_57_UART0_RX   0x338
 
#define UART2CC32XX_PIN_57_UART1_RX   0x638
 
#define UART2CC32XX_PIN_58_UART1_TX   0x639
 
#define UART2CC32XX_PIN_59_UART1_RX   0x63A
 
#define UART2CC32XX_PIN_62_UART0_TX   0xB3D
 
#define UART2CC32XX_PIN_50_UART0_CTS   0xC31
 
#define UART2CC32XX_PIN_50_UART0_RTS   0x331
 
#define UART2CC32XX_PIN_50_UART1_RTS   0xA31
 
#define UART2CC32XX_PIN_52_UART0_RTS   0x633
 
#define UART2CC32XX_PIN_61_UART0_RTS   0x53C
 
#define UART2CC32XX_PIN_61_UART0_CTS   0x63C
 
#define UART2CC32XX_PIN_61_UART1_CTS   0x33C
 
#define UART2CC32XX_PIN_62_UART0_RTS   0xA3D
 
#define UART2CC32XX_PIN_62_UART1_RTS   0x33D
 

Typedefs

typedef struct UART2CC32XX_ObjectUART2CC32XX_Handle
 

Enumerations

enum  UART2CC32XX_FifoThreshold {
  UART2CC32XX_FIFO_THRESHOLD_1_8 = 0, UART2CC32XX_FIFO_THRESHOLD_2_8 = 1, UART2CC32XX_FIFO_THRESHOLD_4_8 = 2, UART2CC32XX_FIFO_THRESHOLD_6_8 = 3,
  UART2CC32XX_FIFO_THRESHOLD_7_8 = 4
}
 UART TX/RX interrupt FIFO threshold select. More...
 

Macro Definition Documentation

§ UART2CC32XX_PIN_UNASSIGNED

#define UART2CC32XX_PIN_UNASSIGNED   0xFFF

Indicates a pin is not being used.

If hardware flow control is not being used, the UART CTS and RTS pins should be set to UART2CC32XX_PIN_UNASSIGNED.

§ UART2CC32XX_DMACH_UNASSIGNED

#define UART2CC32XX_DMACH_UNASSIGNED   0xFF

Indicates a DMA channel is not being used.

If DMA is not being used, the UART rxDmaChannel and txDmaChannel should be set to UART2CC32XX_DMACH_UNASSIGNED.

§ UART2CC32XX_PIN_01_UART1_TX

#define UART2CC32XX_PIN_01_UART1_TX   0x700

PIN 1 is used for UART1 TX

§ UART2CC32XX_PIN_02_UART1_RX

#define UART2CC32XX_PIN_02_UART1_RX   0x701

PIN 2 is used for UART1 RX

§ UART2CC32XX_PIN_03_UART0_TX

#define UART2CC32XX_PIN_03_UART0_TX   0x702

PIN 3 is used for UART0 TX

§ UART2CC32XX_PIN_04_UART0_RX

#define UART2CC32XX_PIN_04_UART0_RX   0x703

PIN 4 is used for UART0 RX

§ UART2CC32XX_PIN_07_UART1_TX

#define UART2CC32XX_PIN_07_UART1_TX   0x506

PIN 7 is used for UART1 TX

§ UART2CC32XX_PIN_08_UART1_RX

#define UART2CC32XX_PIN_08_UART1_RX   0x507

PIN 8 is used for UART1 RX

§ UART2CC32XX_PIN_16_UART1_TX

#define UART2CC32XX_PIN_16_UART1_TX   0x20F

PIN 16 is used for UART1 TX

§ UART2CC32XX_PIN_17_UART1_RX

#define UART2CC32XX_PIN_17_UART1_RX   0x210

PIN 17 is used for UART1 RX

§ UART2CC32XX_PIN_45_UART0_RX

#define UART2CC32XX_PIN_45_UART0_RX   0x92C

PIN 45 is used for UART0 RX

§ UART2CC32XX_PIN_45_UART1_RX

#define UART2CC32XX_PIN_45_UART1_RX   0x22C

PIN 45 is used for UART1 RX

§ UART2CC32XX_PIN_53_UART0_TX

#define UART2CC32XX_PIN_53_UART0_TX   0x934

PIN 53 is used for UART0 TX

§ UART2CC32XX_PIN_55_UART0_TX

#define UART2CC32XX_PIN_55_UART0_TX   0x336

PIN 55 is used for UART0 TX

§ UART2CC32XX_PIN_55_UART1_TX

#define UART2CC32XX_PIN_55_UART1_TX   0x636

PIN 55 is used for UART1 TX

§ UART2CC32XX_PIN_57_UART0_RX

#define UART2CC32XX_PIN_57_UART0_RX   0x338

PIN 57 is used for UART0 RX

§ UART2CC32XX_PIN_57_UART1_RX

#define UART2CC32XX_PIN_57_UART1_RX   0x638

PIN 57 is used for UART1 RX

§ UART2CC32XX_PIN_58_UART1_TX

#define UART2CC32XX_PIN_58_UART1_TX   0x639

PIN 58 is used for UART1 TX

§ UART2CC32XX_PIN_59_UART1_RX

#define UART2CC32XX_PIN_59_UART1_RX   0x63A

PIN 59 is used for UART1 RX

§ UART2CC32XX_PIN_62_UART0_TX

#define UART2CC32XX_PIN_62_UART0_TX   0xB3D

PIN 62 is used for UART0 TX

§ UART2CC32XX_PIN_50_UART0_CTS

#define UART2CC32XX_PIN_50_UART0_CTS   0xC31

PIN 50 is used for UART0 CTS

§ UART2CC32XX_PIN_50_UART0_RTS

#define UART2CC32XX_PIN_50_UART0_RTS   0x331

PIN 50 is used for UART0 RTS

§ UART2CC32XX_PIN_50_UART1_RTS

#define UART2CC32XX_PIN_50_UART1_RTS   0xA31

PIN 50 is used for UART1 RTS

§ UART2CC32XX_PIN_52_UART0_RTS

#define UART2CC32XX_PIN_52_UART0_RTS   0x633

PIN 52 is used for UART0 RTS

§ UART2CC32XX_PIN_61_UART0_RTS

#define UART2CC32XX_PIN_61_UART0_RTS   0x53C

PIN 61 is used for UART0 RTS

§ UART2CC32XX_PIN_61_UART0_CTS

#define UART2CC32XX_PIN_61_UART0_CTS   0x63C

PIN 61 is used for UART0 CTS

§ UART2CC32XX_PIN_61_UART1_CTS

#define UART2CC32XX_PIN_61_UART1_CTS   0x33C

PIN 61 is used for UART1 CTS

§ UART2CC32XX_PIN_62_UART0_RTS

#define UART2CC32XX_PIN_62_UART0_RTS   0xA3D

PIN 62 is used for UART0 RTS

§ UART2CC32XX_PIN_62_UART1_RTS

#define UART2CC32XX_PIN_62_UART1_RTS   0x33D

PIN 62 is used for UART1 RTS

Typedef Documentation

§ UART2CC32XX_Handle

Enumeration Type Documentation

§ UART2CC32XX_FifoThreshold

UART TX/RX interrupt FIFO threshold select.

Defined FIFO thresholds for generation of both TX interrupt and RX interrupt. If the RX and TX FIFO and thresholds are not set in the HwAttrs, the RX interrupt FIFO threshold is set to 1/8 full, and the TX interrupt FIFO threshold is set to 1/8 full.

Enumerator
UART2CC32XX_FIFO_THRESHOLD_1_8 

FIFO threshold of 1/8 full

UART2CC32XX_FIFO_THRESHOLD_2_8 

FIFO threshold of 2/8 full

UART2CC32XX_FIFO_THRESHOLD_4_8 

FIFO threshold of 4/8 full

UART2CC32XX_FIFO_THRESHOLD_6_8 

FIFO threshold of 6/8 full

UART2CC32XX_FIFO_THRESHOLD_7_8 

FIFO threshold of 7/8 full

© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale