Data Fields
UART2CC32XX_Object Struct Reference

UART2CC32XX Object. More...

#include <UART2CC32XX.h>

Collaboration diagram for UART2CC32XX_Object:
Collaboration graph
[legend]

Data Fields

UART2_BASE_OBJECT UDMACC32XX_Handle udmaHandle
 
Power_NotifyObj postNotify
 
PowerCC32XX_ParkState prevParkTX
 
uint16_t txPin
 
PowerCC32XX_ParkState prevParkRTS
 
uint16_t rtsPin
 

Detailed Description

UART2CC32XX Object.

The application must not access any member variables of this structure!

Field Documentation

§ udmaHandle

UART2_BASE_OBJECT UDMACC32XX_Handle UART2CC32XX_Object::udmaHandle

§ postNotify

Power_NotifyObj UART2CC32XX_Object::postNotify

§ prevParkTX

PowerCC32XX_ParkState UART2CC32XX_Object::prevParkTX

§ txPin

uint16_t UART2CC32XX_Object::txPin

§ prevParkRTS

PowerCC32XX_ParkState UART2CC32XX_Object::prevParkRTS

§ rtsPin

uint16_t UART2CC32XX_Object::rtsPin

The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale