SimpleLink CC32xx OTA Library
Simplifies the implementation of Internet connectivity
OtaLib_t Struct Reference

Data Fields

OtaState_e State
 
uint32_t Options
 
uint8_t VendorDir [MAX_VENDIR_DIR_SIZE]
 
Ota_optServerInfo OtaServerInfo
 
CdnClient_t CdnClient
 
OtaArchive_t OtaArchive
 
uint8_t * pOtaFileName
 
int32_t OtaFileSize
 
uint8_t FileUrlBuf [MAX_URL_SIZE]
 
uint8_t * pRecvChunk
 
int16_t RecvChunkSize
 
int16_t RecvChunkOffset
 
int16_t RecvChunkForceReadMode
 
int16_t RecvChunkReserved
 
uint8_t NetBuf [NET_BUF_SIZE+1]
 
int8_t ConsecutiveOtaErrors
 

Detailed Description

Definition at line 59 of file OtaLib.h.

Field Documentation

§ CdnClient

CdnClient_t CdnClient

Definition at line 69 of file OtaLib.h.

§ ConsecutiveOtaErrors

int8_t ConsecutiveOtaErrors

Definition at line 88 of file OtaLib.h.

§ FileUrlBuf

uint8_t FileUrlBuf[MAX_URL_SIZE]

Definition at line 75 of file OtaLib.h.

§ NetBuf

uint8_t NetBuf[NET_BUF_SIZE+1]

Definition at line 85 of file OtaLib.h.

§ Options

uint32_t Options

Definition at line 62 of file OtaLib.h.

§ OtaArchive

OtaArchive_t OtaArchive

Definition at line 70 of file OtaLib.h.

§ OtaFileSize

int32_t OtaFileSize

Definition at line 74 of file OtaLib.h.

§ OtaServerInfo

Ota_optServerInfo OtaServerInfo

Definition at line 66 of file OtaLib.h.

§ pOtaFileName

uint8_t* pOtaFileName

Definition at line 73 of file OtaLib.h.

§ pRecvChunk

uint8_t* pRecvChunk

Definition at line 78 of file OtaLib.h.

§ RecvChunkForceReadMode

int16_t RecvChunkForceReadMode

Definition at line 81 of file OtaLib.h.

§ RecvChunkOffset

int16_t RecvChunkOffset

Definition at line 80 of file OtaLib.h.

§ RecvChunkReserved

int16_t RecvChunkReserved

Definition at line 82 of file OtaLib.h.

§ RecvChunkSize

int16_t RecvChunkSize

Definition at line 79 of file OtaLib.h.

§ State

OtaState_e State

Definition at line 61 of file OtaLib.h.

§ VendorDir

uint8_t VendorDir[MAX_VENDIR_DIR_SIZE]

Definition at line 65 of file OtaLib.h.


The documentation for this struct was generated from the following file: