SimpleLink CC32xx OTA Library
Simplifies the implementation of Internet connectivity
CdnClient_t Struct Reference

Data Fields

Ota_optServerInfopOtaServerInfo
 
int32_t CurrDirFileIndex
 
OtaDirData_t OtaDirData
 
int16_t ServerSockId
 
int32_t PortNum
 
int16_t FileSockId
 
uint8_t * pRecvChunk
 
uint8_t * pNetBuf
 

Detailed Description

Definition at line 54 of file CdnClient.h.

Field Documentation

§ CurrDirFileIndex

int32_t CurrDirFileIndex

Definition at line 60 of file CdnClient.h.

§ FileSockId

int16_t FileSockId

Definition at line 66 of file CdnClient.h.

§ OtaDirData

OtaDirData_t OtaDirData

Definition at line 61 of file CdnClient.h.

§ pNetBuf

uint8_t* pNetBuf

Definition at line 68 of file CdnClient.h.

§ PortNum

int32_t PortNum

Definition at line 65 of file CdnClient.h.

§ pOtaServerInfo

Ota_optServerInfo* pOtaServerInfo

Definition at line 57 of file CdnClient.h.

§ pRecvChunk

uint8_t* pRecvChunk

Definition at line 67 of file CdnClient.h.

§ ServerSockId

int16_t ServerSockId

Definition at line 64 of file CdnClient.h.


The documentation for this struct was generated from the following file: