SimpleLink CC31xx/CC32xx Host Driver
Version 3.0.1.60
Simplifies the implementation of Internet connectivity
|
Controls standard client/server sockets programming options and capabilities. More...
Functions | |
_i16 | sl_Socket (_i16 Domain, _i16 Type, _i16 Protocol) |
Create an endpoint for communication. More... | |
_i16 | sl_Close (_i16 sd) |
Gracefully close socket. More... | |
_i16 | sl_Accept (_i16 sd, SlSockAddr_t *addr, SlSocklen_t *addrlen) |
Accept a connection on a socket. More... | |
_i16 | sl_Bind (_i16 sd, const SlSockAddr_t *addr, _i16 addrlen) |
Assign a name to a socket. More... | |
_i16 | sl_Listen (_i16 sd, _i16 backlog) |
Listen for connections on a socket. More... | |
_i16 | sl_Connect (_i16 sd, const SlSockAddr_t *addr, _i16 addrlen) |
Initiate a connection on a socket. More... | |
_i16 | sl_Select (_i16 nfds, SlFdSet_t *readsds, SlFdSet_t *writesds, SlFdSet_t *exceptsds, struct SlTimeval_t *timeout) |
Monitor socket activity. More... | |
int16_t | SlNetIfWifi_socket (void *ifContext, int16_t Domain, int16_t Type, int16_t Protocol, void **sdContext) |
Create an endpoint for communication. More... | |
int32_t | SlNetIfWifi_close (int16_t sd, void *sdContext) |
Gracefully close socket. More... | |
int16_t | SlNetIfWifi_accept (int16_t sd, void *sdContext, SlNetSock_Addr_t *addr, SlNetSocklen_t *addrlen, uint8_t flags, void **acceptedSdContext) |
Accept a connection on a socket. More... | |
int32_t | SlNetIfWifi_bind (int16_t sd, void *sdContext, const SlNetSock_Addr_t *addr, int16_t addrlen) |
Assign a name to a socket. More... | |
int32_t | SlNetIfWifi_listen (int16_t sd, void *sdContext, int16_t backlog) |
Listen for connections on a socket. More... | |
int32_t | SlNetIfWifi_connect (int16_t sd, void *sdContext, const SlNetSock_Addr_t *addr, SlNetSocklen_t addrlen, uint8_t flags) |
Initiate a connection on a socket. More... | |
int32_t | SlNetIfWifi_getSockName (int16_t sd, void *sdContext, SlNetSock_Addr_t *addr, SlNetSocklen_t *addrlen) |
Get local address info by socket descriptor Returns the local address info of the socket descriptor. More... | |
int32_t | SlNetIfWifi_select (void *ifContext, int16_t nfds, SlNetSock_SdSet_t *readsds, SlNetSock_SdSet_t *writesds, SlNetSock_SdSet_t *exceptsds, SlNetSock_Timeval_t *timeout) |
Monitor socket activity. More... | |
int32_t | SlNetIfWifi_setSockOpt (int16_t sd, void *sdContext, int16_t level, int16_t optname, void *optval, SlNetSocklen_t optlen) |
Set socket options-. More... | |
int32_t | SlNetIfWifi_getSockOpt (int16_t sd, void *sdContext, int16_t level, int16_t optname, void *optval, SlNetSocklen_t *optlen) |
Get socket options. More... | |
int32_t | SlNetIfWifi_recv (int16_t sd, void *sdContext, void *buf, uint32_t len, uint32_t flags) |
Read data from TCP socket. More... | |
int32_t | SlNetIfWifi_recvFrom (int16_t sd, void *sdContext, void *buf, uint32_t len, uint32_t flags, SlNetSock_Addr_t *from, SlNetSocklen_t *fromlen) |
Read data from socket. More... | |
int32_t | SlNetIfWifi_send (int16_t sd, void *sdContext, const void *buf, uint32_t len, uint32_t flags) |
Write data to TCP socket. More... | |
int32_t | SlNetIfWifi_sendTo (int16_t sd, void *sdContext, const void *buf, uint32_t len, uint32_t flags, const SlNetSock_Addr_t *to, SlNetSocklen_t tolen) |
Write data to socket. More... | |
int32_t | SlNetIfWifi_sockstartSec (int16_t sd, void *sdContext, SlNetSockSecAttrib_t *secAttrib, uint8_t flags) |
Start a security session on an opened socket. More... | |
int32_t | SlNetIfWifi_getHostByName (void *ifContext, char *name, const uint16_t nameLen, uint32_t *ipAddr, uint16_t *ipAddrLen, const uint8_t family) |
Get host IP by name Obtain the IP Address of machine on network, by machine name. More... | |
int32_t | SlNetIfWifi_getIPAddr (void *ifContext, SlNetIfAddressType_e addrType, uint16_t *addrConfig, uint32_t *ipAddr) |
Get IP Address of specific interface. More... | |
int32_t | SlNetIfWifi_getConnectionStatus (void *ifContext) |
Get interface connection status. More... | |
int32_t | SlNetIfWifi_loadSecObj (void *ifContext, uint16_t objType, char *objName, int16_t objNameLen, uint8_t *objBuff, int16_t objBuffLen) |
Load secured buffer to the network stack. More... | |
int32_t | SlNetIfWifi_CreateContext (uint16_t ifID, const char *ifName, void **ifContext) |
Allocate and store interface data. More... | |
Typedefs | |
typedef struct SlInAddr_t | SlInAddr_t |
typedef struct SlIn6Addr_t | SlIn6Addr_t |
typedef _i32 | SlTime_t |
typedef _i32 | SlSuseconds_t |
typedef struct SlTimeval_t | SlTimeval_t |
typedef _u16 | SlSocklen_t |
typedef struct SlSockAddr_t | SlSockAddr_t |
typedef struct SlSockAddrIn6_t | SlSockAddrIn6_t |
typedef struct SlSockAddrIn_t | SlSockAddrIn_t |
typedef struct SlFdSet_t | SlFdSet_t |
Variables | |
_u32 | s_addr |
_u8 | s_b1 |
_u8 | s_b2 |
_u8 | s_b3 |
_u8 | s_b4 |
struct { | |
_u8 | s_b1 |
_u8 | s_b2 |
_u8 | s_b3 |
_u8 | s_b4 |
} | S_un_b |
_u16 | s_w1 |
_u16 | s_w2 |
struct { | |
_u16 | s_w1 |
_u16 | s_w2 |
} | S_un_w |
_u32 | S_addr |
union SlInAddr_t::S_un | S_un |
_u8 | _S6_u8 [16] |
_u32 | _S6_u32 [4] |
union { | |
_u8 | _S6_u8 [16] |
_u32 | _S6_u32 [4] |
} | _S6_un |
_u32 | KeepaliveEnabled |
_u32 | ReuseaddrEnabled |
_i32 | RxIpNoBoundaryEnabled |
_u32 | WinSize |
_u32 | NonBlockingEnabled |
_u8 | Sd |
_u8 | Type |
_i16 | Val |
_i8 | pExtraInfo [128] |
_i16 | Status |
_u8 | Sd |
_u8 | Padding |
SlSockTxFailEventData_t | SockTxFailData |
SlSocketAsyncEvent_t | SockAsyncData |
_u32 | Event |
SlSockEventData_u | SocketAsyncEvent |
_u32 | Event |
_u32 | EventData |
_u32 | SecureALPN |
_u32 | SecureMask |
_u8 | SecureMethod |
_u16 | SubjectNameXoredSha1 |
_u16 | IssuerNameXoredSha1 |
_i8 | FromDate [8] |
_i8 | ToDate [8] |
_i8 | SubjectName [SL_MAX_ISSUER_AND_SUBJECT_NAME_LEN] |
_i8 | IssuerName [SL_MAX_ISSUER_AND_SUBJECT_NAME_LEN] |
_i8 | SubjectNameLen |
_i8 | IssuerNameLen |
_i8 | Padding [2] |
_u32 | SecureVersion |
_u32 | SecureCipherSuit |
_u32 | SecureIsPeerValidated |
_u32 | SecureALPNChosenProtocol |
SlSockSSLCertInfo_t | SecurePeerCertinfo |
_u16 | type |
_u16 | length |
SlInAddr_t | imr_multiaddr |
SlInAddr_t | imr_interface |
SlIn6Addr_t | ipv6mr_multiaddr |
_u32 | ipv6mr_interface |
_u32 | l_onoff |
_u32 | l_linger |
SlTime_t | tv_sec |
SlSuseconds_t | tv_usec |
_u16 | sa_family |
_u8 | sa_data [14] |
_u16 | sin6_family |
_u16 | sin6_port |
_u32 | sin6_flowinfo |
SlIn6Addr_t | sin6_addr |
_u32 | sin6_scope_id |
_u16 | sin_family |
_u16 | sin_port |
SlInAddr_t | sin_addr |
_i8 | sin_zero [8] |
_u8 | SecureFiles [4] |
_u32 | fd_array [(SL_FD_SETSIZE+(_u8) 31)/(_u8) 32] |
_u8 | Rate |
_u8 | Channel |
_i8 | Rssi |
_u8 | Padding |
_u32 | Timestamp |
_u32 | enableDisable |
SlNetIf_Config_t | SlNetIfConfigWifi |
Controls standard client/server sockets programming options and capabilities.
_i16 sl_Accept | ( | _i16 | sd, |
SlSockAddr_t * | addr, | ||
SlSocklen_t * | addrlen | ||
) |
Accept a connection on a socket.
This function is used with connection-based socket types (SOCK_STREAM).
It extracts the first connection request on the queue of pending connections, creates a new connected socket, and returns a new file descriptor referring to that socket.
The newly created socket is not in the listening state. The original socket sd is unaffected by this call.
The argument sd is a socket that has been created with sl_Socket(), bound to a local address with sl_Bind(), and is listening for connections after a sl_Listen(). The argument addr is a pointer to a sockaddr structure. This structure is filled in with the address of the peer socket, as known to the communications layer. The exact format of the address returned addr is determined by the socket's address family.
The addrlen argument is a value-result argument: it should initially contain the size of the structure pointed to by addr, on return it will contain the actual length (in bytes) of the address returned.
[in] | sd | Socket descriptor (handle) |
[out] | addr | The argument addr is a pointer to a sockaddr structure. This structure is filled in with the address of the peer socket, as known to the communications layer. The exact format of the address returned addr is determined by the socket's address sockaddr: - code for the address format. On this version only AF_INET is supported. - socket address, the length depends on the code format |
[out] | addrlen | The addrlen argument is a value-result argument: it should initially contain the size of the structure pointed to by addr |
Definition at line 692 of file sl_socket.c.
_i16 sl_Bind | ( | _i16 | sd, |
const SlSockAddr_t * | addr, | ||
_i16 | addrlen | ||
) |
Assign a name to a socket.
This function gives the socket the local address addr. addr is addrlen bytes long. Traditionally, this is called When a socket is created with socket, it exists in a name space (address family) but has no name assigned. It is necessary to assign a local address before a SOCK_STREAM socket may receive connections.
[in] | sd | Socket descriptor (handle) |
[in] | addr | Specifies the destination addrs sockaddr: - code for the address format. On this version only SL_AF_INET is supported. - socket address, the length depends on the code format |
[in] | addrlen | Contains the size of the structure pointed to by addr |
Definition at line 237 of file sl_socket.c.
_i16 sl_Close | ( | _i16 | sd | ) |
Gracefully close socket.
This function causes the system to release resources allocated to a socket.
In case of TCP, the connection is terminated.
[in] | sd | Socket handle (received in sl_Socket) |
Definition at line 176 of file sl_socket.c.
_i16 sl_Connect | ( | _i16 | sd, |
const SlSockAddr_t * | addr, | ||
_i16 | addrlen | ||
) |
Initiate a connection on a socket.
Function connects the socket referred to by the socket descriptor sd, to the address specified by addr. The addrlen argument specifies the size of addr. The format of the address in addr is determined by the address space of the socket. If it is of type SOCK_DGRAM, this call specifies the peer with which the socket is to be associated; this address is that to which datagrams are to be sent, and the only address from which datagrams are to be received. If the socket is of type SOCK_STREAM, this call attempts to make a connection to another socket. The other socket is specified by address, which is an address in the communications space of the socket.
[in] | sd | Socket descriptor (handle) |
[in] | addr | Specifies the destination addr sockaddr: - code for the address format. On this version only AF_INET is supported. - socket address, the length depends on the code format |
[in] | addrlen | Contains the size of the structure pointed to by addr |
Definition at line 449 of file sl_socket.c.
_i16 sl_GetSockOpt | ( | _i16 | sd, |
_i16 | level, | ||
_i16 | optname, | ||
void * | optval, | ||
SlSocklen_t * | optlen | ||
) |
Get socket options.
This function manipulate the options associated with a socket. Options may exist at multiple protocol levels; they are always present at the uppermost socket level.
When manipulating socket options the level at which the option resides and the name of the option must be specified. To manipulate options at the socket level, level is specified as SOL_SOCKET. To manipulate options at any other level the protocol number of the appropriate protocol controlling the option is supplied. For example, to indicate that an option is to be interpreted by the TCP protocol, level should be set to the protocol number of TCP;
The parameters optval and optlen are used to access optvalues for setsockopt(). For getsockopt() they identify a buffer in which the value for the requested option(s) are to be returned. For getsockopt(), optlen is a value-result parameter, initially containing the size of the buffer pointed to by option_value, and modified on return to indicate the actual size of the value returned. If no option value is to be supplied or returned, option_value may be NULL.
[in] | sd | Socket handle |
[in] | level | Defines the protocol level for this option |
[in] | optname | defines the option name to interrogate |
[out] | optval | Specifies a value for the option |
[out] | optlen | Specifies the length of the option value |
Definition at line 975 of file sl_socket.c.
_u32 sl_Htonl | ( | _u32 | val | ) |
Reorder the bytes of a 32-bit unsigned value.
This function is used to Reorder the bytes of a 32-bit unsigned value from processor order to network order.
[in] | val | Variable to reorder |
Definition at line 806 of file sl_socket.c.
_u16 sl_Htons | ( | _u16 | val | ) |
Reorder the bytes of a 16-bit unsigned value.
This function is used to Reorder the bytes of a 16-bit unsigned value from processor order to network order.
[in] | val | Variable to reorder |
Definition at line 827 of file sl_socket.c.
_i16 sl_Listen | ( | _i16 | sd, |
_i16 | backlog | ||
) |
Listen for connections on a socket.
The willingness to accept incoming connections and a queue limit for incoming connections are specified with listen(), and then the connections are accepted with accept. The listen() call applies only to sockets of type SOCK_STREAM The backlog parameter defines the maximum length the queue of pending connections may grow to.
[in] | sd | Socket descriptor (handle) |
[in] | backlog | Specifies the listen queue depth. |
Definition at line 658 of file sl_socket.c.
_i16 sl_Recv | ( | _i16 | sd, |
void * | buf, | ||
_i16 | len, | ||
_i16 | flags | ||
) |
Read data from TCP socket.
Function receives a message from a connection-mode socket
[in] | sd | Socket handle |
[out] | buf | Points to the buffer where the message should be stored. |
[in] | len | Specifies the length in bytes of the buffer pointed to by the buffer argument. Range: 1-16000 bytes |
[in] | flags | Specifies the type of message reception. On this version, this parameter is not supported. |
Definition at line 881 of file sl_socket.c.
_i16 sl_RecvFrom | ( | _i16 | sd, |
void * | buf, | ||
_i16 | len, | ||
_i16 | flags, | ||
SlSockAddr_t * | from, | ||
SlSocklen_t * | fromlen | ||
) |
Read data from socket.
Function receives a message from a connection-mode or connectionless-mode socket
[in] | sd | Socket handle |
[out] | buf | Points to the buffer where the message should be stored. |
[in] | len | Specifies the length in bytes of the buffer pointed to by the buffer argument. Range: 1-16000 bytes |
[in] | flags | Specifies the type of message reception. On this version, this parameter is not supported. |
[in] | from | Pointer to an address structure indicating the source address. sockaddr: - code for the address format. On this version only AF_INET is supported. - socket address, the length depends on the code format |
[in] | fromlen | Source address structure size. This parameter MUST be set to the size of the structure pointed to by addr. |
Definition at line 360 of file sl_socket.c.
_i16 sl_Select | ( | _i16 | nfds, |
SlFdSet_t * | readsds, | ||
SlFdSet_t * | writesds, | ||
SlFdSet_t * | exceptsds, | ||
struct SlTimeval_t * | timeout | ||
) |
Monitor socket activity.
Select allow a program to monitor multiple file descriptors, waiting until one or more of the file descriptors become "ready" for some class of I/O operation. If trigger mode is enabled the active fdset is the one that was retrieved in the first triggered call. To enable the trigger mode, an handler must be statically registered as slcb_SocketTriggerEventHandler in user.h
[in] | nfds | The highest-numbered file descriptor in any of the three sets, plus 1. |
[out] | readsds | Socket descriptors list for read monitoring and accept monitoring |
[out] | writesds | Socket descriptors list for connect monitoring only, write monitoring is not supported |
[out] | exceptsds | Socket descriptors list for exception monitoring, not supported. |
[in] | timeout | Is an upper bound on the amount of time elapsed before select() returns. Null or above 0xffff seconds means infinity timeout. The minimum timeout is 10 milliseconds, less than 10 milliseconds will be set automatically to 10 milliseconds. Max microseconds supported is 0xfffc00. In trigger mode the timout fields must be set to zero. |
Several threads can call sl_Select at the same time.Calling this API while the same command is called from another thread, may result in one of the following scenarios:
In case all the user sockets are open, sl_Select will exhibit the behavior mentioned in (2) This is due to the fact sl_select supports multiple callers by utilizing one user socket internally. User who wish to ensure multiple select calls at any given time, must reserve one socket out of the 16 given.
Definition at line 1761 of file sl_socket.c.
_i16 sl_Send | ( | _i16 | sd, |
const void * | buf, | ||
_i16 | len, | ||
_i16 | flags | ||
) |
Write data to TCP socket.
This function is used to transmit a message to another socket. Returns immediately after sending data to device. In case of TCP failure an async event SL_SOCKET_TX_FAILED_EVENT is going to be received.
In case of a RAW socket (transceiver mode), extra 4 bytes should be reserved at the end of the frame data buffer for WLAN FCS
[in] | sd | Socket handle |
[in] | buf | Points to a buffer containing the message to be sent |
[in] | len | Message size in bytes. |
[in] | flags | Specifies the type of message transmission. On this version, this parameter is not supported for TCP. For transceiver mode, the SL_WLAN_RAW_RF_TX_PARAMS macro can be used to determine transmission parameters (channel,rate,tx_power,preamble) -rate need to be define using slSockTransceiverTXRateTable_e |
Definition at line 594 of file sl_socket.c.
_i16 sl_SendTo | ( | _i16 | sd, |
const void * | buf, | ||
_i16 | len, | ||
_i16 | flags, | ||
const SlSockAddr_t * | to, | ||
SlSocklen_t | tolen | ||
) |
Write data to socket.
This function is used to transmit a message to another socket (connection less socket SOCK_DGRAM, SOCK_RAW).
Returns immediately after sending data to device.
In case of transmission failure an async event SL_SOCKET_TX_FAILED_EVENT is going to be received.
[in] | sd | Socket handle |
[in] | buf | Points to a buffer containing the message to be sent |
[in] | len | message size in bytes. |
[in] | flags | Specifies the type of message transmission. On this version, this parameter is not supported |
[in] | to | Pointer to an address structure indicating the destination address. sockaddr: - code for the address format. On this version only AF_INET is supported. - socket address, the length depends on the code format |
[in] | tolen | Destination address structure size |
Definition at line 283 of file sl_socket.c.
_i16 sl_Socket | ( | _i16 | Domain, |
_i16 | Type, | ||
_i16 | Protocol | ||
) |
Create an endpoint for communication.
The socket function creates a new socket of a certain socket type, identified by an integer number, and allocates system resources to it.
This function is called by the application layer to obtain a socket handle.
[in] | Domain | Specifies the protocol family of the created socket. For example:
|
[in] | Type | specifies the communication semantic, one of:
|
[in] | Protocol | specifies a particular transport to be used with the socket. The most common are
|
Definition at line 133 of file sl_socket.c.
_i16 sl_StartTLS | ( | _i16 | sd | ) |
Initiate TLS connection on a socket.
Function Initiate TLS connection on the socket referred to by the socket descriptor sd. This function will works on blocking mode until the TLS handshake success or fails.
[in] | sd | Socket descriptor (handle) |
Definition at line 1971 of file sl_socket.c.
int16_t SlNetIfWifi_accept | ( | int16_t | sd, |
void * | sdContext, | ||
SlNetSock_Addr_t * | addr, | ||
SlNetSocklen_t * | addrlen, | ||
uint8_t | flags, | ||
void ** | acceptedSdContext | ||
) |
Accept a connection on a socket.
The SlNetIfWifi_accept function is used with connection-based socket types (SOCK_STREAM).
It extracts the first connection request on the queue of pending connections, creates a new connected socket, and returns a new file descriptor referring to that socket.
The newly created socket is not in the listening state. The original socket sd is unaffected by this call.
The argument sd is a socket that has been created with SlNetIfWifi_socket(), bound to a local address with SlNetIfWifi_bind(), and is listening for connections after a SlNetIfWifi_listen().
The argument addr is a pointer to a sockaddr structure. This structure is filled in with the address of the peer socket, as known to the communications layer.
The exact format of the address returned addr is determined by the socket's address family.
The addrlen argument is a value-result argument: it should initially contain the size of the structure pointed to by addr, on return it will contain the actual length (in bytes) of the address returned.
[in] | sd | Socket descriptor (handle) |
[in] | sdContext | May store socket data if implemented in the SlNetIfWifi_socket function. |
[out] | addr | The argument addr is a pointer to a sockaddr structure. This structure is filled in with the address of the peer socket, as known to the communications layer. The exact format of the address returned addr is determined by the socket's address sockaddr: - code for the address format. - socket address, the length depends on the code format |
[out] | addrlen | The addrlen argument is a value-result argument: it should initially contain the size of the structure pointed to by addr |
[in] | flags | Specifies socket descriptor flags. The available flags are:
|
[in] | acceptedSdContext | Allocate and store data for the new socket if needed in other to use it in other slnetwifi socket functions |
Definition at line 151 of file slnetifwifi.c.
int32_t SlNetIfWifi_bind | ( | int16_t | sd, |
void * | sdContext, | ||
const SlNetSock_Addr_t * | addr, | ||
int16_t | addrlen | ||
) |
Assign a name to a socket.
This SlNetIfWifi_bind function gives the socket the local address addr. addr is addrlen bytes long.
Traditionally, this is called When a socket is created with socket, it exists in a name space (address family) but has no name assigned.
It is necessary to assign a local address before a SOCK_STREAM socket may receive connections.
[in] | sd | Socket descriptor (handle) |
[in] | sdContext | May store socket data if implemented in the SlNetIfWifi_socket function. |
[in] | addr | Specifies the destination addrs sockaddr: - code for the address format. - socket address, the length depends on the code format |
[in] | addrlen | Contains the size of the structure pointed to by addr |
Definition at line 162 of file slnetifwifi.c.
int32_t SlNetIfWifi_close | ( | int16_t | sd, |
void * | sdContext | ||
) |
Gracefully close socket.
The SlNetIfWifi_close function causes the system to release resources allocated to a socket.
In case of TCP, the connection is terminated.
[in] | sd | Socket descriptor (handle), received in SlNetIfWifi_socket |
[in] | sdContext | May store socket data if implemented in the SlNetIfWifi_socket function. |
Definition at line 139 of file slnetifwifi.c.
int32_t SlNetIfWifi_connect | ( | int16_t | sd, |
void * | sdContext, | ||
const SlNetSock_Addr_t * | addr, | ||
SlNetSocklen_t | addrlen, | ||
uint8_t | flags | ||
) |
Initiate a connection on a socket.
Function connects the socket referred to by the socket descriptor sd, to the address specified by addr.
The addrlen argument specifies the size of addr.
The format of the address in addr is determined by the address space of the socket.
If it is of type SLNETSOCK_SOCK_DGRAM, this call specifies the peer with which the socket is to be associated; this address is that to which datagrams are to be sent, and the only address from which datagrams are to be received.
If the socket is of type SLNETSOCK_SOCK_STREAM, this call attempts to make a connection to another socket.
The other socket is specified by address, which is an address in the communications space of the socket.
[in] | sd | Socket descriptor (handle) |
[in] | sdContext | May store socket data if implemented in the SlNetIfWifi_socket function. |
[in] | addr | Specifies the destination addr sockaddr: - code for the address format. - socket address, the length depends on the code format |
[in] | addrlen | Contains the size of the structure pointed to by addr |
[in] | flags | Specifies socket descriptor flags. The available flags are:
|
Definition at line 184 of file slnetifwifi.c.
int32_t SlNetIfWifi_CreateContext | ( | uint16_t | ifID, |
const char * | ifName, | ||
void ** | ifContext | ||
) |
Allocate and store interface data.
The SlNetIfWifi_CreateContext function stores interface related data.
[in] | ifContext | Allocate and store interface data if needed. Can be used in all slnetwifi interface functions |
Definition at line 601 of file slnetifwifi.c.
int32_t SlNetIfWifi_getConnectionStatus | ( | void * | ifContext | ) |
Get interface connection status.
The SlNetIfWifi_getConnectionStatus function gets the connection status of the interface (connected Or disconnected).
[in] | ifContext | Stores interface data if CreateContext function supported and implemented. Can be used in all SlNetIf_Config_t functions |
Definition at line 511 of file slnetifwifi.c.
int32_t SlNetIfWifi_getHostByName | ( | void * | ifContext, |
char * | name, | ||
const uint16_t | nameLen, | ||
uint32_t * | ipAddr, | ||
uint16_t * | ipAddrLen, | ||
const uint8_t | family | ||
) |
Get host IP by name
Obtain the IP Address of machine on network, by machine name.
[in] | ifContext | Stores interface data if CreateContext function supported and implemented. Can be used in all SlNetIf_Config_t functions |
[in] | ifBitmap | Specifies the interfaces which the host ip needs to be retrieved from (according to the priority until one of them will return an answer). The values of the interface identifiers is defined with the prefix SLNETIF_ID_ which defined in slnetif.h |
[in] | name | Host name |
[in] | nameLen | Name length |
[out] | ipAddr | This parameter is filled in with host IP addresses. In case that host name is not resolved, out_ip_addr is zero. |
[in,out] | ipAddrLen | Holds the size of the ipAddr array, when function successful, the ipAddrLen parameter will be updated with the number of the IP addresses found. |
[in] | family | Protocol family |
Definition at line 409 of file slnetifwifi.c.
int32_t SlNetIfWifi_getIPAddr | ( | void * | ifContext, |
SlNetIfAddressType_e | addrType, | ||
uint16_t * | addrConfig, | ||
uint32_t * | ipAddr | ||
) |
Get IP Address of specific interface.
The SlNetIfWifi_getIPAddr function retrieve the IP address of a specific interface according to the Address Type, IPv4, IPv6 LOCAL or IPv6 GLOBAL.
[in] | ifContext | Stores interface data if CreateContext function supported and implemented. Can be used in all SlNetIf_Config_t functions |
[in] | ifID | Specifies the interface which its connection state needs to be retrieved. The values of the interface identifier is defined with the prefix SLNETIF_ID_ which defined in slnetif.h |
[in] | addrType | Address type:
|
[out] | addrConfig | Address config:
|
[out] | ipAddr | IP Address according to the Address Type |
Definition at line 490 of file slnetifwifi.c.
int32_t SlNetIfWifi_getSockName | ( | int16_t | sd, |
void * | sdContext, | ||
SlNetSock_Addr_t * | addr, | ||
SlNetSocklen_t * | addrlen | ||
) |
Get local address info by socket descriptor
Returns the local address info of the socket descriptor.
[in] | sd | Socket descriptor (handle) |
[in] | sdContext | May store socket data if implemented in the SlNetIfWifi_socket function. |
[out] | addr | The argument addr is a pointer to a SlNetSock_Addr_t structure. This structure is filled in with the address of the peer socket, as known to the communications layer. The exact format of the address returned addr is determined by the socket's address SlNetSock_Addr_t: - code for the address format. - socket address, the length depends on the code format |
[out] | addrlen | The addrlen argument is a value-result argument: it should initially contain the size of the structure pointed to by addr |
Definition at line 196 of file slnetifwifi.c.
int32_t SlNetIfWifi_getSockOpt | ( | int16_t | sd, |
void * | sdContext, | ||
int16_t | level, | ||
int16_t | optname, | ||
void * | optval, | ||
SlNetSocklen_t * | optlen | ||
) |
Get socket options.
The SlNetIfWifi_getSockOpt function gets the options associated with a socket. Options may exist at multiple protocol levels; they are always present at the uppermost socket level.
The parameters optval and optlen identify a buffer in which the value for the requested option(s) are to be returned. optlen is a value-result parameter, initially containing the size of the buffer pointed to by option_value, and modified on return to indicate the actual size of the value returned. If no option value is to be supplied or returned, option_value may be NULL.
[in] | sd | Socket descriptor (handle) |
[in] | sdContext | May store socket data if implemented in the SlNetIfWifi_socket function. |
[in] | level | Defines the protocol level for this option |
[in] | optname | defines the option name to interrogate |
[out] | optval | Specifies a value for the option |
[out] | optlen | Specifies the length of the option value |
Definition at line 266 of file slnetifwifi.c.
int32_t SlNetIfWifi_listen | ( | int16_t | sd, |
void * | sdContext, | ||
int16_t | backlog | ||
) |
Listen for connections on a socket.
The willingness to accept incoming connections and a queue limit for incoming connections are specified with SlNetIfWifi_listen(), and then the connections are accepted with SlNetIfWifi_accept().
The SlNetIfWifi_listen() call applies only to sockets of type SOCK_STREAM The backlog parameter defines the maximum length the queue of pending connections may grow to.
[in] | sd | Socket descriptor (handle) |
[in] | sdContext | May store socket data if implemented in the SlNetIfWifi_socket function. |
[in] | backlog | Specifies the listen queue depth. |
Definition at line 173 of file slnetifwifi.c.
int32_t SlNetIfWifi_loadSecObj | ( | void * | ifContext, |
uint16_t | objType, | ||
char * | objName, | ||
int16_t | objNameLen, | ||
uint8_t * | objBuff, | ||
int16_t | objBuffLen | ||
) |
Load secured buffer to the network stack.
The SlNetSock_secLoadObj function loads buffer/files into the inputted network stack for future usage of the socket SSL/TLS connection. This option is relevant for network stacks with file system and also for network stacks that lack file system that can store the secured files.
[in] | ifContext | Stores interface data if CreateContext function supported and implemented. Can be used in all SlNetIf_Config_t functions |
[in] | objType | Specifies the security object type which could be one of the following:
|
[in] | objName | Specifies the name/input identifier of the secured buffer loaded for file systems - this can be the file name for plain text buffer loading this can be the name of the object |
[in] | objNameLen | Specifies the buffer name length to be loaded. |
[in] | objBuff | Specifies the pointer to the secured buffer to be loaded. |
[in] | objBuffLen | Specifies the buffer length to be loaded. |
Definition at line 538 of file slnetifwifi.c.
int32_t SlNetIfWifi_recv | ( | int16_t | sd, |
void * | sdContext, | ||
void * | buf, | ||
uint32_t | len, | ||
uint32_t | flags | ||
) |
Read data from TCP socket.
The SlNetIfWifi_recv function receives a message from a connection-mode socket
[in] | sd | Socket descriptor (handle) |
[in] | sdContext | May store socket data if implemented in the SlNetIfWifi_socket function. |
[out] | buf | Points to the buffer where the message should be stored. |
[in] | len | Specifies the length in bytes of the buffer pointed to by the buffer argument. Range: 1-16000 bytes |
[in] | flags | Upper 8 bits specifies the security flags Lower 24 bits specifies the type of message reception. On this version, the lower 24 bits are not supported |
Definition at line 323 of file slnetifwifi.c.
int32_t SlNetIfWifi_recvFrom | ( | int16_t | sd, |
void * | sdContext, | ||
void * | buf, | ||
uint32_t | len, | ||
uint32_t | flags, | ||
SlNetSock_Addr_t * | from, | ||
SlNetSocklen_t * | fromlen | ||
) |
Read data from socket.
SlNetIfWifi_recvFrom function receives a message from a connection-mode or connectionless-mode socket
[in] | sd | Socket descriptor (handle) |
[in] | sdContext | May store socket data if implemented in the SlNetIfWifi_socket function. |
[out] | buf | Points to the buffer where the message should be stored. |
[in] | len | Specifies the length in bytes of the buffer pointed to by the buffer argument. Range: 1-16000 bytes |
[in] | flags | Upper 8 bits specifies the security flags Lower 24 bits specifies the type of message reception. On this version, the lower 24 bits are not supported |
[in] | from | Pointer to an address structure indicating the source address. sockaddr: - code for the address format. - socket address, the length depends on the code format |
[in] | fromlen | Source address structure size. This parameter MUST be set to the size of the structure pointed to by addr. |
Definition at line 335 of file slnetifwifi.c.
int32_t SlNetIfWifi_select | ( | void * | ifContext, |
int16_t | nfds, | ||
SlNetSock_SdSet_t * | readsds, | ||
SlNetSock_SdSet_t * | writesds, | ||
SlNetSock_SdSet_t * | exceptsds, | ||
SlNetSock_Timeval_t * | timeout | ||
) |
Monitor socket activity.
SlNetIfWifi_send allow a program to monitor multiple file descriptors, waiting until one or more of the file descriptors become "ready" for some class of I/O operation. If trigger mode is enabled the active sdset is the one that retrieved in the first triggered call. To enable the trigger mode, an handler must be statically registered to the slcb_SocketTriggerEventHandler (user.h)
[in] | ifContext | Stores interface data if CreateContext function supported and implemented. Can be used in all SlNetIf_Config_t functions |
[in] | nsds | The highest-numbered file descriptor in any of the three sets, plus 1. |
[in,out] | readsds | Socket descriptors list for read monitoring and accept monitoring |
[in,out] | writesds | Socket descriptors list for connect monitoring only, write monitoring is not supported |
[in,out] | exceptsds | Socket descriptors list for exception monitoring, not supported. |
[in] | timeout | Is an upper bound on the amount of time elapsed before SlNetIfWifi_send() returns. Null or above 0xffff seconds means infinity timeout. The minimum timeout is 10 milliseconds, less than 10 milliseconds will be set automatically to 10 milliseconds. Max microseconds supported is 0xfffc00. In trigger mode the timeout fields must be set to zero. |
Definition at line 208 of file slnetifwifi.c.
int32_t SlNetIfWifi_send | ( | int16_t | sd, |
void * | sdContext, | ||
const void * | buf, | ||
uint32_t | len, | ||
uint32_t | flags | ||
) |
Write data to TCP socket.
The SlNetIfWifi_send function is used to transmit a message to another socket. Returns immediately after sending data to device. In case of TCP failure an async event SLNETSOCK_SOCKET_TX_FAILED_EVENT is going to be received.
In case of a RAW socket (transceiver mode), extra 4 bytes should be reserved at the end of the frame data buffer for WLAN FCS
[in] | sd | Socket descriptor (handle) |
[in] | sdContext | May store socket data if implemented in the SlNetIfWifi_socket function. |
[in] | buf | Points to a buffer containing the message to be sent |
[in] | len | Message size in bytes. Range: 1-1460 bytes |
[in] | flags | Upper 8 bits specifies the security flags Lower 24 bits specifies the type of message reception. On this version, the lower 24 bits are not supported for TCP. For transceiver mode, the SLNETSOCK_WLAN_RAW_RF_TX_PARAMS macro can be used to determine transmission parameters (channel,rate,tx_power,preamble) |
Definition at line 347 of file slnetifwifi.c.
int32_t SlNetIfWifi_sendTo | ( | int16_t | sd, |
void * | sdContext, | ||
const void * | buf, | ||
uint32_t | len, | ||
uint32_t | flags, | ||
const SlNetSock_Addr_t * | to, | ||
SlNetSocklen_t | tolen | ||
) |
Write data to socket.
The SlNetIfWifi_sendTo function is used to transmit a message on a connectionless socket (connection less socket SLNETSOCK_SOCK_DGRAM, SLNETSOCK_SOCK_RAW).
Returns immediately after sending data to device.
In case of transmission failure an async event SLNETSOCK_SOCKET_TX_FAILED_EVENT is going to be received.
[in] | sd | Socket descriptor (handle) |
[in] | sdContext | May store socket data if implemented in the SlNetIfWifi_socket function. |
[in] | buf | Points to a buffer containing the message to be sent |
[in] | len | message size in bytes. Range: 1-1460 bytes |
[in] | flags | Upper 8 bits specifies the security flags Lower 24 bits specifies the type of message reception. On this version, the lower 24 bits are not supported |
[in] | to | Pointer to an address structure indicating the destination address. sockaddr: - code for the address format. - socket address, the length depends on the code format |
[in] | tolen | Destination address structure size |
Definition at line 359 of file slnetifwifi.c.
int32_t SlNetIfWifi_setSockOpt | ( | int16_t | sd, |
void * | sdContext, | ||
int16_t | level, | ||
int16_t | optname, | ||
void * | optval, | ||
SlNetSocklen_t | optlen | ||
) |
Set socket options-.
The SlNetIfWifi_setSockOpt function manipulate the options associated with a socket.
Options may exist at multiple protocol levels; they are always present at the uppermost socket level.
When manipulating socket options the level at which the option resides and the name of the option must be specified. To manipulate options at the socket level, level is specified as SOL_SOCKET. To manipulate options at any other level the protocol number of the appropriate protocol controlling the option is supplied. For example, to indicate that an option is to be interpreted by the TCP protocol, level should be set to the protocol number of TCP;
The parameters optval and optlen are used to access opt_values for SlNetIfWifi_setSockOpt(). For SlNetIfWifi_getSockOpt() they identify a buffer in which the value for the requested option(s) are to be returned. For SlNetIfWifi_getSockOpt(), optlen is a value-result parameter, initially containing the size of the buffer pointed to by option_value, and modified on return to indicate the actual size of the value returned. If no option value is to be supplied or returned, option_value may be NULL.
[in] | sd | Socket descriptor (handle) |
[in] | sdContext | May store socket data if implemented in the SlNetIfWifi_socket function. |
[in] | level | Defines the protocol level for this option
|
[in] | optname | Defines the option name to interrogate
|
[in] | optval | Specifies a value for the option |
[in] | optlen | Specifies the length of the option value |
Definition at line 225 of file slnetifwifi.c.
int16_t SlNetIfWifi_socket | ( | void * | ifContext, |
int16_t | Domain, | ||
int16_t | Type, | ||
int16_t | Protocol, | ||
void ** | sdContext | ||
) |
Create an endpoint for communication.
The SlNetIfWifi_socket function creates a new socket of a certain socket type, identified by an integer number, and allocates system resources to it.
This function is called by the application layer to obtain a socket descriptor (handle).
[in] | ifContext | Stores interface data if CreateContext function supported and implemented. |
[in] | domain | Specifies the protocol family of the created socket. For example:
|
[in] | type | Specifies the socket type, which determines the semantics of communication over the socket. The socket types supported by the system are implementation-dependent. Possible socket types include:
|
[in] | protocol | Specifies a particular transport to be used with the socket. The most common are
|
[in] | sdContext | Allocate and store socket data if needed for using in other slnetwifi socket functions |
Definition at line 126 of file slnetifwifi.c.
int32_t SlNetIfWifi_sockstartSec | ( | int16_t | sd, |
void * | sdContext, | ||
SlNetSockSecAttrib_t * | secAttrib, | ||
uint8_t | flags | ||
) |
Start a security session on an opened socket.
The SlNetIfWifi_sockstartSec function is used start a security session on an opened socket. If the security handle is NULL the session would be started with the default security settings.
[in] | sd | Socket descriptor (handle) |
[in] | sdContext | May store socket data if implemented in the SlNetIfWifi_socket function. |
[in] | secAttrib | Secure attribute handle |
[in] | flags | Specifies flags. The available flags are:
|
Definition at line 371 of file slnetifwifi.c.
struct SlInAddr_t |
Definition at line 223 of file sl_socket.h.
Data Fields | ||
---|---|---|
_u32 | s_addr | |
union S_un | S_un |
union SlInAddr_t::S_un |
Definition at line 228 of file sl_socket.h.
Data Fields | ||
---|---|---|
_u32 | S_addr | |
struct S_un | S_un_b | |
struct S_un | S_un_w |
struct SlInAddr_t::S_un.S_un_b |
Definition at line 229 of file sl_socket.h.
Data Fields | ||
---|---|---|
_u8 | s_b1 | |
_u8 | s_b2 | |
_u8 | s_b3 | |
_u8 | s_b4 |
struct SlInAddr_t::S_un.S_un_w |
Definition at line 230 of file sl_socket.h.
Data Fields | ||
---|---|---|
_u16 | s_w1 | |
_u16 | s_w2 |
struct SlIn6Addr_t |
Definition at line 237 of file sl_socket.h.
Data Fields | ||
---|---|---|
union SlIn6Addr_t | _S6_un |
union SlIn6Addr_t._S6_un |
Definition at line 239 of file sl_socket.h.
Data Fields | ||
---|---|---|
_u32 | _S6_u32[4] | |
_u8 | _S6_u8[16] |
struct SlSockKeepalive_t |
Definition at line 248 of file sl_socket.h.
Data Fields | ||
---|---|---|
_u32 | KeepaliveEnabled |
struct SlSockReuseaddr_t |
Definition at line 253 of file sl_socket.h.
Data Fields | ||
---|---|---|
_u32 | ReuseaddrEnabled |
struct SlSockRxNoIpBoundary_t |
Definition at line 258 of file sl_socket.h.
Data Fields | ||
---|---|---|
_i32 | RxIpNoBoundaryEnabled |
struct SlSockWinsize_t |
Definition at line 263 of file sl_socket.h.
Data Fields | ||
---|---|---|
_u32 | WinSize |
struct SlSockNonblocking_t |
Definition at line 268 of file sl_socket.h.
Data Fields | ||
---|---|---|
_u32 | NonBlockingEnabled |
struct SlSocketAsyncEvent_t |
Definition at line 273 of file sl_socket.h.
Data Fields | ||
---|---|---|
_i8 | pExtraInfo[128] | |
_u8 | Sd | |
_u8 | Type | |
_i16 | Val |
struct SlSockTxFailEventData_t |
Definition at line 281 of file sl_socket.h.
Data Fields | ||
---|---|---|
_u8 | Padding | |
_u8 | Sd | |
_i16 | Status |
union SlSockEventData_u |
Definition at line 289 of file sl_socket.h.
Data Fields | ||
---|---|---|
SlSocketAsyncEvent_t | SockAsyncData | |
SlSockTxFailEventData_t | SockTxFailData |
struct SlSockEvent_t |
Definition at line 296 of file sl_socket.h.
Data Fields | ||
---|---|---|
_u32 | Event | |
SlSockEventData_u | SocketAsyncEvent |
struct SlSockTriggerEvent_t |
Definition at line 302 of file sl_socket.h.
Data Fields | ||
---|---|---|
_u32 | Event | |
_u32 | EventData |
struct SlSockSecureALPN_t |
Definition at line 309 of file sl_socket.h.
Data Fields | ||
---|---|---|
_u32 | SecureALPN |
struct SlSockSecureMask_t |
Definition at line 314 of file sl_socket.h.
Data Fields | ||
---|---|---|
_u32 | SecureMask |
struct SlSockSecureMethod_t |
Definition at line 319 of file sl_socket.h.
Data Fields | ||
---|---|---|
_u8 | SecureMethod |
struct SlSockSSLCertInfo_t |
Definition at line 324 of file sl_socket.h.
struct SlSockSSLConnectionParams_t |
Definition at line 338 of file sl_socket.h.
Data Fields | ||
---|---|---|
_u32 | SecureALPNChosenProtocol | |
_u32 | SecureCipherSuit | |
_u32 | SecureIsPeerValidated | |
SlSockSSLCertInfo_t | SecurePeerCertinfo | |
_u32 | SecureVersion |
struct SlRxMetrics_TLV_t |
Definition at line 354 of file sl_socket.h.
Data Fields | ||
---|---|---|
_u16 | length | |
_u16 | type |
struct SlSockIpMreq_t |
Definition at line 421 of file sl_socket.h.
Data Fields | ||
---|---|---|
SlInAddr_t | imr_interface | |
SlInAddr_t | imr_multiaddr |
struct SlSockIpV6Mreq_t |
Definition at line 427 of file sl_socket.h.
Data Fields | ||
---|---|---|
_u32 | ipv6mr_interface | |
SlIn6Addr_t | ipv6mr_multiaddr |
struct SlSocklinger_t |
Definition at line 432 of file sl_socket.h.
Data Fields | ||
---|---|---|
_u32 | l_linger | |
_u32 | l_onoff |
struct SlTimeval_t |
Definition at line 442 of file sl_socket.h.
Data Fields | ||
---|---|---|
SlTime_t | tv_sec | |
SlSuseconds_t | tv_usec |
struct SlSockAddr_t |
Definition at line 451 of file sl_socket.h.
Data Fields | ||
---|---|---|
_u8 | sa_data[14] | |
_u16 | sa_family |
struct SlSockAddrIn6_t |
Definition at line 457 of file sl_socket.h.
Data Fields | ||
---|---|---|
SlIn6Addr_t | sin6_addr | |
_u16 | sin6_family | |
_u32 | sin6_flowinfo | |
_u16 | sin6_port | |
_u32 | sin6_scope_id |
struct SlSockAddrIn_t |
Definition at line 468 of file sl_socket.h.
Data Fields | ||
---|---|---|
SlInAddr_t | sin_addr | |
_u16 | sin_family | |
_u16 | sin_port | |
_i8 | sin_zero[8] |
struct SlSockSecureFiles_t |
Definition at line 476 of file sl_socket.h.
Data Fields | ||
---|---|---|
_u8 | SecureFiles[4] |
struct SlFdSet_t |
Definition at line 481 of file sl_socket.h.
Data Fields | ||
---|---|---|
_u32 | fd_array[(SL_FD_SETSIZE+(_u8) 31)/(_u8) 32] |
struct SlTransceiverRxOverHead_t |
Definition at line 486 of file sl_socket.h.
Data Fields | ||
---|---|---|
_u8 | Channel | |
_u8 | Padding | |
_u8 | Rate | |
_i8 | Rssi | |
_u32 | Timestamp |
struct SlRxMetricsEnableDisableRXOnBSS_t |
Definition at line 495 of file sl_socket.h.
Data Fields | ||
---|---|---|
_u32 | enableDisable |
_u32 _S6_u32[4] |
Definition at line 242 of file sl_socket.h.
_u8 _S6_u8[16] |
Definition at line 241 of file sl_socket.h.
union { ... } _S6_un |
_u8 Channel |
Definition at line 489 of file sl_socket.h.
_u32 enableDisable |
Definition at line 497 of file sl_socket.h.
_u32 Event |
Definition at line 298 of file sl_socket.h.
_u32 Event |
Definition at line 304 of file sl_socket.h.
_u32 EventData |
Definition at line 305 of file sl_socket.h.
_u32 fd_array[(SL_FD_SETSIZE+(_u8) 31)/(_u8) 32] |
Definition at line 483 of file sl_socket.h.
_i8 FromDate[8] |
Definition at line 328 of file sl_socket.h.
SlInAddr_t imr_interface |
Definition at line 424 of file sl_socket.h.
SlInAddr_t imr_multiaddr |
Definition at line 423 of file sl_socket.h.
_u32 ipv6mr_interface |
Definition at line 429 of file sl_socket.h.
SlIn6Addr_t ipv6mr_multiaddr |
Definition at line 428 of file sl_socket.h.
_i8 IssuerName[SL_MAX_ISSUER_AND_SUBJECT_NAME_LEN] |
Definition at line 331 of file sl_socket.h.
_i8 IssuerNameLen |
Definition at line 333 of file sl_socket.h.
_u16 IssuerNameXoredSha1 |
Definition at line 327 of file sl_socket.h.
_u32 KeepaliveEnabled |
Definition at line 250 of file sl_socket.h.
_u32 l_linger |
Definition at line 435 of file sl_socket.h.
_u32 l_onoff |
Definition at line 434 of file sl_socket.h.
_u16 length |
Definition at line 357 of file sl_socket.h.
_u32 NonBlockingEnabled |
Definition at line 270 of file sl_socket.h.
_u8 Padding |
Definition at line 285 of file sl_socket.h.
_i8 Padding[2] |
Definition at line 334 of file sl_socket.h.
_u8 Padding |
Definition at line 491 of file sl_socket.h.
_i8 pExtraInfo[128] |
Definition at line 278 of file sl_socket.h.
_u8 Rate |
Definition at line 488 of file sl_socket.h.
_u32 ReuseaddrEnabled |
Definition at line 255 of file sl_socket.h.
_i8 Rssi |
Definition at line 490 of file sl_socket.h.
_i32 RxIpNoBoundaryEnabled |
Definition at line 260 of file sl_socket.h.
_u32 s_addr |
Definition at line 226 of file sl_socket.h.
_u32 S_addr |
Definition at line 231 of file sl_socket.h.
_u8 s_b1 |
Definition at line 229 of file sl_socket.h.
_u8 s_b2 |
Definition at line 229 of file sl_socket.h.
_u8 s_b3 |
Definition at line 229 of file sl_socket.h.
_u8 s_b4 |
Definition at line 229 of file sl_socket.h.
union SlInAddr_t::S_un S_un |
struct { ... } S_un_b |
struct { ... } S_un_w |
_u16 s_w1 |
Definition at line 230 of file sl_socket.h.
_u16 s_w2 |
Definition at line 230 of file sl_socket.h.
_u8 sa_data[14] |
Definition at line 454 of file sl_socket.h.
_u16 sa_family |
Definition at line 453 of file sl_socket.h.
_u8 Sd |
Definition at line 275 of file sl_socket.h.
_u8 Sd |
Definition at line 284 of file sl_socket.h.
_u32 SecureALPN |
Definition at line 311 of file sl_socket.h.
_u32 SecureALPNChosenProtocol |
Definition at line 343 of file sl_socket.h.
_u32 SecureCipherSuit |
Definition at line 341 of file sl_socket.h.
_u8 SecureFiles[4] |
Definition at line 478 of file sl_socket.h.
_u32 SecureIsPeerValidated |
Definition at line 342 of file sl_socket.h.
_u32 SecureMask |
Definition at line 316 of file sl_socket.h.
_u8 SecureMethod |
Definition at line 321 of file sl_socket.h.
SlSockSSLCertInfo_t SecurePeerCertinfo |
Definition at line 350 of file sl_socket.h.
_u32 SecureVersion |
Definition at line 340 of file sl_socket.h.
SlIn6Addr_t sin6_addr |
Definition at line 462 of file sl_socket.h.
_u16 sin6_family |
Definition at line 459 of file sl_socket.h.
_u32 sin6_flowinfo |
Definition at line 461 of file sl_socket.h.
_u16 sin6_port |
Definition at line 460 of file sl_socket.h.
_u32 sin6_scope_id |
Definition at line 463 of file sl_socket.h.
SlInAddr_t sin_addr |
Definition at line 472 of file sl_socket.h.
_u16 sin_family |
Definition at line 470 of file sl_socket.h.
_u16 sin_port |
Definition at line 471 of file sl_socket.h.
_i8 sin_zero[8] |
Definition at line 473 of file sl_socket.h.
SlNetIf_Config_t SlNetIfConfigWifi |
SlNetIfConfigWifi structure contains all the function callbacks that are expected to be filled by the relevant network stack interface Each interface has different capabilities, so not all the API's must be supported. Interface that is not supporting a non-mandatory API are set to NULL
Definition at line 65 of file slnetifwifi.c.
SlSocketAsyncEvent_t SockAsyncData |
Definition at line 292 of file sl_socket.h.
SlSockEventData_u SocketAsyncEvent |
Definition at line 299 of file sl_socket.h.
SlSockTxFailEventData_t SockTxFailData |
Definition at line 291 of file sl_socket.h.
_i16 Status |
Definition at line 283 of file sl_socket.h.
_i8 SubjectName[SL_MAX_ISSUER_AND_SUBJECT_NAME_LEN] |
Definition at line 330 of file sl_socket.h.
_i8 SubjectNameLen |
Definition at line 332 of file sl_socket.h.
_u16 SubjectNameXoredSha1 |
Definition at line 326 of file sl_socket.h.
_u32 Timestamp |
Definition at line 492 of file sl_socket.h.
_i8 ToDate[8] |
Definition at line 329 of file sl_socket.h.
SlTime_t tv_sec |
Definition at line 444 of file sl_socket.h.
SlSuseconds_t tv_usec |
Definition at line 445 of file sl_socket.h.
_u8 Type |
Definition at line 276 of file sl_socket.h.
_u16 type |
Definition at line 356 of file sl_socket.h.
_i16 Val |
Definition at line 277 of file sl_socket.h.
_u32 WinSize |
Definition at line 265 of file sl_socket.h.