SimpleLink CC31xx/CC32xx Host Driver
Version 3.0.1.60
Simplifies the implementation of Internet connectivity
|
Controls the configuration of the device addresses (i.e. IP and MAC addresses) More...
Functions | |
_i16 | sl_NetCfgSet (const _u16 ConfigId, const _u16 ConfigOpt, const _u16 ConfigLen, const _u8 *pValues) |
Setting network configurations. More... | |
_i16 | sl_NetCfgGet (const _u16 ConfigId, _u16 *pConfigOpt, _u16 *pConfigLen, _u8 *pValues) |
Getting network configurations. More... | |
Controls the configuration of the device addresses (i.e. IP and MAC addresses)
_i16 sl_NetCfgGet | ( | const _u16 | ConfigId, |
_u16 * | pConfigOpt, | ||
_u16 * | pConfigLen, | ||
_u8 * | pValues | ||
) |
Getting network configurations.
[in] | ConfigId | Configuration id |
[out] | pConfigOpt | Get configurations option |
[out] | pConfigLen | The length of the allocated memory as input, when the function complete, the value of this parameter would be the len that actually read from the device. If the device return length that is longer from the input value, the function will cut the end of the returned structure and will return ESMALLBUF |
[out] | pValues | - get configurations values |
Definition at line 104 of file netcfg.c.
_i16 sl_NetCfgSet | ( | const _u16 | ConfigId, |
const _u16 | ConfigOpt, | ||
const _u16 | ConfigLen, | ||
const _u8 * | pValues | ||
) |
Setting network configurations.
[in] | ConfigId | Configuration id:
|
[in] | ConfigOpt | Configurations option:
|
[in] | ConfigLen | Configurations len |
[in] | pValues | Configurations values |
Definition at line 63 of file netcfg.c.
struct SlNetCfgIpV4DnsClientArgs_t |
struct SlNetCfgIpV6DnsClientArgs_t |
struct SlNetCfgIpv4DhcpClient_t |
struct SlNetCfgIpV4Args_t |
struct SlNetCfgIpV6Args_t |