#include <I2SCC32XX.h>
§ pinSD1
uint32_t I2SCC32XX_HWAttrs_::pinSD1 |
Pin used for SD1 signal. Must be chosen between I2SCC32XX_PIN_50_SD1 and I2SCC32XX_PIN_60_SD1. Signal can be deactivated using I2SCC32XX_PIN_UNUSED.
§ pinSD0
uint32_t I2SCC32XX_HWAttrs_::pinSD0 |
Pin used for SD0 signal. Must be chosen between I2SCC32XX_PIN_45_SD0, I2SCC32XX_PIN_50_SD0, I2SCC32XX_PIN_52_SD0, and I2SCC32XX_PIN_64_SD0. Signal can be deactivated using I2SCC32XX_PIN_UNUSED.
§ pinSCK
uint32_t I2SCC32XX_HWAttrs_::pinSCK |
Pin used for SCK signal. Must be chosen between I2SCC32XX_PIN_03_SCK, I2SCC32XX_PIN_52_SCK, and I2SCC32XX_PIN_53_SCK. Signal can be deactivated using I2SCC32XX_PIN_UNUSED.
§ pinSCKX
uint32_t I2SCC32XX_HWAttrs_::pinSCKX |
Pin used for SCKX signal. Must be I2SCC32XX_PIN_62_SCKX.
§ pinWS
uint32_t I2SCC32XX_HWAttrs_::pinWS |
Pin used for WS signal. Must be chosen between I2SCC32XX_PIN_02_WS, I2SCC32XX_PIN_15_WS, I2SCC32XX_PIN_17_WS, I2SCC32XX_PIN_21_WS, I2SCC32XX_PIN_45_WS, I2SCC32XX_PIN_53_WS, and I2SCC32XX_PIN_63_WS. This signal cannot be deactivated.
§ rxChannelIndex
uint32_t I2SCC32XX_HWAttrs_::rxChannelIndex |
§ txChannelIndex
uint32_t I2SCC32XX_HWAttrs_::txChannelIndex |
uDMA channel index used for Rx. Must be chosen between UDMA_CH4_I2S_RX and UDMA_CH18_I2S_RX. Does not need to be set if no using the DMA transfers.
§ intPriority
uint32_t I2SCC32XX_HWAttrs_::intPriority |
uDMA channel index used for Tx. Must be chosen between UDMA_CH5_I2S_TX and UDMA_CH19_I2S_TX. Does not need to be set if no using the DMA transfers.
The documentation for this struct was generated from the following file: