Used to specify the miscellaneous options during EDMA3 Driver Initialization. More...
#include <edma3_drv.h>
Data Fields | |
unsigned short | isSlave |
unsigned short | param |
Used to specify the miscellaneous options during EDMA3 Driver Initialization.
This configuration structure is used to specify some misc options while creating the Driver object. New options may also be added into this structure in future.
unsigned short EDMA3_DRV_MiscParam::isSlave |
In a multi-master system (for e.g. ARM + DSP), this option is used to distinguish between Master and Slave. Only the Master is allowed to program the global EDMA3 registers (like Queue priority, Queue water- mark level, error registers etc).
unsigned short EDMA3_DRV_MiscParam::param |
For future use